License | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
Extra Information for Peripheral DMA Controller | |
Examples for Peripheral DMA Controller | This is a list of the available Quick Start guides (QSGs) and example applications for SAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) Driver |
 Quick Start Guide for PDC - Basic | This is the quickstart guide for SAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) Driver with step-by-step instructions on how to configure and use the driver |
 Peripheral DMA Controller Example | |
Document Revision History | |
Extra Information for Reset Controller Driver | |
Examples for Reset Controller Driver | This is a list of the available Quick Start Guides (QSGs) and example applications for SAM3/4C/4CM/4CP/4E/4N/4S/G/V71/V70/S70/E70 Reset Controller (RSTC) Driver |
 Quick Start guide for SAM RSTC driver | This is the quick start guide for the SAM3/4C/4CM/4CP/4E/4N/4S/G/V71/V70/S70/E70 Reset Controller (RSTC) Driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 Reset Controller (RSTC) Example | |
Document Revision History | |
Quick Start Guide for the SAM PIO driver | This is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
Advanced use case - Interrupt driven edge detection | |
Quick start guide for the SAM PMC module | This is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Extra Information for Timer Counter Driver | |
Examples for Timer Counter | This is a list of the available Quick Start Guides (QSGs) and example applications for SAM3/4S/4L/4E/4N/4CM/4C/G Timer Counter (TC) Driver |
 Quick Start Guide for the TC driver | This is the quick start guide for the SAM3/4S/4L/4E/4N/4CM/4C/G Timer Counter (TC) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
Document Revision History | |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
 Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Quick Start Guide for the System Clock Management service (SAM4S) | This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases |
Advanced use case - Peripheral Bus Clock Management (SAM4S) | |
Quick Start Guide for the ILI93XX | LCD Glass component |
Quick start guide for Serial Interface service | This is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases |
 Advanced use case - Send a packet of serial data | In this use case, the USART module is configured for: |
Quick start guide for the SAM USART module | This is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 USART receive character and echo back | In this use case, the USART module is configured for: |
 USART receive character and echo back via interrupts | In this use case, the USART module is configured for: |
uxQueueMessagesWaiting | Queue |
vQueueDelete | Queue |
vSemaphoreDelete | Semphr |
xTaskHandle | Task |
taskYIELD | Task |
taskENTER_CRITICAL | Task |
taskEXIT_CRITICAL | Task |
taskDISABLE_INTERRUPTS | Task |
taskENABLE_INTERRUPTS | Task |
xTaskGetTickCount | Task |
uxTaskGetNumberOfTasks | Task |
pcTaskGetTaskName | Task |
vTaskList | Task |
vTaskGetRunTimeStats | Task |
Quick Start Guide for the SPI Master Driver | This is the quick start guide for the SPI Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 Basic setup for SPI master on XMEGA devices | |
Quickstart guide for SAM SPI driver | This is the quickstart guide for the SAM SPI driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
"SAM4S-EK - Operating frequencies" | This page lists several definition related to the board operating frequency |
"SAM4S-EK - Board informations" | This page lists several definition related to the board description |
"SAM4S-EK - USB device" | |
"SAM4S-EK - External components" | This page lists the definitions related to external on-board components located in the board.h file for the SAM4S-EK |
"SAM4S-EK - Memories" | This page lists definitions related to internal & external on-board memories |
Todo List | |
Deprecated List | |
Bug List | |