Transmission Control Protocol, incoming traffic.
The input processing functions of the TCP layer.
These functions are generally called in the order (ip_input() ->) tcp_input() -> * tcp_process() -> tcp_receive() (-> application).
#include "lwip/opt.h"
#include "lwip/tcp_impl.h"
#include "lwip/def.h"
#include "lwip/ip_addr.h"
#include "lwip/netif.h"
#include "lwip/mem.h"
#include "lwip/memp.h"
#include "lwip/inet_chksum.h"
#include "lwip/stats.h"
#include "lwip/snmp.h"
#include "arch/perf.h"
Functions | |
void | tcp_input (struct pbuf *p, struct netif *inp) |
The initial input processing of TCP. More... | |
static err_t | tcp_listen_input (struct tcp_pcb_listen *pcb) |
Called by tcp_input() when a segment arrives for a listening connection (from tcp_input()). More... | |
static void | tcp_oos_insert_segment (struct tcp_seg *cseg, struct tcp_seg *next) |
Insert segment into the list (segments covered with new one will be deleted) More... | |
static void | tcp_parseopt (struct tcp_pcb *pcb) |
Parses the options contained in the incoming segment. More... | |
static err_t | tcp_process (struct tcp_pcb *pcb) |
Implements the TCP state machine. More... | |
static void | tcp_receive (struct tcp_pcb *pcb) |
Called by tcp_process. More... | |
static err_t | tcp_timewait_input (struct tcp_pcb *pcb) |
Called by tcp_input() when a segment arrives for a connection in TIME_WAIT. More... | |
Variables | |
static u32_t | ackno |
static u8_t | flags |
static struct tcp_seg | inseg |
static struct ip_hdr * | iphdr |
static struct pbuf * | recv_data |
static u8_t | recv_flags |
static u32_t | seqno |
struct tcp_pcb * | tcp_input_pcb |
static struct tcp_hdr * | tcphdr |
static u16_t | tcplen |
The initial input processing of TCP.
It verifies the TCP header, demultiplexes the segment between the PCBs and passes it on to tcp_process(), which implements the TCP finite state machine. This function is called by the IP layer (in ip_input()).
p | received TCP segment to process (p->payload pointing to the IP header) |
inp | network interface on which this segment was received |
References tcp_pcb::acked, ackno, CLOSED, current_iphdr_dest, current_iphdr_src, ERR_ABRT, ERR_CLSD, ERR_OK, ERR_RST, tcp_pcb::errf, flags, pbuf::flags, tcp_pcb::flags, inet_chksum_pseudo(), inseg, ip_addr_cmp, ip_addr_isany, ip_addr_isbroadcast, ip_addr_ismulticast, ip_current_dest_addr, ip_current_src_addr, IP_PROTO_TCP, IPH_HL, tcp_seg::len, LISTEN, tcp_listen_pcbs_t::listen_pcbs, LWIP_ASSERT, LWIP_DEBUGF, memp_free(), tcp_seg::next, ntohl, ntohs, NULL, tcp_seg::p, pbuf::payload, PBUF_FLAG_PUSH, PBUF_FLAG_TCP_FIN, pbuf_free(), pbuf_header(), PERF_START, PERF_STOP, tcp_pcb::rcv_wnd, recv_data, recv_flags, tcp_pcb::refused_data, tcp_pcb::remote_port, seqno, snmp_inc_tcpinerrs, snmp_inc_tcpinsegs, tcp_abort(), tcp_active_pcbs, tcp_debug_print, tcp_debug_print_flags, tcp_debug_print_state, TCP_EVENT_CLOSED, TCP_EVENT_ERR, TCP_EVENT_RECV, TCP_EVENT_SENT, TCP_FIN, TCP_INPUT_DEBUG, tcp_listen_input(), tcp_listen_pcbs, tcp_output(), tcp_pcb_remove(), tcp_pcbs_sane, tcp_process(), tcp_process_refused_data(), TCP_PSH, TCP_RST, tcp_rst(), TCP_RST_DEBUG, TCP_STATS_INC, TCP_SYN, tcp_timewait_input(), tcp_tw_pcbs, TCP_WND, TCPH_FLAGS, TCPH_HDRLEN, tcphdr, tcp_seg::tcphdr, tcplen, TF_CLOSED, TF_GOT_FIN, TF_RESET, TF_RXCLOSED, TIME_WAIT, pbuf::tot_len, U16_F, and X16_F.
Referenced by ip_input().
|
static |
Called by tcp_input() when a segment arrives for a listening connection (from tcp_input()).
pcb | the tcp_pcb_listen for which a segment arrived |
References ackno, current_iphdr_dest, current_iphdr_src, ERR_ABRT, ERR_MEM, ERR_OK, flags, ip_addr_copy, ip_current_dest_addr, ip_current_src_addr, LWIP_DEBUGF, tcp_pcb::mss, NULL, tcp_pcb::rcv_ann_right_edge, tcp_pcb::rcv_nxt, tcp_pcb::remote_port, seqno, tcp_pcb::snd_wl1, tcp_pcb::snd_wnd, tcp_pcb::snd_wnd_max, snmp_inc_tcppassiveopens, SOF_INHERITED, tcp_pcb::ssthresh, SYN_RCVD, tcp_abandon(), TCP_ACK, tcp_alloc(), TCP_DEBUG, tcp_eff_send_mss(), tcp_enqueue_flags(), tcp_output(), tcp_parseopt(), TCP_REG_ACTIVE, TCP_RST, tcp_rst(), TCP_RST_DEBUG, TCP_STATS_INC, TCP_SYN, tcplen, and U16_F.
Referenced by tcp_input().
Insert segment into the list (segments covered with new one will be deleted)
Called from tcp_receive()
References tcp_seg::len, next, tcp_seg::next, NULL, tcp_seg::p, pbuf_realloc(), seqno, TCP_FIN, tcp_seg_free(), tcp_segs_free(), TCP_SEQ_GEQ, TCP_SEQ_GT, TCPH_FLAGS, TCPH_SET_FLAG, and tcp_seg::tcphdr.
Referenced by tcp_receive().
Parses the options contained in the incoming segment.
Called from tcp_listen_input() and tcp_process(). Currently, only the MSS option is supported!
pcb | the tcp_pcb for which a segment arrived |
References flags, tcp_pcb::flags, LWIP_DEBUGF, tcp_pcb::mss, ntohl, seqno, TCP_HLEN, TCP_INPUT_DEBUG, TCP_MSS, TCP_SEQ_BETWEEN, TCP_SYN, TCPH_HDRLEN, tcplen, and TF_TIMESTAMP.
Referenced by tcp_listen_input(), and tcp_process().
Implements the TCP state machine.
Called by tcp_input. In some states tcp_receive() is called to receive data. The tcp_seg argument will be freed by the caller (tcp_input()) unless the recv_data pointer in the pcb is set.
pcb | the tcp_pcb for which a segment arrived |
References tcp_pcb::acked, ackno, CLOSE_WAIT, CLOSED, CLOSING, tcp_pcb::cwnd, ERR_ABRT, ERR_OK, ERR_RST, ESTABLISHED, FIN_WAIT_1, FIN_WAIT_2, flags, tcp_pcb::flags, inseg, ip_current_dest_addr, ip_current_src_addr, tcp_pcb::keep_cnt_sent, LAST_ACK, tcp_pcb::lastack, LWIP_ASSERT, LWIP_DEBUGF, tcp_pcb::mss, tcp_seg::next, tcp_pcb::nrtx, ntohl, NULL, tcp_pcb::rcv_ann_right_edge, tcp_pcb::rcv_nxt, tcp_pcb::rcv_wnd, recv_flags, tcp_pcb::rtime, seqno, tcp_pcb::snd_buf, tcp_pcb::snd_nxt, tcp_pcb::snd_queuelen, tcp_pcb::snd_wl1, tcp_pcb::snd_wnd, tcp_pcb::snd_wnd_max, tcp_pcb::ssthresh, SYN_RCVD, SYN_SENT, tcp_abort(), TCP_ACK, tcp_ack_now, TCP_DEBUG, tcp_eff_send_mss(), TCP_EVENT_ACCEPT, TCP_EVENT_CONNECTED, TCP_INPUT_DEBUG, tcp_parseopt(), tcp_pcb_purge(), TCP_QLEN_DEBUG, tcp_receive(), TCP_REG, tcp_rexmit(), TCP_RMV_ACTIVE, TCP_RST, tcp_rst(), tcp_seg_free(), TCP_SEQ_BETWEEN, TCP_SYN, tcp_ticks, tcp_tw_pcbs, tcp_seg::tcphdr, tcplen, TF_ACK_DELAY, TF_CLOSED, TF_GOT_FIN, TF_RESET, TF_RXCLOSED, TIME_WAIT, tcp_pcb::tmr, U16_F, U32_F, and tcp_pcb::unacked.
Referenced by tcp_input().
Called by tcp_process.
Checks if the given segment is an ACK for outstanding data, and if so frees the memory of the buffered data. Next, is places the segment on any of the receive queues (pcb->recved or pcb->ooseq). If the segment is buffered, the pbuf is referenced by pbuf_ref so that it will not be freed until it has been removed from the buffer.
If the incoming segment constitutes an ACK for a segment that was used for RTT estimation, the RTT is estimated here as well.
Called from tcp_process().
References tcp_pcb::acked, ackno, CLOSE_WAIT, tcp_pcb::cwnd, tcp_pcb::dupacks, ESTABLISHED, flags, tcp_pcb::flags, inseg, tcp_pcb::lastack, pbuf::len, tcp_seg::len, LWIP_ASSERT, LWIP_DEBUGF, tcp_pcb::mss, pbuf::next, next, tcp_seg::next, tcp_pcb::nrtx, ntohl, NULL, tcp_pcb::ooseq, tcp_seg::p, pbuf_cat(), pbuf_clen(), pbuf_header(), pbuf_realloc(), tcp_pcb::persist_backoff, tcp_pcb::persist_cnt, tcp_pcb::polltmr, tcp_pcb::rcv_nxt, tcp_pcb::rcv_wnd, recv_flags, tcp_pcb::rtime, tcp_pcb::rto, tcp_pcb::rtseq, tcp_pcb::rttest, tcp_pcb::sa, seqno, tcp_pcb::snd_buf, tcp_pcb::snd_nxt, tcp_pcb::snd_queuelen, tcp_pcb::snd_wl1, tcp_pcb::snd_wl2, tcp_pcb::snd_wnd, tcp_pcb::snd_wnd_max, tcp_pcb::ssthresh, tcp_pcb::sv, TCP_ACK, tcp_ack, tcp_ack_now, TCP_CWND_DEBUG, TCP_FIN, TCP_INPUT_DEBUG, tcp_oos_insert_segment(), TCP_QLEN_DEBUG, tcp_rexmit_fast(), TCP_RTO_DEBUG, tcp_seg_copy(), tcp_seg_free(), tcp_segs_free(), tcp_send_empty_ack(), TCP_SEQ_BETWEEN, TCP_SEQ_GEQ, TCP_SEQ_GT, TCP_SEQ_LEQ, TCP_SEQ_LT, TCP_SLOW_INTERVAL, TCP_SYN, TCP_TCPLEN, tcp_ticks, tcp_update_rcv_ann_wnd(), TCP_WND_DEBUG, TCPH_FLAGS, TCPH_FLAGS_SET, TCPH_SET_FLAG, tcp_seg::tcphdr, tcplen, TF_GOT_FIN, TF_INFR, pbuf::tot_len, U16_F, U32_F, tcp_pcb::unacked, tcp_pcb::unsent, and tcp_pcb::unsent_oversize.
Referenced by tcp_process().
Called by tcp_input() when a segment arrives for a connection in TIME_WAIT.
pcb | the tcp_pcb for which a segment arrived |
References ackno, ERR_OK, flags, tcp_pcb::flags, ip_current_dest_addr, ip_current_src_addr, tcp_pcb::rcv_nxt, tcp_pcb::rcv_wnd, seqno, TCP_FIN, tcp_output(), TCP_RST, tcp_rst(), TCP_SEQ_BETWEEN, TCP_SYN, tcp_ticks, tcplen, TF_ACK_NOW, and tcp_pcb::tmr.
Referenced by tcp_input().
|
static |
Referenced by tcp_abandon(), tcp_input(), tcp_listen_input(), tcp_process(), tcp_receive(), and tcp_timewait_input().
|
static |
Referenced by cpu_irq_save(), tcp_input(), tcp_listen_input(), tcp_parseopt(), tcp_process(), tcp_receive(), and tcp_timewait_input().
|
static |
Referenced by tcp_input(), tcp_process(), and tcp_receive().
|
static |
Referenced by icmp_input(), icmp_send_response(), ip_frag(), ip_input(), and udp_input().
|
static |
Referenced by tcp_input().
|
static |
Referenced by tcp_input(), tcp_process(), and tcp_receive().
|
static |
Referenced by tcp_abandon(), tcp_input(), tcp_listen_input(), tcp_oos_insert_segment(), tcp_parseopt(), tcp_process(), tcp_receive(), and tcp_timewait_input().
struct tcp_pcb* tcp_input_pcb |
Referenced by tcp_output().
|
static |
Referenced by tcp_input(), tcp_keepalive(), tcp_output_alloc_header(), tcp_rst(), tcp_send_empty_ack(), and tcp_zero_window_probe().
|
static |
Referenced by tcp_input(), tcp_listen_input(), tcp_parseopt(), tcp_process(), tcp_receive(), and tcp_timewait_input().