The Phy Tester Tool example demonstrates how to use the PRIME PHY layer on PLC boards.
This package should be used with any PLC board on which there is PLC hardware dedicated.
This application will configure the PRIME PHY and its serial interface to communicate with ATMEL PLC Phy Tester Tool and test PLC transmission/reception processes.
The tool is ready for set up the device configuration and perform some communications test.