PLC PRIME CRC calculation service.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
|
static uint16_t | _eval_crc_16 (const uint8_t *puc_buf_ptr, uint32_t ul_len, uint32_t ul_crc_init) |
| This function calculates the CRC16 of the input data. More...
|
|
static uint32_t | _eval_crc_32 (const uint8_t *puc_buf_ptr, uint32_t ul_len, uint32_t ul_crc_init) |
| This function calculates the CRC32 of the input data. More...
|
|
static uint8_t | _eval_crc_8 (const uint8_t *puc_buf_ptr, uint32_t ul_len, uint32_t ul_crc_init) |
| This function calculates the CRC8 of the input data. More...
|
|
static uint8_t | _eval_crc_8_usi (const uint8_t *puc_buf_ptr, uint32_t ul_len, uint32_t ul_crc_init) |
| This function calculates the CRC8 of the input data for USI. More...
|
|
uint32_t | pcrc_calculate_prime_crc (uint8_t *puc_buf, uint32_t ul_len, uint8_t uc_header_type, uint8_t uc_crc_type) |
| Calculates the CRC of the input buffer according to the PRIME spec. More...
|
|
void | pcrc_configure_sna (uint8_t *puc_sna) |
| Through this function, the SNA is configured for the PCRC service. More...
|
|