This module defines all the MAC Data Structures.
Modules | |
MAC Definitions | |
All Definitions used by the MAC Layer is described here. | |
Data Structures | |
struct | mcps_data_conf_tag |
This is the MCPS-DATA.confirm message structure. More... | |
struct | mcps_data_ind_tag |
This is the MCPS-DATA.indication message structure. More... | |
struct | mcps_data_req_tag |
This is the MCPS-DATA.request message structure. More... | |
struct | mcps_purge_conf_tag |
This is the MCPS-PURGE.confirm message structure. More... | |
struct | mcps_purge_req_tag |
This is the MCPS-PURGE.request message structure. More... | |
struct | mlme_associate_conf_tag |
This is the MLME-ASSOCIATE.confirm message structure. More... | |
struct | mlme_associate_ind_tag |
This is the MLME-ASSOCIATE.indication message structure. More... | |
struct | mlme_associate_req_tag |
This is the MLME-ASSOCIATE.request message structure. More... | |
struct | mlme_associate_resp_tag |
This is the MLME-ASSOCIATE.response message structure. More... | |
struct | mlme_beacon_notify_ind_tag |
This is the MLME-BEACON-NOTIFY.indication message structure. More... | |
struct | mlme_comm_status_ind_tag |
This is the MLME-COMM-STATUS.indication message structure. More... | |
struct | mlme_disassociate_conf_tag |
This is the MLME-DISASSOCIATE.confirm message structure. More... | |
struct | mlme_disassociate_ind_tag |
This is the MLME-DISASSOCIATE.indication message structure. More... | |
struct | mlme_disassociate_req_tag |
This is the MLME-DISASSOCIATE.request message structure. More... | |
struct | mlme_get_conf_tag |
This is the MLME-GET.confirm message structure. More... | |
struct | mlme_get_req_tag |
This is the MLME-GET.request message structure. More... | |
struct | mlme_orphan_ind_tag |
This is the MLME-ORPHAN.indication message structure. More... | |
struct | mlme_orphan_resp_tag |
This is the MLME-ORPHAN.response message structure. More... | |
struct | mlme_poll_conf_tag |
This is the MLME-POLL.confirm message structure. More... | |
struct | mlme_poll_req_tag |
This is the MLME-POLL.request message structure. More... | |
struct | mlme_reset_conf_tag |
This is the MLME-RESET.confirm message structure. More... | |
struct | mlme_reset_req_tag |
This is the MLME-RESET.request message structure. More... | |
struct | mlme_rx_enable_conf_tag |
This is the MLME-RX-ENABLE.confirm message structure. More... | |
struct | mlme_rx_enable_req_tag |
This is the MLME-RX-ENABLE.request message structure. More... | |
struct | mlme_scan_conf_tag |
This is the MLME-SCAN.confirm message structure. More... | |
struct | mlme_scan_req_tag |
This is the MLME-SCAN.request message structure. More... | |
struct | mlme_set_conf_tag |
This is the MLME-SET.confirm message structure. More... | |
struct | mlme_set_req_tag |
This is the MLME-SET.request message structure. More... | |
struct | mlme_start_conf_tag |
This is the MLME-START.confirm message structure. More... | |
struct | mlme_start_req_tag |
This is the MLME-START.request message structure. More... | |
struct | mlme_sync_loss_ind_tag |
This is the MLME-SYNC-LOSS.indication message structure. More... | |
struct | mlme_sync_req_tag |
This is the MLME-SYNC.request message structure. More... | |
union | scan_result_list_t |
Union to force alignment of variable portion of scan confirm with wpan_pandescriptor_t. More... | |
struct | wpan_addr_spec_tag |
Device address specification structure. More... | |
struct | wpan_pandescriptor_tag |
PAN descriptor information structure. More... | |
Typedefs | |
typedef struct mcps_data_conf_tag | mcps_data_conf_t |
This is the MCPS-DATA.confirm message structure. More... | |
typedef __PACK__DATA__ struct mcps_data_ind_tag | mcps_data_ind_t |
This is the MCPS-DATA.indication message structure. More... | |
typedef struct mcps_data_req_tag | mcps_data_req_t |
This is the MCPS-DATA.request message structure. More... | |
typedef struct mcps_purge_conf_tag | mcps_purge_conf_t |
This is the MCPS-PURGE.confirm message structure. More... | |
typedef struct mcps_purge_req_tag | mcps_purge_req_t |
This is the MCPS-PURGE.request message structure. More... | |
typedef struct mlme_associate_conf_tag | mlme_associate_conf_t |
This is the MLME-ASSOCIATE.confirm message structure. More... | |
typedef struct mlme_associate_ind_tag | mlme_associate_ind_t |
This is the MLME-ASSOCIATE.indication message structure. More... | |
typedef struct mlme_associate_req_tag | mlme_associate_req_t |
This is the MLME-ASSOCIATE.request message structure. More... | |
typedef struct mlme_associate_resp_tag | mlme_associate_resp_t |
This is the MLME-ASSOCIATE.response message structure. More... | |
typedef struct mlme_beacon_notify_ind_tag | mlme_beacon_notify_ind_t |
This is the MLME-BEACON-NOTIFY.indication message structure. More... | |
typedef struct mlme_comm_status_ind_tag | mlme_comm_status_ind_t |
This is the MLME-COMM-STATUS.indication message structure. More... | |
typedef struct mlme_disassociate_conf_tag | mlme_disassociate_conf_t |
This is the MLME-DISASSOCIATE.confirm message structure. More... | |
typedef struct mlme_disassociate_ind_tag | mlme_disassociate_ind_t |
This is the MLME-DISASSOCIATE.indication message structure. More... | |
typedef struct mlme_disassociate_req_tag | mlme_disassociate_req_t |
This is the MLME-DISASSOCIATE.request message structure. More... | |
typedef struct mlme_get_conf_tag | mlme_get_conf_t |
This is the MLME-GET.confirm message structure. More... | |
typedef struct mlme_get_req_tag | mlme_get_req_t |
This is the MLME-GET.request message structure. More... | |
typedef struct mlme_orphan_ind_tag | mlme_orphan_ind_t |
This is the MLME-ORPHAN.indication message structure. More... | |
typedef struct mlme_orphan_resp_tag | mlme_orphan_resp_t |
This is the MLME-ORPHAN.response message structure. More... | |
typedef struct mlme_poll_conf_tag | mlme_poll_conf_t |
This is the MLME-POLL.confirm message structure. More... | |
typedef struct mlme_poll_req_tag | mlme_poll_req_t |
This is the MLME-POLL.request message structure. More... | |
typedef struct mlme_reset_conf_tag | mlme_reset_conf_t |
This is the MLME-RESET.confirm message structure. More... | |
typedef struct mlme_reset_req_tag | mlme_reset_req_t |
This is the MLME-RESET.request message structure. More... | |
typedef struct mlme_rx_enable_conf_tag | mlme_rx_enable_conf_t |
This is the MLME-RX-ENABLE.confirm message structure. More... | |
typedef struct mlme_rx_enable_req_tag | mlme_rx_enable_req_t |
This is the MLME-RX-ENABLE.request message structure. More... | |
typedef struct mlme_scan_conf_tag | mlme_scan_conf_t |
This is the MLME-SCAN.confirm message structure. More... | |
typedef struct mlme_scan_req_tag | mlme_scan_req_t |
This is the MLME-SCAN.request message structure. More... | |
typedef struct mlme_set_conf_tag | mlme_set_conf_t |
This is the MLME-SET.confirm message structure. More... | |
typedef struct mlme_set_req_tag | mlme_set_req_t |
This is the MLME-SET.request message structure. More... | |
typedef struct mlme_start_conf_tag | mlme_start_conf_t |
This is the MLME-START.confirm message structure. More... | |
typedef struct mlme_start_req_tag | mlme_start_req_t |
This is the MLME-START.request message structure. More... | |
typedef struct mlme_sync_loss_ind_tag | mlme_sync_loss_ind_t |
This is the MLME-SYNC-LOSS.indication message structure. More... | |
typedef struct mlme_sync_req_tag | mlme_sync_req_t |
This is the MLME-SYNC.request message structure. More... | |
typedef struct wpan_addr_spec_tag | wpan_addr_spec_t |
Device address specification structure. More... | |
typedef struct wpan_pandescriptor_tag | wpan_pandescriptor_t |
PAN descriptor information structure. More... | |
Functions | |
uint8_t | mac_get_pib_attribute_size (uint8_t pib_attribute_id) |
Variables | |
uint8_t * | mlme_beacon_notify_ind_tag::AddrList |
The list of addresses of the devices for which the beacon source has data. More... | |
uint8_t | mlme_orphan_resp_tag::AssociatedMember |
TRUE if the orphaned device is associated with this coordinator or FALSE otherwise. More... | |
uint16_t | mlme_associate_resp_tag::AssocShortAddress |
The short device address allocated by the coordinator on successful association. More... | |
uint16_t | mlme_associate_conf_tag::AssocShortAddress |
The short device address allocated by the coordinator on successful association. More... | |
uint8_t | mlme_start_req_tag::BatteryLifeExtension |
If this value is TRUE, the receiver of the beaconing device is disabled macBattLifeExtPeriods full backoff periods after the interframe spacing (IFS) period of the beacon frame. More... | |
uint8_t | mlme_start_req_tag::BeaconOrder |
How often the beacon is to be transmitted. More... | |
uint8_t | mlme_beacon_notify_ind_tag::BSN |
The beacon sequence number. More... | |
uint8_t | mlme_associate_req_tag::CapabilityInformation |
Specifies the operational capabilities of the associating device. More... | |
uint8_t | mlme_associate_ind_tag::CapabilityInformation |
The operational capabilities of the device requesting association. More... | |
uint8_t | mlme_associate_req_tag::ChannelPage |
The channel page on which to attempt association. More... | |
uint8_t | mlme_scan_req_tag::ChannelPage |
The channel page on which to perform the scan. More... | |
uint8_t | mlme_scan_conf_tag::ChannelPage |
The channel page on which the scan was performed. More... | |
uint8_t | mlme_start_req_tag::ChannelPage |
The channel page on which to begin using the new superframe configuration. More... | |
uint8_t | mlme_sync_req_tag::ChannelPage |
The channel page on which to attempt coordinator synchronization. More... | |
uint8_t | mlme_sync_loss_ind_tag::ChannelPage |
The channel page on which the device lost synchronization or to which it was realigned. More... | |
enum msg_code | mcps_data_req_tag::cmdcode |
< This identifies the message as MCPS_DATA_REQUEST More... | |
enum msg_code | mcps_data_conf_tag::cmdcode |
< This identifies the message as MCPS_DATA_CONFIRM More... | |
enum msg_code | mcps_data_ind_tag::cmdcode |
< This identifies the message as MCPS_DATA_INDICATION More... | |
enum msg_code | mcps_purge_req_tag::cmdcode |
< This identifies the message as MCPS_PURGE_REQUEST More... | |
enum msg_code | mcps_purge_conf_tag::cmdcode |
< This identifies the message as MCPS_PURGE_CONFIRM More... | |
enum msg_code | mlme_associate_req_tag::cmdcode |
< This identifies the message as MLME_ASSOCIATE_REQUEST More... | |
enum msg_code | mlme_associate_ind_tag::cmdcode |
This identifies the message as MLME_ASSOCIATE_INDICATION. More... | |
enum msg_code | mlme_associate_resp_tag::cmdcode |
This identifies the message as MLME_ASSOCIATE_RESPONSE. More... | |
enum msg_code | mlme_associate_conf_tag::cmdcode |
This identifies the message as MLME_ASSOCIATE_CONFIRM. More... | |
enum msg_code | mlme_disassociate_req_tag::cmdcode |
This identifies the message as MLME_DISASSOCIATE_REQUEST. More... | |
enum msg_code | mlme_disassociate_ind_tag::cmdcode |
This identifies the message as MLME_DISASSOCIATE_INDICATION. More... | |
enum msg_code | mlme_disassociate_conf_tag::cmdcode |
This identifies the message as MLME_DISASSOCIATE_CONFIRM. More... | |
enum msg_code | mlme_beacon_notify_ind_tag::cmdcode |
This identifies the message as MLME_BEACON_NOTIFY_INDICATION. More... | |
enum msg_code | mlme_orphan_ind_tag::cmdcode |
This identifies the message as MLME_ORPHAN_INDICATION. More... | |
enum msg_code | mlme_orphan_resp_tag::cmdcode |
This identifies the message as MLME_ORPHAN_RESPONSE. More... | |
enum msg_code | mlme_reset_req_tag::cmdcode |
< This identifies the message as MLME_RESET_REQUEST More... | |
enum msg_code | mlme_reset_conf_tag::cmdcode |
< This identifies the message as MLME_RESET_CONFIRM More... | |
enum msg_code | mlme_get_req_tag::cmdcode |
< This identifies the message as MLME_GET_REQUEST More... | |
enum msg_code | mlme_get_conf_tag::cmdcode |
< This identifies the message as MLME_GET_CONFIRM More... | |
enum msg_code | mlme_set_req_tag::cmdcode |
< This identifies the message as MLME_SET_REQUEST More... | |
enum msg_code | mlme_set_conf_tag::cmdcode |
< This identifies the message as MLME_SET_CONFIRM More... | |
enum msg_code | mlme_rx_enable_req_tag::cmdcode |
This identifies the message as MLME_RX_ENABLE_REQUEST. More... | |
enum msg_code | mlme_rx_enable_conf_tag::cmdcode |
This identifies the message as MLME_RX_ENABLE_CONFIRM. More... | |
enum msg_code | mlme_scan_req_tag::cmdcode |
This identifies the message as MLME_SCAN_REQUEST. More... | |
enum msg_code | mlme_scan_conf_tag::cmdcode |
This identifies the message as MLME_SCAN_CONFIRM. More... | |
enum msg_code | mlme_comm_status_ind_tag::cmdcode |
This identifies the message as MLME_COMM_STATUS_INDICATION. More... | |
enum msg_code | mlme_start_req_tag::cmdcode |
This identifies the message as MLME_START_REQUEST. More... | |
enum msg_code | mlme_start_conf_tag::cmdcode |
This identifies the message as MLME_START_CONFIRM. More... | |
enum msg_code | mlme_sync_req_tag::cmdcode |
This identifies the message as MLME_SYNC_REQUEST. More... | |
enum msg_code | mlme_sync_loss_ind_tag::cmdcode |
This identifies the message as MLME_SYNC_LOSS_INDICATION. More... | |
enum msg_code | mlme_poll_req_tag::cmdcode |
This identifies the message as MLME_POLL_REQUEST. More... | |
enum msg_code | mlme_poll_conf_tag::cmdcode |
This identifies the message as MLME_POLL_CONFIRM. More... | |
address_field_t | mlme_associate_req_tag::CoordAddress |
The address of the coordinator with which to associate. More... | |
uint64_t | mlme_poll_req_tag::CoordAddress |
The address of the coordinator to which the poll is intended. More... | |
uint8_t | mlme_associate_req_tag::CoordAddrMode |
The coordinator addressing mode for this primitive and subsequent MPDU. More... | |
uint8_t | mlme_poll_req_tag::CoordAddrMode |
The addressing mode of the coordinator to which the poll is intended. More... | |
uint16_t | mlme_associate_req_tag::CoordPANId |
The identifier of the PAN with which to associate. More... | |
uint16_t | mlme_poll_req_tag::CoordPANId |
The PAN identifier of the coordinator to which the poll is intended. More... | |
uint8_t | mlme_start_req_tag::CoordRealignment |
TRUE if a coordinator realignment command is to be transmitted prior to changing the superframe configuration or FALSE otherwise. More... | |
uint8_t | mlme_rx_enable_req_tag::DeferPermit |
TRUE if the receiver enable can be deferred until during the next superframe if the requested time has already passed. More... | |
uint64_t | mlme_associate_ind_tag::DeviceAddress |
The address of the device requesting association. More... | |
uint64_t | mlme_associate_resp_tag::DeviceAddress |
The address of the device requesting association. More... | |
uint64_t | mlme_disassociate_req_tag::DeviceAddress |
The address of the device to which to send the disassociation notification command. More... | |
uint64_t | mlme_disassociate_ind_tag::DeviceAddress |
The address of the device requesting disassociation. More... | |
uint64_t | mlme_disassociate_conf_tag::DeviceAddress |
The address of the device that has either requested disassociation or been instructed to disassociate by its coordinator. More... | |
uint8_t | mlme_disassociate_req_tag::DeviceAddrMode |
The addressing mode of the device to which to send the disassociation notification command. More... | |
uint8_t | mlme_disassociate_conf_tag::DeviceAddrMode |
The addressing mode of the device that has either requested disassociation or been instructed to disassociate by its coordinator. More... | |
uint16_t | mlme_disassociate_req_tag::DevicePANId |
The PAN identifier of the device to which to send the disassociation notification command. More... | |
uint16_t | mlme_disassociate_conf_tag::DevicePANId |
The PAN identifier of the device that has either requested disassociation or been instructed to disassociate by its coordinator. More... | |
uint8_t | mlme_disassociate_req_tag::DisassociateReason |
The reason for the disassociation (see 7.3.1.3.2). More... | |
uint8_t | mlme_disassociate_ind_tag::DisassociateReason |
The reason for the disassociation (see 7.3.1.3.2). More... | |
uint8_t | mcps_data_ind_tag::DSN |
The DSN of the received data frame. More... | |
uint64_t | mcps_data_req_tag::DstAddr |
The individual device address of the entity to which the MSDU is being transferred. More... | |
uint64_t | mcps_data_ind_tag::DstAddr |
The individual device address of the entity to which the MSDU is being transferred. More... | |
uint64_t | mlme_comm_status_ind_tag::DstAddr |
The individual device address of the device for which the frame was intended. More... | |
uint8_t | mcps_data_req_tag::DstAddrMode |
The destination addressing mode for this primitive and subsequent MPDU. More... | |
uint8_t | mcps_data_ind_tag::DstAddrMode |
The destination addressing mode for this primitive corresponding to the received MPDU. More... | |
uint8_t | mlme_comm_status_ind_tag::DstAddrMode |
The destination addressing mode for this primitive. More... | |
uint16_t | mcps_data_req_tag::DstPANId |
The 16 bit PAN identifier of the entity to which the MSDU is being transferred. More... | |
uint16_t | mcps_data_ind_tag::DstPANId |
The 16 bit PAN identifier of the entity to which the MSDU is being transferred. More... | |
uint8_t | scan_result_list_t::ed_value [1] |
uint8_t | mlme_associate_req_tag::LogicalChannel |
The logical channel on which to attempt association. More... | |
uint8_t | mlme_start_req_tag::LogicalChannel |
The logical channel on which to start using the new superframe configuration. More... | |
uint8_t | mlme_sync_req_tag::LogicalChannel |
The logical channel on which to attempt coordinator synchronization. More... | |
uint8_t | mlme_sync_loss_ind_tag::LogicalChannel |
The logical channel on which the device lost synchronization or to which it was realigned. More... | |
uint8_t | mlme_sync_loss_ind_tag::LossReason |
The reason that synchronization was lost. More... | |
uint8_t | mcps_data_ind_tag::mpduLinkQuality |
LQI value measured during reception of the MPDU. More... | |
uint8_t * | mcps_data_req_tag::msdu |
The set of octets forming the MSDU to be transmitted by the MAC sublayer entity. More... | |
uint8_t * | mcps_data_ind_tag::msdu |
The set of octets forming the MSDU being indicated by the MAC sublayer entity. More... | |
uint8_t | mcps_data_req_tag::msduHandle |
The handle associated with the MSDU to be transmitted by the MAC sublayer entity. More... | |
uint8_t | mcps_data_conf_tag::msduHandle |
The handle associated with the MSDU being confirmed. More... | |
uint8_t | mcps_purge_req_tag::msduHandle |
The handle of the MSDU to be purged from the transaction queue. More... | |
uint8_t | mcps_purge_conf_tag::msduHandle |
The handle of the MSDU requested to be purge from the transaction queue. More... | |
uint8_t | mcps_data_req_tag::msduLength |
The number of octets contained in the MSDU to be transmitted by the MAC sublayer entity. More... | |
uint8_t | mcps_data_ind_tag::msduLength |
The number of octets contained in the MSDU being indicated by the MAC sublayer entity. More... | |
uint64_t | mlme_orphan_ind_tag::OrphanAddress |
The address of the orphaned device. More... | |
uint64_t | mlme_orphan_resp_tag::OrphanAddress |
The address of the orphaned device. More... | |
uint8_t | mlme_start_req_tag::PANCoordinator |
If this value is TRUE, the device will become the PAN coordinator of a new PAN. More... | |
wpan_pandescriptor_t | mlme_beacon_notify_ind_tag::PANDescriptor |
The PANDescriptor for the received beacon. More... | |
uint16_t | mlme_comm_status_ind_tag::PANId |
The 16 bit PAN identifier of the device from which the frame was received or to which the frame was being sent. More... | |
uint16_t | mlme_start_req_tag::PANId |
The PAN identifier to be used by the device. More... | |
uint16_t | mlme_sync_loss_ind_tag::PANId |
The PAN identifier with which the device lost synchronization or to which it was realigned. More... | |
uint8_t | mlme_beacon_notify_ind_tag::PendAddrSpec |
The beacon pending address specification. More... | |
uint8_t | mlme_get_req_tag::PIBAttribute |
uint8_t | mlme_get_conf_tag::PIBAttribute |
uint8_t | mlme_set_req_tag::PIBAttribute |
uint8_t | mlme_set_conf_tag::PIBAttribute |
pib_value_t | mlme_get_conf_tag::PIBAttributeValue |
< The value of the indicated MAC PIB attribute that was read. More... | |
pib_value_t | mlme_set_req_tag::PIBAttributeValue |
< The value to write to the indicated MAC PIB attribute. More... | |
uint8_t | mlme_scan_conf_tag::ResultListSize |
The number of elements returned in the appropriate result lists. More... | |
uint32_t | mlme_rx_enable_req_tag::RxOnDuration |
The number of symbols for which the receiver is to be enabled. More... | |
uint32_t | mlme_rx_enable_req_tag::RxOnTime |
The number of symbols from the start of the superframe before the receiver is to be enabled. More... | |
scan_result_list_t | mlme_scan_conf_tag::scan_result_list [1] |
ResultListSize - The number of elements returned in the appropriate result lists. More... | |
uint32_t | mlme_scan_req_tag::ScanChannels |
The 5 MSBs (b27, ... More... | |
uint8_t | mlme_scan_req_tag::ScanDuration |
A value used to calculate the length of time to spend scanning each channel for ED, active, and passive scans. More... | |
uint8_t | mlme_scan_req_tag::ScanType |
Indicates the type of scan performed: 0 x 00 = ED scan (FFD only). More... | |
uint8_t | mlme_scan_conf_tag::ScanType |
ScanType Integer 0 x 00 0 x 03 Indicates if the type of scan performed: 0 x 00 = ED scan (FFD only). More... | |
uint8_t * | mlme_beacon_notify_ind_tag::sdu |
The set of octets comprising the beacon payload to be transferred from the MAC sublayerentity to the next higher layer. More... | |
uint8_t | mlme_beacon_notify_ind_tag::sduLength |
The number of octets contained in the beacon payload of the beacon frame received by the MAC sublayer. More... | |
uint8_t | mlme_reset_req_tag::SetDefaultPIB |
If TRUE, the MAC sublayer is reset and all MAC PIB attributes are set to their default values. More... | |
uint16_t | mlme_orphan_resp_tag::ShortAddress |
The short address allocated to the orphaned device if it is associated with this coordinator. More... | |
uint64_t | mcps_data_ind_tag::SrcAddr |
The individual device address of the entity from which the MSDU was received. More... | |
uint64_t | mlme_comm_status_ind_tag::SrcAddr |
The source addressing mode for this primitive. More... | |
uint8_t | mcps_data_ind_tag::SrcAddrMode |
The source addressing mode for this primitive corresponding to the received MPDU. More... | |
uint8_t | mcps_data_req_tag::SrcAddrMode |
The source addressing mode for this primitive and subsequent MPDU. More... | |
uint8_t | mlme_comm_status_ind_tag::SrcAddrMode |
The source addressing mode for this primitive. More... | |
uint16_t | mcps_data_ind_tag::SrcPANId |
The 16 bit PAN identifier of the entity from which the MSDU was received. More... | |
uint8_t | mcps_data_conf_tag::status |
The status of the last MSDU transmission. More... | |
uint8_t | mcps_purge_conf_tag::status |
The status of the request to be purged an MSDU from the transaction queue. More... | |
uint8_t | mlme_associate_resp_tag::status |
The status of the association attempt. More... | |
uint8_t | mlme_associate_conf_tag::status |
The status of the association attempt. More... | |
uint8_t | mlme_disassociate_conf_tag::status |
The status of the disassociation attempt. More... | |
uint8_t | mlme_reset_conf_tag::status |
The result of the reset operation. More... | |
uint8_t | mlme_get_conf_tag::status |
The identifier of the MAC PIB attribute to get. More... | |
uint8_t | mlme_set_conf_tag::status |
The identifier of the MAC PIB attribute that was written. More... | |
uint8_t | mlme_rx_enable_conf_tag::status |
The result of the receiver enable request. More... | |
uint8_t | mlme_scan_conf_tag::status |
The status of the scan request. More... | |
uint8_t | mlme_comm_status_ind_tag::status |
The communications status. More... | |
uint8_t | mlme_start_conf_tag::status |
The result of the attempt to start using an updated superframe configuration. More... | |
uint8_t | mlme_poll_conf_tag::status |
The status of the data request. More... | |
uint8_t | mlme_start_req_tag::SuperframeOrder |
The length of the active portion of the superframe, including the beacon frame. More... | |
uint32_t | mcps_data_ind_tag::Timestamp |
Optional. More... | |
uint32_t | mcps_data_conf_tag::Timestamp |
Optional. More... | |
bool | mlme_sync_req_tag::TrackBeacon |
TRUE if the MLME is to synchronize with the next beacon and attempt to track all future beacons. More... | |
uint8_t | mlme_disassociate_req_tag::TxIndirect |
TRUE if the disassociation notification command is to be sent indirectly. More... | |
uint8_t | mcps_data_req_tag::TxOptions |
The transmission options for this MSDU. More... | |
uint32_t | mlme_scan_conf_tag::UnscannedChannels |
Indicates which channels given in the request were not scanned (1 = not scanned, 0 = scanned or not requested). More... | |
wpan_pandescriptor_t | scan_result_list_t::wpan_pan_desc |
typedef struct mcps_data_conf_tag mcps_data_conf_t |
This is the MCPS-DATA.confirm message structure.
typedef __PACK__DATA__ struct mcps_data_ind_tag mcps_data_ind_t |
This is the MCPS-DATA.indication message structure.
typedef struct mcps_data_req_tag mcps_data_req_t |
This is the MCPS-DATA.request message structure.
typedef struct mcps_purge_conf_tag mcps_purge_conf_t |
This is the MCPS-PURGE.confirm message structure.
typedef struct mcps_purge_req_tag mcps_purge_req_t |
This is the MCPS-PURGE.request message structure.
typedef struct mlme_associate_conf_tag mlme_associate_conf_t |
This is the MLME-ASSOCIATE.confirm message structure.
typedef struct mlme_associate_ind_tag mlme_associate_ind_t |
This is the MLME-ASSOCIATE.indication message structure.
typedef struct mlme_associate_req_tag mlme_associate_req_t |
This is the MLME-ASSOCIATE.request message structure.
typedef struct mlme_associate_resp_tag mlme_associate_resp_t |
This is the MLME-ASSOCIATE.response message structure.
typedef struct mlme_beacon_notify_ind_tag mlme_beacon_notify_ind_t |
This is the MLME-BEACON-NOTIFY.indication message structure.
typedef struct mlme_comm_status_ind_tag mlme_comm_status_ind_t |
This is the MLME-COMM-STATUS.indication message structure.
typedef struct mlme_disassociate_conf_tag mlme_disassociate_conf_t |
This is the MLME-DISASSOCIATE.confirm message structure.
typedef struct mlme_disassociate_ind_tag mlme_disassociate_ind_t |
This is the MLME-DISASSOCIATE.indication message structure.
typedef struct mlme_disassociate_req_tag mlme_disassociate_req_t |
This is the MLME-DISASSOCIATE.request message structure.
typedef struct mlme_get_conf_tag mlme_get_conf_t |
This is the MLME-GET.confirm message structure.
typedef struct mlme_get_req_tag mlme_get_req_t |
This is the MLME-GET.request message structure.
typedef struct mlme_orphan_ind_tag mlme_orphan_ind_t |
This is the MLME-ORPHAN.indication message structure.
typedef struct mlme_orphan_resp_tag mlme_orphan_resp_t |
This is the MLME-ORPHAN.response message structure.
typedef struct mlme_poll_conf_tag mlme_poll_conf_t |
This is the MLME-POLL.confirm message structure.
typedef struct mlme_poll_req_tag mlme_poll_req_t |
This is the MLME-POLL.request message structure.
typedef struct mlme_reset_conf_tag mlme_reset_conf_t |
This is the MLME-RESET.confirm message structure.
typedef struct mlme_reset_req_tag mlme_reset_req_t |
This is the MLME-RESET.request message structure.
typedef struct mlme_rx_enable_conf_tag mlme_rx_enable_conf_t |
This is the MLME-RX-ENABLE.confirm message structure.
typedef struct mlme_rx_enable_req_tag mlme_rx_enable_req_t |
This is the MLME-RX-ENABLE.request message structure.
typedef struct mlme_scan_conf_tag mlme_scan_conf_t |
This is the MLME-SCAN.confirm message structure.
typedef struct mlme_scan_req_tag mlme_scan_req_t |
This is the MLME-SCAN.request message structure.
typedef struct mlme_set_conf_tag mlme_set_conf_t |
This is the MLME-SET.confirm message structure.
typedef struct mlme_set_req_tag mlme_set_req_t |
This is the MLME-SET.request message structure.
typedef struct mlme_start_conf_tag mlme_start_conf_t |
This is the MLME-START.confirm message structure.
typedef struct mlme_start_req_tag mlme_start_req_t |
This is the MLME-START.request message structure.
typedef struct mlme_sync_loss_ind_tag mlme_sync_loss_ind_t |
This is the MLME-SYNC-LOSS.indication message structure.
typedef struct mlme_sync_req_tag mlme_sync_req_t |
This is the MLME-SYNC.request message structure.
typedef struct wpan_addr_spec_tag wpan_addr_spec_t |
Device address specification structure.
typedef struct wpan_pandescriptor_tag wpan_pandescriptor_t |
PAN descriptor information structure.
uint8_t mac_get_pib_attribute_size | ( | uint8_t | pib_attribute_id | ) |
References macBeaconPayload, MAX_MAC_PIB_ATTRIBUTE_ID, MAX_PHY_PIB_ATTRIBUTE_ID, MIN_MAC_PIB_ATTRIBUTE_ID, MIN_PRIVATE_PIB_ATTRIBUTE_ID, PGM_READ_BYTE, and rcv_frame_ptr.
Referenced by wpan_mlme_set_req().
uint8_t* mlme_beacon_notify_ind_tag::AddrList |
The list of addresses of the devices for which the beacon source has data.
uint8_t mlme_orphan_resp_tag::AssociatedMember |
TRUE if the orphaned device is associated with this coordinator or FALSE otherwise.
uint16_t mlme_associate_resp_tag::AssocShortAddress |
The short device address allocated by the coordinator on successful association.
This parameter is set to 0xffff if the association was unsuccessful.
uint16_t mlme_associate_conf_tag::AssocShortAddress |
The short device address allocated by the coordinator on successful association.
This parameter will be equal to 0 x ffff if the association attempt was unsuccessful.
uint8_t mlme_start_req_tag::BatteryLifeExtension |
If this value is TRUE, the receiver of the beaconing device is disabled macBattLifeExtPeriods full backoff periods after the interframe spacing (IFS) period of the beacon frame.
If this value is FALSE, the receiver of the beaconing device remains enabled for the entire CAP.
uint8_t mlme_start_req_tag::BeaconOrder |
How often the beacon is to be transmitted.
The beacon order, BO, and the beacon interval, BI, are related as follows: for 0 d BO d 14, BI = BaseSuperframeDuration * 2^BO symbols. If BO = 15, the coordinator will not transmit a beacon, and the SuperframeOrder parameter value is ignored.
uint8_t mlme_beacon_notify_ind_tag::BSN |
The beacon sequence number.
uint8_t mlme_associate_req_tag::CapabilityInformation |
Specifies the operational capabilities of the associating device.
uint8_t mlme_associate_ind_tag::CapabilityInformation |
The operational capabilities of the device requesting association.
uint8_t mlme_associate_req_tag::ChannelPage |
The channel page on which to attempt association.
uint8_t mlme_scan_req_tag::ChannelPage |
The channel page on which to perform the scan.
uint8_t mlme_scan_conf_tag::ChannelPage |
The channel page on which the scan was performed.
uint8_t mlme_start_req_tag::ChannelPage |
The channel page on which to begin using the new superframe configuration.
uint8_t mlme_sync_req_tag::ChannelPage |
The channel page on which to attempt coordinator synchronization.
uint8_t mlme_sync_loss_ind_tag::ChannelPage |
The channel page on which the device lost synchronization or to which it was realigned.
enum msg_code mcps_data_req_tag::cmdcode |
< This identifies the message as MCPS_DATA_REQUEST
enum msg_code mcps_data_conf_tag::cmdcode |
< This identifies the message as MCPS_DATA_CONFIRM
enum msg_code mcps_data_ind_tag::cmdcode |
< This identifies the message as MCPS_DATA_INDICATION
enum msg_code mcps_purge_req_tag::cmdcode |
< This identifies the message as MCPS_PURGE_REQUEST
enum msg_code mcps_purge_conf_tag::cmdcode |
< This identifies the message as MCPS_PURGE_CONFIRM
enum msg_code mlme_associate_req_tag::cmdcode |
< This identifies the message as MLME_ASSOCIATE_REQUEST
enum msg_code mlme_associate_ind_tag::cmdcode |
This identifies the message as MLME_ASSOCIATE_INDICATION.
enum msg_code mlme_associate_resp_tag::cmdcode |
This identifies the message as MLME_ASSOCIATE_RESPONSE.
enum msg_code mlme_associate_conf_tag::cmdcode |
This identifies the message as MLME_ASSOCIATE_CONFIRM.
enum msg_code mlme_disassociate_req_tag::cmdcode |
This identifies the message as MLME_DISASSOCIATE_REQUEST.
enum msg_code mlme_disassociate_ind_tag::cmdcode |
This identifies the message as MLME_DISASSOCIATE_INDICATION.
enum msg_code mlme_disassociate_conf_tag::cmdcode |
This identifies the message as MLME_DISASSOCIATE_CONFIRM.
enum msg_code mlme_beacon_notify_ind_tag::cmdcode |
This identifies the message as MLME_BEACON_NOTIFY_INDICATION.
enum msg_code mlme_orphan_ind_tag::cmdcode |
This identifies the message as MLME_ORPHAN_INDICATION.
enum msg_code mlme_orphan_resp_tag::cmdcode |
This identifies the message as MLME_ORPHAN_RESPONSE.
enum msg_code mlme_reset_req_tag::cmdcode |
< This identifies the message as MLME_RESET_REQUEST
enum msg_code mlme_reset_conf_tag::cmdcode |
< This identifies the message as MLME_RESET_CONFIRM
enum msg_code mlme_get_req_tag::cmdcode |
< This identifies the message as MLME_GET_REQUEST
The identifier of the MAC PIB attribute to get.
enum msg_code mlme_get_conf_tag::cmdcode |
< This identifies the message as MLME_GET_CONFIRM
The result of the request for PHY PIB attribute information.
enum msg_code mlme_set_req_tag::cmdcode |
< This identifies the message as MLME_SET_REQUEST
The identifier of the MAC PIB attribute to set.
enum msg_code mlme_set_conf_tag::cmdcode |
< This identifies the message as MLME_SET_CONFIRM
The result of the request to write the MAC PIB attribute.
enum msg_code mlme_rx_enable_req_tag::cmdcode |
This identifies the message as MLME_RX_ENABLE_REQUEST.
enum msg_code mlme_rx_enable_conf_tag::cmdcode |
This identifies the message as MLME_RX_ENABLE_CONFIRM.
enum msg_code mlme_scan_req_tag::cmdcode |
This identifies the message as MLME_SCAN_REQUEST.
enum msg_code mlme_scan_conf_tag::cmdcode |
This identifies the message as MLME_SCAN_CONFIRM.
enum msg_code mlme_comm_status_ind_tag::cmdcode |
This identifies the message as MLME_COMM_STATUS_INDICATION.
enum msg_code mlme_start_req_tag::cmdcode |
This identifies the message as MLME_START_REQUEST.
enum msg_code mlme_start_conf_tag::cmdcode |
This identifies the message as MLME_START_CONFIRM.
enum msg_code mlme_sync_req_tag::cmdcode |
This identifies the message as MLME_SYNC_REQUEST.
enum msg_code mlme_sync_loss_ind_tag::cmdcode |
This identifies the message as MLME_SYNC_LOSS_INDICATION.
enum msg_code mlme_poll_req_tag::cmdcode |
This identifies the message as MLME_POLL_REQUEST.
enum msg_code mlme_poll_conf_tag::cmdcode |
This identifies the message as MLME_POLL_CONFIRM.
address_field_t mlme_associate_req_tag::CoordAddress |
The address of the coordinator with which to associate.
uint64_t mlme_poll_req_tag::CoordAddress |
The address of the coordinator to which the poll is intended.
The address of the coordinator to which the poll is intended.
uint8_t mlme_associate_req_tag::CoordAddrMode |
The coordinator addressing mode for this primitive and subsequent MPDU.
This value can take one of the following values: 2 = 16 bit short address. 3 = 64 bit extended address.
uint8_t mlme_poll_req_tag::CoordAddrMode |
The addressing mode of the coordinator to which the poll is intended.
This parameter can take one of the following values: 2 = 16 bit short address, 3 = 64 bit extended address.
uint16_t mlme_associate_req_tag::CoordPANId |
The identifier of the PAN with which to associate.
uint16_t mlme_poll_req_tag::CoordPANId |
The PAN identifier of the coordinator to which the poll is intended.
uint8_t mlme_start_req_tag::CoordRealignment |
TRUE if a coordinator realignment command is to be transmitted prior to changing the superframe configuration or FALSE otherwise.
uint8_t mlme_rx_enable_req_tag::DeferPermit |
TRUE if the receiver enable can be deferred until during the next superframe if the requested time has already passed.
FALSE if the receiver enable is only to be attempted in the current superframe. This parameter is ignored for nonbeacon-enabled PANs.
uint64_t mlme_associate_ind_tag::DeviceAddress |
The address of the device requesting association.
uint64_t mlme_associate_resp_tag::DeviceAddress |
The address of the device requesting association.
uint64_t mlme_disassociate_req_tag::DeviceAddress |
The address of the device to which to send the disassociation notification command.
uint64_t mlme_disassociate_ind_tag::DeviceAddress |
The address of the device requesting disassociation.
uint64_t mlme_disassociate_conf_tag::DeviceAddress |
The address of the device that has either requested disassociation or been instructed to disassociate by its coordinator.
uint8_t mlme_disassociate_req_tag::DeviceAddrMode |
The addressing mode of the device to which to send the disassociation notification command.
uint8_t mlme_disassociate_conf_tag::DeviceAddrMode |
The addressing mode of the device that has either requested disassociation or been instructed to disassociate by its coordinator.
uint16_t mlme_disassociate_req_tag::DevicePANId |
The PAN identifier of the device to which to send the disassociation notification command.
uint16_t mlme_disassociate_conf_tag::DevicePANId |
The PAN identifier of the device that has either requested disassociation or been instructed to disassociate by its coordinator.
uint8_t mlme_disassociate_req_tag::DisassociateReason |
The reason for the disassociation (see 7.3.1.3.2).
uint8_t mlme_disassociate_ind_tag::DisassociateReason |
The reason for the disassociation (see 7.3.1.3.2).
uint8_t mcps_data_ind_tag::DSN |
The DSN of the received data frame.
uint64_t mcps_data_req_tag::DstAddr |
The individual device address of the entity to which the MSDU is being transferred.
uint64_t mcps_data_ind_tag::DstAddr |
The individual device address of the entity to which the MSDU is being transferred.
uint64_t mlme_comm_status_ind_tag::DstAddr |
The individual device address of the device for which the frame was intended.
uint8_t mcps_data_req_tag::DstAddrMode |
The destination addressing mode for this primitive and subsequent MPDU.
This value can take one of the following values: 0 x 00 = no address (addressing fields omitted). 0 x 01 = reserved. 0 x 02 = 16 bit short address. 0 x 03 = 64 bit extended address.
uint8_t mcps_data_ind_tag::DstAddrMode |
The destination addressing mode for this primitive corresponding to the received MPDU.
This value can take one of the following values: 0 x 00 = no address (addressing fields omitted). 0 x 01 = reserved. 0 x 02 = 16 bit short device address. 0 x 03 = 64 bit extended device address.
uint8_t mlme_comm_status_ind_tag::DstAddrMode |
The destination addressing mode for this primitive.
This value can take one of the following values: 0 x 00 = no address (addressing fields omitted). 0 x 01 = reserved. 0 x 02 = 16 bit short address. 0 x 03 = 64 bit extended address.
uint16_t mcps_data_req_tag::DstPANId |
The 16 bit PAN identifier of the entity to which the MSDU is being transferred.
uint16_t mcps_data_ind_tag::DstPANId |
The 16 bit PAN identifier of the entity to which the MSDU is being transferred.
uint8_t scan_result_list_t::ed_value[1] |
uint8_t mlme_associate_req_tag::LogicalChannel |
The logical channel on which to attempt association.
uint8_t mlme_start_req_tag::LogicalChannel |
The logical channel on which to start using the new superframe configuration.
uint8_t mlme_sync_req_tag::LogicalChannel |
The logical channel on which to attempt coordinator synchronization.
uint8_t mlme_sync_loss_ind_tag::LogicalChannel |
The logical channel on which the device lost synchronization or to which it was realigned.
uint8_t mlme_sync_loss_ind_tag::LossReason |
The reason that synchronization was lost.
uint8_t mcps_data_ind_tag::mpduLinkQuality |
LQI value measured during reception of the MPDU.
Lower values represent lower LQI (see 6.7.8).
uint8_t* mcps_data_req_tag::msdu |
The set of octets forming the MSDU to be transmitted by the MAC sublayer entity.
uint8_t* mcps_data_ind_tag::msdu |
The set of octets forming the MSDU being indicated by the MAC sublayer entity.
uint8_t mcps_data_req_tag::msduHandle |
The handle associated with the MSDU to be transmitted by the MAC sublayer entity.
uint8_t mcps_data_conf_tag::msduHandle |
The handle associated with the MSDU being confirmed.
uint8_t mcps_purge_req_tag::msduHandle |
The handle of the MSDU to be purged from the transaction queue.
uint8_t mcps_purge_conf_tag::msduHandle |
The handle of the MSDU requested to be purge from the transaction queue.
uint8_t mcps_data_req_tag::msduLength |
The number of octets contained in the MSDU to be transmitted by the MAC sublayer entity.
uint8_t mcps_data_ind_tag::msduLength |
The number of octets contained in the MSDU being indicated by the MAC sublayer entity.
uint64_t mlme_orphan_ind_tag::OrphanAddress |
The address of the orphaned device.
uint64_t mlme_orphan_resp_tag::OrphanAddress |
The address of the orphaned device.
uint8_t mlme_start_req_tag::PANCoordinator |
If this value is TRUE, the device will become the PAN coordinator of a new PAN.
If this value is FALSE, the device will begin transmitting beacons on the PAN with which it is associated.
wpan_pandescriptor_t mlme_beacon_notify_ind_tag::PANDescriptor |
The PANDescriptor for the received beacon.
uint16_t mlme_comm_status_ind_tag::PANId |
The 16 bit PAN identifier of the device from which the frame was received or to which the frame was being sent.
uint16_t mlme_start_req_tag::PANId |
The PAN identifier to be used by the device.
uint16_t mlme_sync_loss_ind_tag::PANId |
The PAN identifier with which the device lost synchronization or to which it was realigned.
uint8_t mlme_beacon_notify_ind_tag::PendAddrSpec |
The beacon pending address specification.
uint8_t mlme_get_req_tag::PIBAttribute |
uint8_t mlme_get_conf_tag::PIBAttribute |
uint8_t mlme_set_req_tag::PIBAttribute |
uint8_t mlme_set_conf_tag::PIBAttribute |
pib_value_t mlme_get_conf_tag::PIBAttributeValue |
< The value of the indicated MAC PIB attribute that was read.
pib_value_t mlme_set_req_tag::PIBAttributeValue |
< The value to write to the indicated MAC PIB attribute.
uint8_t mlme_scan_conf_tag::ResultListSize |
The number of elements returned in the appropriate result lists.
This value is 0 for the result of an orphan scan.
uint32_t mlme_rx_enable_req_tag::RxOnDuration |
The number of symbols for which the receiver is to be enabled.
uint32_t mlme_rx_enable_req_tag::RxOnTime |
The number of symbols from the start of the superframe before the receiver is to be enabled.
The precision of this value is a minimum of 20 bits, with the lowest 4 bits being the least significant. This parameter is ignored for nonbeacon-enabled PANs.
scan_result_list_t mlme_scan_conf_tag::scan_result_list[1] |
ResultListSize - The number of elements returned in the appropriate result lists.
This value is 0 for the result of an orphan scan. EnergyDetectList - The number of elements returned in the appropriate result lists. This value is 0 for the result of an orphan scan. PANDescriptorList - The list of PAN descriptors, one for each beacon found during an active or passive scan. This parameter is null for ED and orphan scans.
uint32_t mlme_scan_req_tag::ScanChannels |
The 5 MSBs (b27, ...
, b31) are reserved. The 27 LSBs (b0, b1, ... b26) indicate which channels are to be scanned (1 = scan, 0 = do not scan) for each of the 27 valid channels (see 6.1.2).
uint8_t mlme_scan_req_tag::ScanDuration |
A value used to calculate the length of time to spend scanning each channel for ED, active, and passive scans.
This parameter is ignored for orphan scans. The time spent scanning each channel is [aBaseSuperframeDuration * (2n + 1)] symbols, where n is the value of the ScanDuration parameter.
uint8_t mlme_scan_req_tag::ScanType |
Indicates the type of scan performed: 0 x 00 = ED scan (FFD only).
0 x 01 = active scan (FFD only). 0 x 02 = passive scan. 0 x 03 = orphan scan.
uint8_t mlme_scan_conf_tag::ScanType |
ScanType Integer 0 x 00 0 x 03 Indicates if the type of scan performed: 0 x 00 = ED scan (FFD only).
0 x 01 = active scan (FFD only). 0 x 02 = passive scan. 0 x 03 = orphan scan.
uint8_t* mlme_beacon_notify_ind_tag::sdu |
The set of octets comprising the beacon payload to be transferred from the MAC sublayerentity to the next higher layer.
uint8_t mlme_beacon_notify_ind_tag::sduLength |
The number of octets contained in the beacon payload of the beacon frame received by the MAC sublayer.
uint8_t mlme_reset_req_tag::SetDefaultPIB |
If TRUE, the MAC sublayer is reset and all MAC PIB attributes are set to their default values.
If FALSE, the MAC sublayer is reset but all MAC PIB attributes retain their values prior to the generation of the MLME-RESET.request primitive.
uint16_t mlme_orphan_resp_tag::ShortAddress |
The short address allocated to the orphaned device if it is associated with this coordinator.
The special short address 0 x fffe indicates that no short address was allocated, and the device will use its 64 bit extended address in all communications. If the device was not associated with thiscoordinator, this field will contain the value 0 x ffff and be ignored on receipt.
uint64_t mcps_data_ind_tag::SrcAddr |
The individual device address of the entity from which the MSDU was received.
uint64_t mlme_comm_status_ind_tag::SrcAddr |
The source addressing mode for this primitive.
This value can take one of the following values: 0 = no address (addressing fields omitted). 0 x 01 = reserved. 0 x 02 = 16 bit short address. 0 x 03 = 64 bit extended address.
uint8_t mcps_data_ind_tag::SrcAddrMode |
The source addressing mode for this primitive corresponding to the received MPDU.
This value can take one of the following values: 0 x 00 = no address (addressing fields omitted). 0 x 01 = reserved. 0 x 02 = 16 bit short address. 0 x 03 = 64 bit extended address.
uint8_t mcps_data_req_tag::SrcAddrMode |
The source addressing mode for this primitive and subsequent MPDU.
This value can take one of the following values: 0 x 00 = no address (addressingfields omitted). 0 x 01 = reserved. 0 x 02 = 16 bit short address. 0 x 03 = 64 bit extended address.
uint8_t mlme_comm_status_ind_tag::SrcAddrMode |
The source addressing mode for this primitive.
This value can take one of the following values: 0 = no address (addressing fields omitted). 0 x 01 = reserved. 0 x 02 = 16 bit short address. 0 x 03 = 64 bit extended address.
uint16_t mcps_data_ind_tag::SrcPANId |
The 16 bit PAN identifier of the entity from which the MSDU was received.
uint8_t mcps_data_conf_tag::status |
The status of the last MSDU transmission.
uint8_t mcps_purge_conf_tag::status |
The status of the request to be purged an MSDU from the transaction queue.
uint8_t mlme_associate_resp_tag::status |
The status of the association attempt.
uint8_t mlme_associate_conf_tag::status |
The status of the association attempt.
uint8_t mlme_disassociate_conf_tag::status |
The status of the disassociation attempt.
uint8_t mlme_reset_conf_tag::status |
The result of the reset operation.
uint8_t mlme_get_conf_tag::status |
The identifier of the MAC PIB attribute to get.
uint8_t mlme_set_conf_tag::status |
The identifier of the MAC PIB attribute that was written.
uint8_t mlme_rx_enable_conf_tag::status |
The result of the receiver enable request.
uint8_t mlme_scan_conf_tag::status |
The status of the scan request.
uint8_t mlme_comm_status_ind_tag::status |
The communications status.
uint8_t mlme_start_conf_tag::status |
The result of the attempt to start using an updated superframe configuration.
uint8_t mlme_poll_conf_tag::status |
The status of the data request.
uint8_t mlme_start_req_tag::SuperframeOrder |
The length of the active portion of the superframe, including the beacon frame.
The superframe order, SO, and the superframe duration, SD, are related as follows: for 0 d SO d BO d 14, SD = aBaseSuperframeDuration * 2^SO symbols. If SO = 15, the superframe will not be active after the beacon.
uint32_t mcps_data_ind_tag::Timestamp |
Optional.
The time, in symbols, at which the data were received (see 7.5.4.1). The symbol boundary is described by macSyncSymbolOffset (see Table 86 in 7.4.1). This is a 24-bit value, and the precision of this value shall be a minimum of 20 bits, with the lowest 4 bits being the least significant.
uint32_t mcps_data_conf_tag::Timestamp |
Optional.
The time, in symbols, at which the data were transmitted (see 7.5.4.1). The value of this parameter will be considered valid only if the value of the status parameter is MAC_SUCCESS; if the status parameter is not equal to MAC_SUCCESS, the value of the Timestamp parameter shall not be used for any other purpose. The symbol boundary is described by macSyncSymbolOffset (see Table 86 in 7.4.1). This is a 24-bit value, and the precision of this value shall be a minimum of 20 bits, with the lowest 4 bits being the least significant.
bool mlme_sync_req_tag::TrackBeacon |
TRUE if the MLME is to synchronize with the next beacon and attempt to track all future beacons.
FALSE if the MLME is to synchronize with only the next beacon.
uint8_t mlme_disassociate_req_tag::TxIndirect |
TRUE if the disassociation notification command is to be sent indirectly.
uint8_t mcps_data_req_tag::TxOptions |
The transmission options for this MSDU.
These are a bitwise OR of one or more of the following: 0 x 01 = acknowledged transmission. 0 x 04 = indirect transmission.
uint32_t mlme_scan_conf_tag::UnscannedChannels |
Indicates which channels given in the request were not scanned (1 = not scanned, 0 = scanned or not requested).
This parameter is only valid for passive or active scans.
wpan_pandescriptor_t scan_result_list_t::wpan_pan_desc |