![]() | See Quickstart guide for SAM FLASHCALW driver |
![]() | Receiver Transmitter (USART) |
![]() | Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices |
![]() ![]() | Common standard serial I/O management driver that implements a stdio serial interface on AVR and SAM devices |
![]() | This module is responsible for encoding and decoding the serial bytes to/from NCP into MAC APIs to provide seamless working for application similar to stack running in same processor or on NCP.This module is used for Two Processor Approach |
![]() ![]() | The API Encoder Module Decodes the incoming command byte stream to corresponding MAC Api's |
![]() ![]() | The API Encoder Module Encodes the MAC Api's into appropriate command byte stream |
![]() | All General Definitions used by the Wireless Stack applications are defined in this module |
![]() ![]() | Includes IEEE Constant Definitions |
![]() ![]() | All Build configurations Macros are defined in this module |
![]() ![]() | All return Value Enumerations are defined in this module |
![]() ![]() | Includes Stack Definitions |
![]() | The IEEE standard 802.15.4 MAC Layer defines the protocol and compatible interconnection for data communication devices using low data rate, low power and low complexity, short-range radio frequency (RF) transmissions in a wireless personal area network (WPAN) |
![]() ![]() | All Build configurations Macros are defined in this module |
![]() ![]() | This module defines all the MAC Data Structures |
![]() ![]() ![]() | All Definitions used by the MAC Layer is described here |
![]() ![]() | All Definitions used by the MAC Layer is described here |
![]() ![]() | All MAC Prototypes are described in this module |
![]() ![]() ![]() | This module describes all Mac Core Layer(MCL) API's |
![]() ![]() ![]() ![]() | This module describes all MCL Request API's |
![]() ![]() ![]() ![]() | This module describes all MCL General API's |
![]() ![]() ![]() ![]() | This module describes all MCL Confirmation API's |
![]() ![]() ![]() ![]() | This module describes all MCL Indication API's |
![]() ![]() ![]() ![]() | This module describes all MCL Response API's |
![]() ![]() ![]() | This module describes all MAC Callback's |
![]() ![]() ![]() ![]() | This module describes all MAC Confirmation Callback's |
![]() ![]() ![]() ![]() | This module describes all MAC Indication Callback's |
![]() | Implements the software Algorithm for Timer Handling in the Stack |
![]() ![]() | Implements a common api interface for accessing timer drivers of all architectures |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Timer Counter functionality |
![]() | |
![]() ![]() | A Digital Frequency Locked Loop can be used to generate a highly accurate frequency from a slower-running reference clock, in much the same way as a PLL |
![]() ![]() | Generic clocks are configurable clocks which run outside the system clock domain |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs |
![]() ![]() | See Quick Start Guide for the System Clock Management service (SAM4L) |
![]() ![]() ![]() | |
![]() | Compiler abstraction layer and code utilities for AT91SAM |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | This is a driver for global enabling and disabling of interrupts |
![]() ![]() | |
![]() | This collection of macros identify which series and families that the various Atmel parts belong to |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | Driver for the BPM (Backup Power Manager) |
![]() | This module performs serial input/output functionalities via UART from and to the HOST |
![]() | See Quick start guide for Serial Interface service |
![]() | Transmitter (USART) |
![]() | This module performs serial input/output functionalities via UART |
![]() | This module provides simple loop-based delay routines for those applications requiring a brief wait during execution |
![]() | See Quick start guide for the common IOPORT service |
![]() | Driver for the WDT (Watchdog Timer) |
![]() | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
![]() ![]() | |
![]() ![]() ![]() | Symbols to use for configuring the board and its initialization |
![]() ![]() ![]() | Symbols that describe features and capabilities of the board |