The MAC Core Layer (MCL) abstracts and implements IEEE 802.15.4-2006 compliant behavior for non-beacon enabled and beacon-enabled network support.
Macros | |
#define | MAKE_MAC_BUSY() |
This macro sets the MAC to busy. More... | |
#define | MAKE_MAC_NOT_BUSY() |
This macro sets the MAC to not busy. More... | |
Functions | |
void | dispatch_event (uint8_t *event) |
Obtains the message type from the buffer and calls the respective handler. More... | |
void | mac_build_and_tx_beacon (bool beacon_enabled, buffer_t *beacon_buffer_header) |
Builds and transmits the beacon frame. More... | |
bool | mac_build_and_tx_data_req (bool expl_poll, bool force_own_long_addr, uint8_t expl_dest_addr_mode, address_field_t *expl_dest_addr, uint16_t expl_dest_pan_id) |
Build and transmits data request command frame. More... | |
static void | mac_check_persistence_timer (void) |
void | mac_coord_realignment_command_tx_success (uint8_t tx_status, buffer_t *buf_ptr) |
Continues handling of MLME_START.request (Coordinator realignment) command. More... | |
void | mac_gen_mcps_data_conf (buffer_t *buf_ptr, uint8_t status, uint8_t handle, uint32_t timestamp) |
void | mac_gen_mlme_associate_conf (buffer_t *buf_ptr, uint8_t status, uint16_t assoc_short_addr) |
void | mac_handle_tx_null_data_frame (void) |
void | mac_idle_trans (void) |
Resets the MAC helper variables and transition to idle state. More... | |
void | mac_mlme_comm_status (uint8_t status, buffer_t *buf_ptr) |
Creates a Communication Status Indication message to the upper layer. More... | |
void | mac_prep_disassoc_conf (buffer_t *buf_ptr, uint8_t status) |
Prepares a disassociation confirm message with device address information. More... | |
void | mac_process_associate_request (buffer_t *buf_ptr) |
Processes a received association request command frame. More... | |
void | mac_process_associate_response (buffer_t *buf_ptr) |
Processing of an associaton reponse command frame. More... | |
void | mac_process_beacon_frame (buffer_t *msg) |
Processes received beacon frame. More... | |
void | mac_process_beacon_request (buffer_t *buf_ptr) |
Processes a beacon request. More... | |
void | mac_process_coord_realign (buffer_t *buf_ptr) |
Processing a coordinator realignment command frame. More... | |
void | mac_process_data_frame (buffer_t *buf_ptr) |
Processes data frames. More... | |
void | mac_process_data_request (buffer_t *buf_ptr) |
Processes a received data request command frame. More... | |
void | mac_process_data_response (void) |
Processes a data response to an MLME-POLL.request. More... | |
void | mac_process_disassociate_notification (buffer_t *buf_ptr) |
Process a disassociation notification command. More... | |
void | mac_process_orphan_notification (buffer_t *buf_ptr) |
Handles an orphan notification. More... | |
void | mac_process_orphan_realign (buffer_t *buf_ptr) |
Processing a coordinator realignment command frame during Orphan scan. More... | |
void | mac_process_tal_data_ind (uint8_t *msg) |
Depending on received frame the appropriate function is called. More... | |
void | mac_scan_send_complete (retval_t status) |
Continue scanning after the completion of frame transmission. More... | |
void | mac_sleep_trans (void) |
Puts the radio to sleep if this is allowed. More... | |
void | mac_start_persistence_timer (void) |
void | mac_sync_loss (uint8_t loss_reason) |
Function to initiate MLME-SYNC-LOSS.indication to NHLE. More... | |
void | mac_t_assocresponsetime_cb (void *callback_parameter) |
void | mac_t_poll_wait_time_cb (void *callback_parameter) |
T_Poll_Wait_Time timer callback. More... | |
void | mac_t_response_wait_cb (void *callback_parameter) |
Handle T_Poll_Wait_Time timer after successful transmission of an association request frame and before sending out the subsequent data request frame. More... | |
void | mac_trx_init_sleep (void) |
MAC function to put the radio to sleep mode. More... | |
void | mac_trx_wakeup (void) |
MAC function to wake-up the radio from sleep state. More... | |
bool | mac_tx_coord_realignment_command (frame_msgtype_t cmd_type, buffer_t *buf_ptr, uint16_t new_panid, uint8_t new_channel, uint8_t new_page) |
Sends a coordinator realignment command frame. More... | |
retval_t | set_tal_pib_internal (uint8_t attribute, pib_value_t *attribute_value) |
Wakes-up the radio and sets the corresponding TAL PIB attribute. More... | |
#define MAKE_MAC_BUSY | ( | ) |
This macro sets the MAC to busy.
Referenced by mac_awake_disassociate(), mac_build_and_tx_beacon(), mac_build_and_tx_data_req(), mac_handle_tx_null_data_frame(), mac_process_data_request(), mac_process_tal_tx_status(), mac_tx_coord_realignment_command(), mcps_data_request(), mlme_associate_request(), scan_set_complete(), send_scan_cmd(), and tx_pan_id_conf_notif().
#define MAKE_MAC_NOT_BUSY | ( | ) |
This macro sets the MAC to not busy.
Referenced by mac_process_data_response(), mac_t_poll_wait_time_cb(), tal_ed_end_cb(), and tal_tx_frame_done_cb().
void dispatch_event | ( | uint8_t * | event | ) |
Obtains the message type from the buffer and calls the respective handler.
This function decodes all events/messages and calls the appropriate handler.
event | Pointer to the buffer header whose body part holds the message type and message elemnets |
References Assert, bmm_buffer_free(), BMM_BUFFER_POINTER, CMD_ID_OCTET, LAST_MESSAGE, and PGM_READ_WORD.
Referenced by mac_task(), and wpan_task().
void mac_build_and_tx_beacon | ( | bool | beacon_enabled, |
buffer_t * | beacon_buffer_header | ||
) |
Builds and transmits the beacon frame.
This function is called to build a beacon frame. For beaconless network this function also transmits the generated beacon frame.
beacon_enabled | Flag indicating the mode of beacon transmission |
beacon_buffer_header | For build without beacon support only: Pointer to buffer of beacon frame to be transmitted in nonbeacon network. |
References ASSOC_PERMIT_BIT_POS, BATT_LIFE_EXT_BIT_POS, BEACON_MESSAGE, BEACON_PAYLOAD_LEN, BMM_BUFFER_POINTER, frame_info_tag::buffer_header, CCPU_ENDIAN_TO_LE16, convert_16_bit_to_byte_array, convert_64_bit_to_byte_array, convert_spec_16_bit_to_byte_array, CSMA_UNSLOTTED, mcps_data_req_tag::DstPANId, FCF_FRAME_PENDING, FCF_FRAME_VERSION_2006, FCF_FRAMETYPE_BEACON, FCF_LONG_ADDR, FCF_SECURITY_ENABLED, FCF_SET_FRAMETYPE, FCF_SET_SOURCE_ADDR_MODE, FCF_SHORT_ADDR, FINAL_CAP_SLOT_DEFAULT, indirect_data_q, LARGE_BUFFER_SIZE, mac_pib_tag::mac_AssociationPermit, mac_beacon_payload, mac_pib_tag::mac_BeaconPayloadLength, mac_pib_tag::mac_BSN, mac_buffer_add_pending(), MAC_COORDINATOR, MAC_NO_SHORT_ADDR_VALUE, MAC_PAN_COORD_STARTED, mac_pib, mac_state, MAC_SUCCESS, MAKE_MAC_BUSY, frame_info_tag::mpdu, mcps_data_req_tag::msduLength, frame_info_tag::msg_type, NON_BEACON_NWK, PAN_COORD_BIT_POS, mac_pib_tag::privateVirtualPANs, queue_tag::size, mcps_data_req_tag::SrcAddrMode, tal_pib, tal_tx_frame(), and vpan_no.
Referenced by mac_process_beacon_request().
bool mac_build_and_tx_data_req | ( | bool | expl_poll, |
bool | force_own_long_addr, | ||
uint8_t | expl_dest_addr_mode, | ||
address_field_t * | expl_dest_addr, | ||
uint16_t | expl_dest_pan_id | ||
) |
Build and transmits data request command frame.
This function builds and transmits a data request command frame.
expl_poll | Data request due to explicit MLME poll request |
force_own_long_addr | Forces the usage of the Extended Address as Source Address. This a allows for implicitly poll for pending data at the coordinator if the Extended Address was used in the Beacon frame. |
expl_dest_addr_mode | Mode of subsequent destination address to be used explicitly (0/2/3). 0: No explicit destination address attached, use either macCoordShortAddress or macCoordExtendedAddress 2: Use explicitly attached address in parameter expl_dest_addr as destination address as short address 3: Use explicitly attached address in parameter expl_dest_addr as destination address as extended address |
expl_dest_addr | Explicitly attached destination address for data request frame. This is to be treated as either not present, short or extended address, depending on parameter expl_dest_addr_mode. |
expl_dest_pan_id | Explicitly attached destination PAN-Id (Coordinator PAN-Id) for data request frame. This is to be treated only as present, depending on parameter expl_dest_addr_mode. |
References bmm_buffer_alloc(), bmm_buffer_free(), BMM_BUFFER_POINTER, BROADCAST, frame_info_tag::buffer_header, CCPU_ENDIAN_TO_LE16, convert_16_bit_to_byte_array, convert_64_bit_to_byte_array, convert_spec_16_bit_to_byte_array, CSMA_SLOTTED, CSMA_UNSLOTTED, DATA_REQ_PAYLOAD_LEN, DATAREQUEST, DATAREQUEST_IMPL_POLL, FCF_ACK_REQUEST, FCF_FRAMETYPE_MAC_CMD, FCF_LONG_ADDR, FCF_NO_ADDR, FCF_PAN_ID_COMPRESSION, FCF_SET_DEST_ADDR_MODE, FCF_SET_FRAMETYPE, FCF_SET_SOURCE_ADDR_MODE, FCF_SHORT_ADDR, LARGE_BUFFER_SIZE, address_field_t::long_address, MAC_ASSOCIATED, mac_pib_tag::mac_CoordExtendedAddress, MAC_COORDINATOR, mac_pib_tag::mac_CoordShortAddress, mac_pib_tag::mac_DSN, MAC_IDLE, MAC_NO_SHORT_ADDR_VALUE, mac_pib, MAC_START_REQUEST_CONFIRM, mac_state, MAC_SUCCESS, MAC_SYNC_BEFORE_ASSOC, mac_sync_state, MAKE_MAC_BUSY, frame_info_tag::mpdu, frame_info_tag::msg_type, NON_BEACON_NWK, address_field_t::short_address, tal_pib, and tal_tx_frame().
Referenced by mac_process_beacon_frame(), mac_process_data_frame(), mac_t_response_wait_cb(), and mlme_poll_request().
|
inlinestatic |
References mac_start_persistence_timer(), pal_is_timer_running(), and T_Data_Persistence.
Referenced by mcps_data_request(), mlme_associate_response(), and mlme_disassociate_request().
void mac_coord_realignment_command_tx_success | ( | uint8_t | tx_status, |
buffer_t * | buf_ptr | ||
) |
Continues handling of MLME_START.request (Coordinator realignment) command.
This function is called once the coordinator realignment command is sent out to continue the handling of the MLME_START.request command.
tx_status | Status of the coordinator realignment command transmission |
buf_ptr | Buffer for start confirmation |
References Assert, mlme_start_req_tag::BeaconOrder, mlme_start_req_tag::ChannelPage, gen_mlme_start_conf(), mlme_start_req_tag::LogicalChannel, MAC_INVALID_PARAMETER, mac_sleep_trans(), MAC_SUCCESS, macBattLifeExt, macBeaconOrder, macPANId, macSuperframeOrder, NON_BEACON_NWK, mlme_start_req_tag::PANId, phyCurrentChannel, phyCurrentPage, set_tal_pib_internal(), mlme_start_req_tag::SuperframeOrder, and tal_pib.
Referenced by mac_process_tal_tx_status().
void mac_gen_mcps_data_conf | ( | buffer_t * | buf_ptr, |
uint8_t | status, | ||
uint8_t | handle, | ||
uint32_t | timestamp | ||
) |
References BMM_BUFFER_POINTER, mcps_data_conf_tag::cmdcode, mac_nhle_q, MCPS_DATA_CONFIRM, mcps_data_conf_tag::msduHandle, qmm_queue_append(), mcps_data_conf_tag::status, and mcps_data_conf_tag::Timestamp.
Referenced by handle_exp_persistence_timer(), mac_process_tal_tx_status(), and mcps_data_request().
void mac_gen_mlme_associate_conf | ( | buffer_t * | buf_ptr, |
uint8_t | status, | ||
uint16_t | assoc_short_addr | ||
) |
References mlme_associate_conf_tag::AssocShortAddress, BMM_BUFFER_POINTER, mlme_associate_conf_tag::cmdcode, mac_nhle_q, MLME_ASSOCIATE_CONFIRM, qmm_queue_append(), and mlme_associate_conf_tag::status.
Referenced by mac_process_associate_response(), mac_process_tal_tx_status(), mac_t_assocresponsetime_cb(), mac_t_response_wait_cb(), and mlme_associate_request().
void mac_handle_tx_null_data_frame | ( | void | ) |
References bmm_buffer_free(), BMM_BUFFER_POINTER, build_null_data_frame(), MAC_SUCCESS, MAKE_MAC_BUSY, NO_CSMA_WITH_IFS, and tal_tx_frame().
Referenced by mac_process_data_request(), mac_process_tal_data_ind(), and process_data_ind_not_transient().
void mac_idle_trans | ( | void | ) |
Resets the MAC helper variables and transition to idle state.
This function sets the MAC to idle state and resets MAC helper variables
References Assert, mac_sleep_trans(), mac_soft_reset(), MAC_SUCCESS, mac_trx_wakeup(), macPANId, macPANId_def, macShortAddress, macShortAddress_def, and set_tal_pib_internal().
Referenced by mac_process_tal_data_ind(), mac_process_tal_tx_status(), and process_data_ind_not_transient().
void mac_mlme_comm_status | ( | uint8_t | status, |
buffer_t * | buf_ptr | ||
) |
Creates a Communication Status Indication message to the upper layer.
status | Status of the last operation |
buf_ptr | Buffer for Communication Status Indication to the NHLE |
References BMM_BUFFER_POINTER, mlme_comm_status_ind_tag::cmdcode, mlme_comm_status_ind_tag::DstAddr, mlme_comm_status_ind_tag::DstAddrMode, FCF_LONG_ADDR, mac_nhle_q, MLME_COMM_STATUS_INDICATION, frame_info_tag::mpdu, mlme_comm_status_ind_tag::PANId, PL_POS_DST_ADDR_START, qmm_queue_append(), mlme_comm_status_ind_tag::SrcAddr, mlme_comm_status_ind_tag::SrcAddrMode, mlme_comm_status_ind_tag::status, and tal_pib.
Referenced by handle_exp_persistence_timer(), mac_process_tal_tx_status(), mlme_associate_response(), and mlme_orphan_response().
void mac_prep_disassoc_conf | ( | buffer_t * | buf, |
uint8_t | status | ||
) |
Prepares a disassociation confirm message with device address information.
This functions prepares a disassociation confirm message in case the device address information needs to be extracted.
buf | Buffer for sending MLME disassociate confirm message to NHLE |
status | Status of disassociation |
References BMM_BUFFER_POINTER, BROADCAST, CCPU_ENDIAN_TO_LE16, convert_byte_array_to_16_bit, convert_byte_array_to_64_bit, FCF_2_DEST_ADDR_OFFSET, FCF_LONG_ADDR, FCF_SHORT_ADDR, mac_pib_tag::mac_CoordExtendedAddress, MAC_COORDINATOR, mac_pib_tag::mac_CoordShortAddress, mac_gen_mlme_disassociate_conf(), MAC_NO_SHORT_ADDR_VALUE, MAC_PAN_COORD_STARTED, mac_pib, mac_state, frame_info_tag::mpdu, PL_POS_DST_ADDR_START, PL_POS_FCF_2, and tal_pib.
Referenced by handle_exp_persistence_timer(), and mac_process_tal_tx_status().
void mac_process_associate_request | ( | buffer_t * | assoc_req | ) |
Processes a received association request command frame.
This function will process a received association request command frame and generates a MLME associate indication to the NHLE.
assoc_req | Specifies a pointer to the received association request frame |
References ADDR_COPY_DST_SRC_64, frame_payload_t::assoc_req_data, bmm_buffer_free(), BMM_BUFFER_POINTER, mlme_associate_ind_tag::CapabilityInformation, mlme_associate_ind_tag::cmdcode, mlme_associate_ind_tag::DeviceAddress, address_field_t::long_address, mac_pib_tag::mac_AssociationPermit, mac_nhle_q, mac_parse_data, parse_tag::mac_payload_data, mac_pib, MLME_ASSOCIATE_INDICATION, qmm_queue_append(), and parse_tag::src_addr.
Referenced by mac_process_tal_data_ind(), and process_data_ind_not_transient().
void mac_process_associate_response | ( | buffer_t * | assoc_resp | ) |
Processing of an associaton reponse command frame.
This function processes the received association response command frame.
assoc_resp | Association response receive buffer |
References ADDR_COPY_DST_SRC_64, Assert, frame_payload_t::assoc_response_data, ASSOCIATION_SUCCESSFUL, bmm_buffer_free(), INVALID_SHORT_ADDRESS, address_field_t::long_address, MAC_ASSOCIATED, mac_conf_buf_ptr, mac_pib_tag::mac_CoordExtendedAddress, mac_pib_tag::mac_CoordShortAddress, mac_gen_mlme_associate_conf(), mac_parse_data, parse_tag::mac_payload_data, mac_pib, MAC_POLL_IDLE, mac_poll_state, mac_sleep_trans(), mac_state, MAC_SUCCESS, MAC_SYNC_BEFORE_ASSOC, mac_sync_state, MAC_SYNC_TRACKING_BEACON, macCoordShortAddress_def, macPANId, macPANId_def, macShortAddress, set_tal_pib_internal(), and parse_tag::src_addr.
Referenced by mac_process_tal_data_ind().
void mac_process_beacon_frame | ( | buffer_t * | beacon | ) |
Processes received beacon frame.
This function processes a received beacon frame. When the system is scanning it records PAN descriptor information contained in the beacon. These PAN descriptors will be reported to the next higher layer via MLME_SCAN.confirm. Also this routine constructs the MLME_BEACON_NOTIFY.indication. Additionally when a device is synced with the coordinator, it tracks beacon frames, checks whether the coordinator does have pending data and will initiate the transmission of a data request frame. The routine uses global "parse_data" structure. The PAN descriptors are stored in the mlme_scan_conf_t structure.
beacon | Pointer to the buffer in which the beacon was received |
References wpan_addr_spec_tag::Addr, ADDR_COPY_DST_SRC_16, ADDR_COPY_DST_SRC_64, mlme_beacon_notify_ind_tag::AddrList, wpan_addr_spec_tag::AddrMode, aMaxSIFSFrameSize, Assert, aUnitBackoffPeriod, frame_payload_t::beacon_data, mac_beacon_payload_tag::beacon_payload_len, bmm_buffer_free(), BMM_BUFFER_POINTER, mlme_beacon_notify_ind_tag::BSN, wpan_pandescriptor_tag::ChannelPage, mlme_beacon_notify_ind_tag::cmdcode, convert_byte_array_to_16_bit, convert_byte_array_to_64_bit, wpan_pandescriptor_tag::CoordAddrSpec, parse_tag::fcf, FCF_FRAME_PENDING, FCF_SHORT_ADDR, FUNC_PTR, GET_BEACON_ORDER, GET_FINAL_CAP, GET_GTS_PERMIT, GET_SUPERFRAME_ORDER, mac_beacon_payload_tag::gts_spec, wpan_pandescriptor_tag::GTSPermit, wpan_pandescriptor_tag::LinkQuality, wpan_pandescriptor_tag::LogicalChannel, address_field_t::long_address, mac_pib_tag::mac_AutoRequest, mac_pib_tag::mac_BattLifeExtPeriods, mac_build_and_tx_data_req(), mac_conf_buf_ptr, mac_pib_tag::mac_MaxFrameTotalWaitTime, mac_nhle_q, MAC_NO_DATA, MAC_PAN_COORD_STARTED, mac_parse_data, parse_tag::mac_payload_data, mac_pib, MAC_POLL_IDLE, mac_poll_state, MAC_SCAN_ACTIVE, MAC_SCAN_IDLE, MAC_SCAN_PASSIVE, mac_scan_state, mac_state, MAC_SUCCESS, MAC_SYNC_NEVER, mac_sync_state, macBeaconOrder, macMinLIFSPeriod_def, macMinSIFSPeriod_def, macSuperframeOrder, MAX_PANDESCRIPTORS, MLME_BEACON_NOTIFY_INDICATION, parse_tag::mpdu_length, NON_BEACON_NWK, NUM_LONG_PEND_ADDR, NUM_SHORT_PEND_ADDR, pal_timer_start(), mlme_beacon_notify_ind_tag::PANDescriptor, wpan_addr_spec_tag::PANId, mlme_beacon_notify_ind_tag::PendAddrSpec, mac_beacon_payload_tag::pending_addr_list, mac_beacon_payload_tag::pending_addr_spec, PHY_OVERHEAD, parse_tag::ppdu_link_quality, qmm_queue_append(), mlme_scan_conf_tag::ResultListSize, mlme_scan_conf_tag::scan_result_list, mlme_beacon_notify_ind_tag::sdu, mlme_beacon_notify_ind_tag::sduLength, parse_tag::sequence_number, set_tal_pib_internal(), address_field_t::short_address, parse_tag::src_addr, parse_tag::src_addr_mode, parse_tag::src_panid, mac_beacon_payload_tag::superframe_spec, wpan_pandescriptor_tag::SuperframeSpec, SYMBOLS_PER_OCTET, T_Poll_Wait_Time, TAL_CONVERT_SYMBOLS_TO_US, tal_pib, parse_tag::time_stamp, TIMEOUT_RELATIVE, wpan_pandescriptor_tag::TimeStamp, and WPAN_ADDRMODE_SHORT.
Referenced by process_data_ind_not_transient(), and process_data_ind_scanning().
void mac_process_beacon_request | ( | buffer_t * | msg | ) |
Processes a beacon request.
This function is called in case a beacon request frame has been received by a coordinator. In a nonbeacon-enabled PAN the generation of a beacon frame using CSMA-CA is initiated. In a beacon-enabled PAN no extra beacon frame will be transmitted apart from the standard beacon frames.
msg | Pointer to the buffer in which the beaocn request was received |
References bmm_buffer_free(), mac_build_and_tx_beacon(), NON_BEACON_NWK, and tal_pib.
Referenced by mac_process_tal_data_ind(), and process_data_ind_not_transient().
void mac_process_coord_realign | ( | buffer_t * | ind | ) |
Processing a coordinator realignment command frame.
This function processes a coordinator realignment command frame received from the coordinator (while NOT being in the middle of an Orphan scan, but rather after initiation of a start request primitive from the coordinator indicating realingment. The PAN ID, coord. short address, logical channel, and the device's new short address will be written to the PIB.
ind | Frame reception buffer |
References Assert, bmm_buffer_free(), BROADCAST, mac_coord_realign_tag::channel_page, frame_payload_t::coord_realign_data, parse_tag::fcf, FCF_FRAME_VERSION_2006, mac_coord_realign_tag::logical_channel, mac_pib_tag::mac_CoordShortAddress, mac_parse_data, parse_tag::mac_payload_data, mac_pib, MAC_REALIGNMENT, MAC_SUCCESS, mac_sync_loss(), macPANId, macShortAddress, mac_coord_realign_tag::pan_id, phyCurrentChannel, phyCurrentPage, set_tal_pib_internal(), and mac_coord_realign_tag::short_addr.
Referenced by mac_process_tal_data_ind(), and process_data_ind_not_transient().
void mac_process_data_frame | ( | buffer_t * | buf_ptr | ) |
Processes data frames.
This function processes the data frames received and sends mcps_data_indication to the NHLE.
buf_ptr | Pointer to receive buffer of the data frame |
References ADDR_COPY_DST_SRC_16, ADDR_COPY_DST_SRC_64, bmm_buffer_free(), BMM_BUFFER_POINTER, frame_payload_t::data, parse_tag::dest_addr, parse_tag::dest_addr_mode, parse_tag::dest_panid, parse_tag::fcf, FCF_FRAME_PENDING, FCF_LONG_ADDR, FCF_SHORT_ADDR, address_field_t::long_address, mac_build_and_tx_data_req(), mac_last_dsn, mac_last_src_addr, mac_nhle_q, MAC_PAN_COORD_STARTED, mac_parse_data, parse_tag::mac_payload_data, parse_tag::mac_payload_length, mac_sleep_trans(), mac_state, MCPS_DATA_INDICATION, mac_data_payload_tag::payload, parse_tag::ppdu_link_quality, qmm_queue_append(), parse_tag::sequence_number, address_field_t::short_address, parse_tag::src_addr, parse_tag::src_addr_mode, parse_tag::src_panid, and parse_tag::time_stamp.
Referenced by mac_process_tal_data_ind(), and process_data_ind_not_transient().
void mac_process_data_request | ( | buffer_t * | msg | ) |
Processes a received data request command frame.
This function processes a received data request command frame at the coordinator, searches for pending indirect data frames for the originator and initiates the frame transmission of the data frame with CSMA-CA.
msg | Frame reception buffer pointer |
References Assert, bmm_buffer_free(), BMM_BUFFER_POINTER, frame_info_tag::buffer_header, convert_byte_array_to_16_bit, search_t::criteria_func, FCF_FRAME_PENDING, FCF_LONG_ADDR, FCF_SECURITY_ENABLED, FCF_SHORT_ADDR, find_long_buffer(), find_short_buffer(), search_t::handle, indirect_data_q, frame_info_tag::indirect_in_transit, address_field_t::long_address, MAC_ASSOCIATED, mac_handle_tx_null_data_frame(), MAC_IDLE, mac_parse_data, mac_state, MAC_SUCCESS, MAKE_MAC_BUSY, frame_info_tag::mpdu, NO_CSMA_WITH_IFS, PL_POS_DST_PAN_ID_START, PL_POS_FCF_1, qmm_queue_read(), address_field_t::short_address, parse_tag::src_addr, parse_tag::src_addr_mode, parse_tag::src_panid, and tal_tx_frame().
Referenced by mac_process_tal_data_ind(), and process_data_ind_not_transient().
void mac_process_data_response | ( | void | ) |
Processes a data response to an MLME-POLL.request.
This function processes a data response to an MLME-POLL.request. Our coordinator has responded with a data frame. It is checked whether any data has been received, and the appropriate MLME-POLL.confirm message is constructed.
References Assert, FCF_FRAMETYPE_BEACON, FCF_FRAMETYPE_DATA, parse_tag::frame_type, gen_mlme_poll_conf(), mac_conf_buf_ptr, MAC_NO_DATA, mac_parse_data, parse_tag::mac_payload_length, MAC_POLL_EXPLICIT, MAC_POLL_IDLE, mac_poll_state, MAC_SUCCESS, MAKE_MAC_NOT_BUSY, pal_is_timer_running(), pal_timer_stop(), and T_Poll_Wait_Time.
Referenced by mac_process_tal_data_ind().
void mac_process_disassociate_notification | ( | buffer_t * | msg | ) |
Process a disassociation notification command.
This functions processes a received disassociation notification command frame. Actual data are taken from the incoming frame in mac_parse_buffer.
msg | Frame buffer to be filled in |
References ADDR_COPY_DST_SRC_64, BMM_BUFFER_POINTER, mlme_disassociate_ind_tag::cmdcode, mlme_disassociate_ind_tag::DeviceAddress, frame_payload_t::disassoc_req_data, mlme_disassociate_ind_tag::DisassociateReason, INVALID_SHORT_ADDRESS, address_field_t::long_address, mac_pib_tag::mac_CoordExtendedAddress, mac_pib_tag::mac_CoordShortAddress, mac_nhle_q, mac_parse_data, parse_tag::mac_payload_data, mac_pib, MLME_DISASSOCIATE_INDICATION, qmm_queue_append(), and parse_tag::src_addr.
Referenced by mac_process_tal_data_ind(), and process_data_ind_not_transient().
void mac_process_orphan_notification | ( | buffer_t * | msg | ) |
Handles an orphan notification.
This function processes an incoming orphan notification command. A PAN coordinator gets to this function through a TAL data indication message.
msg | Frame reception buffer |
References ADDR_COPY_DST_SRC_64, BMM_BUFFER_POINTER, mlme_orphan_ind_tag::cmdcode, address_field_t::long_address, mac_nhle_q, mac_parse_data, MLME_ORPHAN_INDICATION, mlme_orphan_ind_tag::OrphanAddress, qmm_queue_append(), and parse_tag::src_addr.
Referenced by mac_process_tal_data_ind(), and process_data_ind_not_transient().
void mac_process_orphan_realign | ( | buffer_t * | buf_ptr | ) |
Processing a coordinator realignment command frame during Orphan scan.
This function processes a coordinator realignment command frame received as a response to the reception of an orphan notification command frame (i.e. while being in the middle of an orphan scan procedure). The PAN ID, coord. short address, logical channel, and the device's new short address will be written to the PIB.
ind | Frame reception buffer |
References Assert, bmm_buffer_free(), BMM_BUFFER_POINTER, BROADCAST, mac_coord_realign_tag::channel_page, mlme_scan_conf_tag::cmdcode, frame_payload_t::coord_realign_data, parse_tag::fcf, FCF_FRAME_VERSION_2006, mac_coord_realign_tag::logical_channel, mac_conf_buf_ptr, mac_pib_tag::mac_CoordShortAddress, mac_nhle_q, mac_parse_data, parse_tag::mac_payload_data, mac_pib, mac_scan_cmd_buf_ptr, MAC_SCAN_IDLE, mac_scan_state, mac_sleep_trans(), MAC_SUCCESS, macPANId, macShortAddress, MLME_SCAN_CONFIRM, MLME_SCAN_TYPE_ORPHAN, mac_coord_realign_tag::pan_id, phyCurrentChannel, phyCurrentPage, qmm_queue_append(), mlme_scan_conf_tag::ResultListSize, scan_set_complete(), mlme_scan_conf_tag::ScanType, set_tal_pib_internal(), mac_coord_realign_tag::short_addr, mlme_scan_conf_tag::status, and mlme_scan_conf_tag::UnscannedChannels.
Referenced by process_data_ind_scanning().
void mac_process_tal_data_ind | ( | uint8_t * | msg | ) |
Depending on received frame the appropriate function is called.
msg | Pointer to the buffer header. |
References Assert, ASSOCIATIONREQUEST, ASSOCIATIONRESPONSE, BEACONREQUEST, bmm_buffer_free(), BMM_BUFFER_POINTER, COORDINATORREALIGNMENT, DATAREQUEST, DISASSOCIATIONNOTIFICATION, FCF_FRAMETYPE_DATA, FCF_FRAMETYPE_MAC_CMD, parse_tag::frame_type, indirect_data_q, LQI_LEN, MAC_AWAIT_ASSOC_RESPONSE, mac_busy, parse_tag::mac_command, MAC_COORDINATOR, mac_handle_tx_null_data_frame(), mac_idle_trans(), mac_parse_data, MAC_POLL_EXPLICIT, MAC_POLL_IDLE, MAC_POLL_IMPLICIT, mac_poll_state, mac_process_associate_request(), mac_process_associate_response(), mac_process_beacon_request(), mac_process_coord_realign(), mac_process_data_frame(), mac_process_data_request(), mac_process_data_response(), mac_process_disassociate_notification(), mac_process_orphan_notification(), MAC_SCAN_IDLE, mac_scan_state, mac_state, frame_info_tag::mpdu, parse_tag::mpdu_length, ORPHANNOTIFICATION, pal_is_timer_running(), pal_timer_stop(), PANIDCONFLICTNOTIFICAION, parse_mpdu(), parse_tag::ppdu_link_quality, process_data_ind_not_transient(), process_data_ind_scanning(), qmm_queue_append(), queue_tag::size, T_Poll_Wait_Time, tal_mac_q, and tal_pib.
void mac_scan_send_complete | ( | retval_t | status | ) |
Continue scanning after the completion of frame transmission.
This functions continues the corresponding scaning depending on status from the transmission of a beacon request or orphan notification frame.
status | Status of transmission |
References Assert, FUNC_PTR, MAC_CALCULATE_SYMBOL_TIME_SCANDURATION, mac_conf_buf_ptr, mac_pib_tag::mac_DSN, mac_pib, mac_pib_tag::mac_ResponseWaitTime, MAC_SCAN_ACTIVE, mac_scan_state, MAC_SUCCESS, mac_t_scan_duration_cb(), pal_timer_start(), scan_curr_channel, scan_duration, scan_proceed(), scan_type, T_Scan_Duration, TAL_CONVERT_SYMBOLS_TO_US, and TIMEOUT_RELATIVE.
Referenced by tal_tx_frame_done_cb().
void mac_sleep_trans | ( | void | ) |
Puts the radio to sleep if this is allowed.
References MAC_INACTIVE, mac_pib, mac_rx_enabled, mac_pib_tag::mac_RxOnWhenIdle, MAC_SYNC_NEVER, mac_sync_state, mac_trx_init_sleep(), NON_BEACON_NWK, pal_is_timer_running(), and tal_pib.
Referenced by gen_mlme_poll_conf(), mac_awake_scan(), mac_coord_realignment_command_tx_success(), mac_idle_trans(), mac_init(), mac_process_associate_response(), mac_process_data_frame(), mac_process_orphan_realign(), mac_process_tal_tx_status(), mac_sync_loss(), mac_t_assocresponsetime_cb(), mac_t_rx_off_cb(), mcps_data_request(), mlme_associate_request(), mlme_disassociate_request(), mlme_reset_request(), mlme_set(), mlme_start_request(), process_data_ind_not_transient(), scan_clean_up(), scan_proceed(), and set_tal_pib_internal().
void mac_start_persistence_timer | ( | void | ) |
References Assert, BO_USED_FOR_MAC_PERS_TIME, FAILURE, FUNC_PTR, MAC_SUCCESS, mac_t_persistence_cb(), NON_BEACON_NWK, pal_timer_start(), T_Data_Persistence, TAL_CONVERT_SYMBOLS_TO_US, TAL_GET_BEACON_INTERVAL_TIME, tal_pib, and TIMEOUT_RELATIVE.
Referenced by mac_check_persistence_timer(), and mac_t_persistence_cb().
void mac_sync_loss | ( | uint8_t | loss_reason | ) |
Function to initiate MLME-SYNC-LOSS.indication to NHLE.
loss_reason | MAC_REALIGNMENT if sync loss is due to receiving coordinator realignment command and MAC_BEACON_LOSS if beacon was lost following a sync request. |
References buffer_t::body, mlme_sync_loss_ind_tag::cmdcode, MAC_ASSOCIATED, MAC_IDLE, mac_nhle_q, MAC_POLL_IDLE, mac_poll_state, MAC_SCAN_IDLE, mac_scan_orig_channel, mac_scan_orig_page, mac_scan_orig_panid, mac_scan_state, mac_sleep_trans(), mac_state, MAC_SYNC_NEVER, mac_sync_state, MLME_SYNC_LOSS_INDICATION, qmm_queue_append(), and tal_pib.
Referenced by check_for_pan_id_conflict_as_pc(), mac_process_coord_realign(), mac_process_tal_tx_status(), and process_data_ind_not_transient().
void mac_t_assocresponsetime_cb | ( | void * | callback_parameter | ) |
References Assert, BROADCAST, mac_conf_buf_ptr, mac_pib_tag::mac_CoordExtendedAddress, mac_pib_tag::mac_CoordShortAddress, mac_gen_mlme_associate_conf(), MAC_NO_DATA, mac_pib, MAC_POLL_IDLE, mac_poll_state, mac_sleep_trans(), MAC_SUCCESS, macCoordShortAddress_def, macPANId, macPANId_def, and set_tal_pib_internal().
Referenced by mac_t_response_wait_cb().
void mac_t_poll_wait_time_cb | ( | void * | callback_parameter | ) |
T_Poll_Wait_Time timer callback.
This function implements the T_Poll_Wait_Time timer callback. If a poll request is pending, a mlme-poll-confirm is generated.
callback_parameter | Callback parameter |
References gen_mlme_poll_conf(), mac_conf_buf_ptr, MAC_NO_DATA, MAC_POLL_EXPLICIT, MAC_POLL_IDLE, mac_poll_state, and MAKE_MAC_NOT_BUSY.
Referenced by mac_process_tal_tx_status().
void mac_t_response_wait_cb | ( | void * | callback_parameter | ) |
Handle T_Poll_Wait_Time timer after successful transmission of an association request frame and before sending out the subsequent data request frame.
callback_parameter | Callback parameter. |
References Assert, FUNC_PTR, INVALID_SHORT_ADDRESS, mac_build_and_tx_data_req(), MAC_CHANNEL_ACCESS_FAILURE, mac_conf_buf_ptr, mac_gen_mlme_associate_conf(), mac_pib, mac_pib_tag::mac_ResponseWaitTime, MAC_SUCCESS, mac_t_assocresponsetime_cb(), pal_timer_start(), T_Poll_Wait_Time, TAL_CONVERT_SYMBOLS_TO_US, and TIMEOUT_RELATIVE.
Referenced by mac_process_tal_tx_status().
void mac_trx_init_sleep | ( | void | ) |
MAC function to put the radio to sleep mode.
References mac_radio_sleep_state, MAC_SUCCESS, pal_timer_source_select(), RADIO_AWAKE, RADIO_SLEEPING, SLEEP_MODE_1, tal_trx_sleep(), TMR_CLK_SRC_DURING_TRX_AWAKE, and TMR_CLK_SRC_DURING_TRX_SLEEP.
Referenced by mac_sleep_trans().
void mac_trx_wakeup | ( | void | ) |
MAC function to wake-up the radio from sleep state.
References FAILURE, mac_radio_sleep_state, pal_timer_source_select(), RADIO_AWAKE, RADIO_SLEEPING, tal_trx_wakeup(), and TMR_CLK_SRC_DURING_TRX_AWAKE.
Referenced by mac_idle_trans(), mac_rx_enable(), mcps_data_request(), mlme_associate_request(), mlme_disassociate_request(), mlme_poll_request(), mlme_reset_request(), mlme_scan_request(), mlme_set(), mlme_start_request(), process_data_ind_not_transient(), and set_tal_pib_internal().
bool mac_tx_coord_realignment_command | ( | frame_msgtype_t | cmd_type, |
buffer_t * | buf_ptr, | ||
uint16_t | new_panid, | ||
uint8_t | new_channel, | ||
uint8_t | new_page | ||
) |
Sends a coordinator realignment command frame.
This function is called either in response to the reception of an orphan notification command from a device (cmd_type = ORPHANREALIGNMENT), or gratuitously whenever the PAN parameters are about to be changed (cmd_type = COORDINATORREALIGNMENT). In the first case, the paramater mor contains a pointer to the respective MLME_ORPHAN.response message, while in the latter case this parameter is unused, and can be passed as NULL.
cmd_type | Determines directed or broadcast mode |
buf_ptr | Pointer to the buffer, using which coord_realignment_command to be sent |
new_panid | Contains the new PAN-ID in case there is a network realignment |
new_channel | Contains the new channel in case there is a network realignment |
new_page | Contains the new channel page in case there is a network realignment |
References BMM_BUFFER_POINTER, BROADCAST, frame_info_tag::buffer_header, convert_16_bit_to_byte_array, convert_64_bit_to_byte_array, convert_spec_16_bit_to_byte_array, COORD_REALIGN_PAYLOAD_LEN, COORDINATORREALIGNMENT, CSMA_SLOTTED, CSMA_UNSLOTTED, FCF_ACK_REQUEST, FCF_FRAME_VERSION_2006, FCF_FRAMETYPE_MAC_CMD, FCF_LONG_ADDR, FCF_SET_DEST_ADDR_MODE, FCF_SET_FRAMETYPE, FCF_SET_SOURCE_ADDR_MODE, FCF_SHORT_ADDR, LARGE_BUFFER_SIZE, mac_pib_tag::mac_DSN, mac_pib, MAC_SUCCESS, MAKE_MAC_BUSY, frame_info_tag::mpdu, frame_info_tag::msg_type, NON_BEACON_NWK, mlme_orphan_resp_tag::OrphanAddress, ORPHANREALIGNMENT, qmm_queue_append(), QUEUE_FULL, mlme_orphan_resp_tag::ShortAddress, tal_pib, and tal_tx_frame().
Referenced by mlme_orphan_response(), and mlme_start_request().
retval_t set_tal_pib_internal | ( | uint8_t | attribute, |
pib_value_t * | attribute_value | ||
) |
Wakes-up the radio and sets the corresponding TAL PIB attribute.
attribute | PIB attribute to be set |
attribute_value | Attribute value to be set |
References mac_radio_sleep_state, mac_sleep_trans(), mac_trx_wakeup(), RADIO_SLEEPING, and tal_pib_set().
Referenced by mac_awake_scan(), mac_coord_realignment_command_tx_success(), mac_idle_trans(), mac_process_associate_response(), mac_process_beacon_frame(), mac_process_coord_realign(), mac_process_orphan_realign(), mac_t_assocresponsetime_cb(), mlme_associate_request(), mlme_start_request(), process_data_ind_not_transient(), scan_clean_up(), and scan_proceed().