Microchip® Advanced Software Framework

wait_for_event.c File Reference

Event handling functionalities to start Peer Search - Performance Analyzer application.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include "app_init.h"
#include "ieee_const.h"
#include "app_frame_format.h"
#include "sio2host.h"
#include "app_peer_search.h"

Macros

#define CONFIG_ED_THRESHOLD   (0x1f)
 

Functions

static void configure_pibs (void)
 Configure the TAL PIB's relevant to the Performance analyzer application. More...
 
void wait_for_event_init (void *arg)
 Application task when the node is in the WAIT_FOR_EVENT state. More...
 
void wait_for_event_rx_cb (frame_info_t *mac_frame_info)
 Callback that is called if data has been received by trx in WAIT_FOR_EVENT state. More...
 
void wait_for_event_task (void)
 Application task handling user events like key press or character on UART. More...
 

#define CONFIG_ED_THRESHOLD   (0x1f)

Referenced by wait_for_event_rx_cb().