app_config.h | These are application-specific resources which are used in the application in addition to the underlaying stack |
 app_frame_format.h | Defines various structure definitions, used to communicate with Peer node over the air - Performance Analyzer application |
 app_init.h | Initialization prototypes and enumerations - Performance Analyzer application |
 app_peer_search.h | Function prototypes for Peera Search process - Performance Analyzer application Copyright (c) 2013-2018 Microchip Technology Inc |
 app_per_mode.h | PER Measuremnt mode prototypes and defines |
 app_range_mode.h | Range Measurement mode related prototypes and defines |
 at86rf212.h | File contains register and command defines specific for AT86RF212 |
 avr2025_mac.h | Copyright (c) 2014-2018 Microchip Technology Inc |
 bmm.c | This file implements the functions for initializing buffer module, allocating and freeing up buffers |
 bmm.h | This file contains the Buffer Management Module definitions |
 board.h | Standard board header file |
 common_hw_timer.h | Copyright (c) 2014-2018 Microchip Technology Inc |
 common_sw_timer.c | Copyright (c) 2013-2018 Microchip Technology Inc |
 common_sw_timer.h | Copyright (c) 2013-2018 Microchip Technology Inc |
 compiler.h | Commonly used includes, types and macros |
 conf_board.h | Board configuration |
 conf_clock.h | Example specific clock configuration file |
 conf_common_sw_timer.h | USART Serial configuration |
 conf_hw_timer.h | USART Serial configuration |
 conf_perf_analyzer.h | Module configuration |
 conf_sio2host.h | USART Serial configuration |
 conf_sleepmgr.h | Sleep manager configuration |
 conf_spi_master.h | Spi Master configuration for spi example |
 conf_trx_access.h | Common TRX Access Configuration |
 conf_usb.h | USB configuration file for CDC application |
 cycle_counter.h | |
 delay.h | Common Delay Service |
 flashc.c | FLASHC driver for AVR32 UC3 |
 flashc.h | FLASHC driver for AVR32 UC3 |
 genclk.h | Generic clock management |
 uc3a3_a4/genclk.h | Chip-specific generic clock management |
 gpio.c | |
 gpio.h | |
 hw_timer.c | Copyright (c) 2014-2018 Microchip Technology Inc |
 hw_timer.h | Copyright (c) 2014-2018 Microchip Technology Inc |
 ieee_154g.h | This header holds all IEEE 802.15.4g-2012 constants and attribute identifiers |
 ieee_const.h | This header holds all IEEE 802.15.4-2006 constants and attribute identifiers |
 init.c | RZ600 board init |
 init_state.c | Initilization functions and utilities - Performance Analyzer application |
 interrupt.h | Global interrupt management for 8- and 32-bit AVR |
 interrupt_avr32.h | Global interrupt management for 32-bit AVR |
 ioport.h | Common IOPORT service main header file for AVR, UC3 and ARM architectures |
 uc3/ioport.h | UC3 architecture specific IOPORT service implementation header file |
 led.c | AT32UC3A3 RZ600 board LEDs support package |
 led.h | AT32UC3A3 RZ600 board LEDs support package |
 mac.h | Provides MAC API to access MAC Layer functionality |
 mac_api.h | MAC API for IEEE 802.15.4-2006 |
 mac_build_config.h | This header file declares macros for various build configurations |
 mac_config.h | These are all timer IDs which are used in MAC |
 mac_msg_const.h | This file defines all message constants |
 mac_msg_type_data_ind.h | This file defines all message structures for the MAC |
 mac_msg_types.h | This file defines all message structures for the MAC |
 main.c | Main of Performance_Analyzer application |
 mrepeat.h | |
 osc.h | Oscillator management |
 uc3a3_a4/osc.h | Chip-specific oscillator management functions |
 pal.c | |
 pal.h | PAL related APIs |
 pal_generic.h | PAL Generic APIs |
 parts.h | Atmel part identification macros |
 peer_search_initiator.c | Initiator/Transmitter functionalities in Peer Search Process - Performance Analyzer application |
 peer_search_receptor.c | Receptor functionalities in Peer Search Process - Performance Analyzer application Copyright (c) 2013-2018 Microchip Technology Inc |
 per_mode_common_utils.c | Common utilities for both Initiator and Receptor in PER Measurement mode - Performance Analyzer application |
 per_mode_initiator.c | Initiator/Transmitter functionalities in PER Measurement mode - Performance Analyzer application This is the source code of a Packet Error Rate Measurement mode as Initiator |
 per_mode_receptor.c | Receptor functionalities in PER Measurement mode - Performance Analyzer application Copyright (c) 2013-2018 Microchip Technology Inc |
 perf_api.h | API function protypes - Performance Analyzer application |
 perf_api_serial_handler.c | SIO service implementation - Performance Analyzer application |
 perf_api_serial_handler.h | This file contains macros and function prototypes for SIO handling |
 perf_msg_const.h | This file defines all Req, confirm, Indication message constants |
 performance_main.c | Main of Performance_Analyzer application |
 performance_main.h | API function protypes - Performance Analyzer application |
 pll.h | PLL management |
 uc3a3_a4/pll.h | Chip-specific PLL definitions |
 pm.c | |
 pm.h | |
 pm_conf_clocks.c | |
 power_clocks_lib.c | |
 power_clocks_lib.h | |
 preprocessor.h | |
 qmm.c | This file implements the functions for initializing the queues, appending a buffer into the queue, removing a buffer from the queue and reading a buffer from the queue as per the search criteria |
 qmm.h | This file contains the Queue Management Module definitions |
 range_measure.c | Range Measurement mode functionaities - Performance Anallyzer application |
 read.c | System-specific implementation of the _read function used by the standard library |
 return_val.h | Return values of APIs |
 rz600.h | AT32UC3A3 RZ600 board header file |
 sio2host.c | Event handling Serial I/O Functionalities |
 sio2host.h | Event handling Serial I/O Functionalities |
 sleep.h | Sleep mode access |
 sleepmgr.c | AVR UC3 Sleep manager implementation |
 sleepmgr.h | Sleep manager |
 uc3/sleepmgr.h | AVR UC3 Sleep manager implementation |
 spi.c | |
 spi.h | |
 spi_master.c | |
 spi_master.h | SPI Master Mode management |
 uc3_spi/spi_master.h | |
 stack_config.h | Stack configuration parameters |
 status_codes.h | Status code definitions |
 stdio_usb.c | USB CDC Standard I/O Serial Management |
 stdio_usb.h | USB Standard I/O Serial Management |
 stringz.h | |
 sysclk.c | Chip-specific system clock management functions |
 sysclk.h | System clock management |
 uc3a3_a4/sysclk.h | Chip-specific system clock management functions |
 tal.c | This file implements the TAL state machine and provides general functionality used by the TAL |
 tal.h | This file contains TAL API function declarations |
 tal_build_config.h | This file contains TAL API function declarations |
 tal_config.h | File contains TAL configuration parameters |
 tal_constants.h | This file contains constants used througthout the TAL |
 tal_ed.c | This file implements ED Scan |
 tal_generic.h | This file contains defines for TAL types |
 tal_helper.c | |
 tal_helper.h | This file contains TAL helper function declarations |
 tal_init.c | This file implements functions for initializing TAL |
 tal_internal.h | This header file contains types and variable definition that are used within the TAL only |
 tal_irq_handler.c | This file handles the interrupts generated by the transceiver |
 tal_irq_handler.h | This header file contains the interrupt handling definitions |
 tal_pib.c | This file handles the TAL PIB attributes, set/get and initialization |
 tal_pib.h | This file contains the prototypes for TAL PIB functions |
 tal_pwr_mgmt.c | This file implements TAL power management functionality of the transceiver |
 tal_rx.c | This file implements the frame reception functions |
 tal_rx.h | File contains macros and modules used while processing a received frame |
 tal_rx_enable.c | File provides functionality supporting RX-Enable feature |
 tal_slotted_csma.c | This file implements slotted CSMA-CA functions |
 tal_slotted_csma.h | File provides CSMA-CA states |
 tal_timer_config.h | File contains TAL timer configuration parameters |
 tal_tx.c | This file handles the frame transmission within the TAL |
 tal_tx.h | File contains the TAL sub-state macros and functions that perform frame transmission |
 tal_types.h | This file contains defines for TAL types |
 tc.c | |
 tc.h | |
 tfa.c | Implementation of Transceiver Feature Access (TFA) functionality |
 tfa.h | This file is the interface for Transceiver Feature Access (TFA) functionality |
 tpaste.h | |
 trampoline_uc3.h | |
 trx_access.c | |
 trx_access.h | HAL related APIs for externally plugged transceivers |
 uc3d_defines_fix.h | Missing Toolchain Definition for UC3 D header files |
 uc3l3_l4_defines_fix.h | Missing Toolchain Definition for UC3 L3 and UC3 L4 header files |
 udc.c | USB Device Controller (UDC) |
 udc.h | Interface of the USB Device Controller (UDC) |
 udc_desc.h | Common API for USB Device Interface |
 udd.h | Common API for USB Device Drivers (UDD) |
 udi.h | Common API for USB Device Interface |
 udi_cdc.c | USB Device Communication Device Class (CDC) interface |
 udi_cdc.h | USB Device Communication Device Class (CDC) interface definitions |
 udi_cdc_conf.h | Default CDC configuration for a USB Device with a single interface |
 udi_cdc_desc.c | Default descriptors for a USB Device with a single interface CDC |
 usb_atmel.h | All USB VIDs and PIDs from Atmel USB applications |
 usb_protocol.h | USB protocol definitions |
 usb_protocol_cdc.h | USB Communication Device Class (CDC) protocol definitions |
 usbb_device.c | USB Device driver Compliance with common driver UDD |
 usbb_device.h | USBB Device Driver header file |
 usbb_otg.h | USBB OTG Driver header file |
 user_interface.c | LED, Button and terminal print functions - Performance Analyzer application |
 user_interface.h | LED,Button,Terminal print event prototypes and defines |
 wait_for_event.c | Event handling functionalities to start Peer Search - Performance Analyzer application |
 write.c | System-specific implementation of the _write function used by the standard library |