Receptor functionalities in PER Measurement mode - Performance Analyzer application for AT86RF215.
Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.
|
static void | app_reset_cb (void *parameter) |
| Timer Callback function if disconnect command is received on air by a node in reflector configuration.This is used to do a software reset on the reflector side. More...
|
|
static void | get_node_info (trx_id_t trx, peer_info_rsp_t *data) |
| Function used to get the board details of peer node. More...
|
|
static void | identify_timer_handler_cb (void *parameter) |
| Timer Callback function if identify command is received on air by a node in reflector configuration. More...
|
|
void | marker_rsp_timer_handler_cb (void *parameter) |
| Timer Callback function if marker command is received on air This is used to blink the LED and thus identify that the marker frame is received. More...
|
|
void | marker_tx_timer_handler_cb (void *parameter) |
| Timer Callback function if marker response command is transmitted on air This is used to blink the LED and thus identify that the transmission is done. More...
|
|
void | per_mode_receptor_init (trx_id_t trx, void *parameter) |
| Initialize the application in PER Measurement mode as Receptor. More...
|
|
void | per_mode_receptor_rx_cb (trx_id_t trx, frame_info_t *frame) |
| Callback that is called if data has been received by trx in the PER_TEST_RECEPTOR state This call back is used when the node is operating as PER Measurement mode Receptor. More...
|
|
void | per_mode_receptor_task (trx_id_t trx) |
| The application task when the node is in PER_TEST_RECEPTOR state i.e.PER Measurement mode as Receptor. More...
|
|
void | per_mode_receptor_tx_done_cb (trx_id_t trx, retval_t status, frame_info_t *frame) |
| Callback that is called once tx is done in PER_TEST_RECEPTOR state This call back is used when the node is operating as PER Measurement mode Receptor. More...
|
|
static void | send_crc_status_rsp (trx_id_t trx) |
| Function used to send crc settings on remote node to host node. More...
|
|
static void | send_peer_info_rsp (trx_id_t trx) |
| Function used to send peer_info_rsp command. More...
|
|
static bool | send_range_test_marker_cmd (trx_id_t trx) |
| Function to send the range test marker command to the initiator node. More...
|
|
static void | send_range_test_rsp (trx_id_t trx, uint8_t seq_num, uint32_t frame_count, int8_t ed, uint8_t lqi) |
| Function used to send response to the received range test packet. More...
|
|
static void | send_result_rsp (trx_id_t trx) |
| Function used to send PER test result. More...
|
|
static void | set_default_configuration_peer_node (trx_id_t trx) |
| Function used to set default configurations on peer node on reception of set_default req. More...
|
|
static void | set_paramter_on_recptor_node (trx_id_t trx, app_payload_t *msg) |
| Extract the received command frame and set the parameters like channel, tx power etc on Receptor node. More...
|
|