These are application-specific resources which are used in the example application of the coordinator in addition to the underlaying stack.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
#define APP_CAPABILITIES |
#define APP_USER_STRING |
Defines the number of additional large buffers used by the application.
#define BOOT_LOADER_SIZE 0 |
#define EE_IEEE_ADDR (0) |
Referenced by main().
#define IEEE_FLASH_OFFSET (INT_FLASH_END - STACK_FLASH_SIZE + 1) |
#define NUM_SUPPORTED_DEV_TYPES (1) |
#define NUM_SUPPORTED_PROFILES (1) |
#define NUMBER_OF_APP_TIMERS (1) |
Defines the number of timers used by the application.
#define SUPPORTED_CEC_CMDS |
#define SUPPORTED_DEV_TYPE_0 DEV_TYPE_TELEVISION |
#define SUPPORTED_DEV_TYPE_1 DEV_TYPE_TELEVISION |
#define SUPPORTED_DEV_TYPE_2 DEV_TYPE_TELEVISION |
#define SUPPORTED_PROFILE_ID_0 PROFILE_ID_ZRC |
#define SUPPORTED_PROFILE_ID_1 PROFILE_ID_ZRC |
#define SUPPORTED_PROFILE_ID_2 PROFILE_ID_ZRC |
#define SUPPORTED_PROFILE_ID_3 PROFILE_ID_ZRC |
#define SUPPORTED_PROFILE_ID_4 PROFILE_ID_ZRC |
#define SUPPORTED_PROFILE_ID_5 PROFILE_ID_ZRC |
#define SUPPORTED_PROFILE_ID_6 PROFILE_ID_ZRC |
#define TOTAL_NUMBER_OF_TIMERS NUMBER_OF_APP_TIMERS |
Defines the total number of timers used by the application and the layers below.
#define USER_STRING_AVAILABLE true |
#define WDT_TIMEOUT_PERIOD WDT_TO_4S |
#define WDT_WAKEUP_INTERVAL WDT_TO_1S |
#define WDT_WAKEUP_INTERVAL_US (1000000) /* micro seconds */ |