Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
RF4CE Single button controller application - ATmega256RFR2 Xplained Pro Documentation

Preface

This is the reference manual for ZRC Single button controller demo application.

Application Files

Application Introduction

Single Button Controller is the RF4CE demo application which can be used in the ZRC target - controller setup This will support push button pairing procedure and zrc commands i.e Sending the button events to the remote terminal target over the air.

Application supports cold reset and warm reset. While powering on the device, if the Select key is pressed then it does cold reset. Otherwise it does warm reset i.e retreiving the network information base from NVM.

If the Select key is pressed on power on, it does the push pairing procedure following the cold reset.

The Application will use the ZRC Commands to send the key press event to paired device.

Application Dependent Modules

Compilation Info

This software was written for the GNU GCC and IAR . Other compilers may or may not work.

References

1) IEEE Std 802.15.4-2006 Part 15.4: Wireless Medium Access Control (MAC) and Physical Layer (PHY) Specifications for Low-Rate Wireless Personal Area Networks (WPANs).

2) Atmel Design Support.

Contact Information

For further information,visit www.microchip.com.