Single button controller application.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
#include <asf.h>
#include "conf_board.h"
#include "common_sw_timer.h"
#include "keyboard.h"
#include "app_config.h"
#include "rf4ce.h"
#include "zrc.h"
#include "pb_pairing.h"
#include "vendor_data.h"
#include "nwk_config.h"
Macros | |
#define | DEBOUNCE_TIME_US 200000 |
#define | TX_OPTIONS |
Typedefs | |
typedef enum node_status_tag | node_status_t |
Enumerations | |
enum | node_status_tag { IDLE, WARM_START, COLD_START, TRANSMITTING } |
Functions | |
static void | app_task (void) |
Application task and state machine. More... | |
FLASH_DECLARE (uint16_t VendorIdentifier) | |
FLASH_DECLARE (uint8_t vendor_string[7]) | |
FLASH_DECLARE (uint8_t app_user_string[15]) | |
FLASH_DECLARE (uint8_t supported_cec_cmds[32]) | |
static void | indicate_fault_behavior (void) |
Indicating malfunction. More... | |
static key_state_t | key_state_read (key_id_t key_no) |
Read key_state. More... | |
int | main (void) |
Main function of the Single Button Controller application. More... | |
static void | nlme_reset_confirm (nwk_enum_t Status) |
void | nlme_rx_enable_confirm (nwk_enum_t Status) |
static void | nlme_start_confirm (nwk_enum_t Status) |
static void | pbp_org_pair_confirm (nwk_enum_t Status, uint8_t PairingRef) |
Push button pairing confirm; target and controller use. More... | |
static void | start_cmd_disc_cb (void *callback_parameter) |
void | vendor_app_alive_req (void) |
Vendor-spefic callback; handles reaction to incoming alive request. More... | |
void | vendor_data_ind (uint8_t PairingRef, uint16_t VendorId, uint8_t nsduLength, uint8_t *nsdu, uint8_t RxLinkQuality, uint8_t RxFlags) |
static void | zrc_cmd_confirm (nwk_enum_t Status, uint8_t PairingRef, cec_code_t RcCmd) |
ZRC command confirm. More... | |
static void | zrc_cmd_disc_confirm (nwk_enum_t Status, uint8_t PairingRef, uint8_t *SupportedCmd) |
static void | zrc_cmd_disc_indication (uint8_t PairingRef) |
Variables | |
uint8_t | app_timer |
static node_status_t | node_status |
static uint8_t | pairing_ref = 0xFF |
zrc_indication_callback_t | zrc_ind |
#define DEBOUNCE_TIME_US 200000 |
Referenced by app_task().
#define TX_OPTIONS |
Referenced by app_task().
typedef enum node_status_tag node_status_t |
enum node_status_tag |
|
static |
Application task and state machine.
References DEBOUNCE_TIME_US, FUNC_PTR, IDLE, KEY_PRESSED, key_state_read(), LED0, LED_On, node_status, nwk_ready_to_sleep(), nwk_stack_idle(), pairing_ref, POWER_TOGGLE_FUNCTION, SELECT_KEY, sw_timer_get_time(), TRANSMITTING, TX_OPTIONS, USER_CONTROL_PRESSED, zrc_cmd_confirm(), and zrc_cmd_request().
Referenced by main().
FLASH_DECLARE | ( | uint16_t | VendorIdentifier | ) |
FLASH_DECLARE | ( | uint8_t | vendor_string[7] | ) |
FLASH_DECLARE | ( | uint8_t | app_user_string[15] | ) |
FLASH_DECLARE | ( | uint8_t | supported_cec_cmds[32] | ) |
|
static |
Indicating malfunction.
References delay_ms, LED0, LED_Off, and LED_On.
Referenced by main(), nlme_reset_confirm(), nlme_rx_enable_confirm(), nlme_start_confirm(), pbp_org_pair_confirm(), and zrc_cmd_confirm().
|
static |
Read key_state.
key_no | Key to be read. |
References GPIO_PUSH_BUTTON_0, ioport_get_pin_level(), KEY_PRESSED, KEY_RELEASED, and SELECT_KEY.
Referenced by app_task(), and main().
int main | ( | void | ) |
Main function of the Single Button Controller application.
References app_task(), app_timer, board_init(), COLD_START, cpu_irq_enable, delay_init, FUNC_PTR, indicate_fault_behavior(), irq_initialize_vectors, KEY_PRESSED, key_state_read(), LED0, LED_On, nlme_reset_confirm(), nlme_reset_request(), node_status, nwk_init(), NWK_SUCCESS, nwk_task(), register_zrc_indication_callback(), SELECT_KEY, sm_init(), sw_timer_get_id(), sw_timer_init(), sysclk_init(), vendor_data_ind(), zrc_indication_callback::vendor_data_ind_cb, WARM_START, zrc_cmd_disc_indication(), and zrc_indication_callback::zrc_cmd_disc_indication_cb.
|
static |
References COLD_START, FUNC_PTR, indicate_fault_behavior(), nlme_rx_enable_confirm(), nlme_rx_enable_request(), nlme_start_confirm(), nlme_start_request(), node_status, NWK_SUCCESS, nwkcMinActivePeriod, pairing_ref, and RX_DURATION_OFF.
Referenced by main().
void nlme_rx_enable_confirm | ( | nwk_enum_t | Status | ) |
References COLD_START, delay_ms, IDLE, indicate_fault_behavior(), LED0, LED_Off, LED_On, node_status, NWK_SUCCESS, and WARM_START.
Referenced by nlme_reset_confirm(), pbp_org_pair_confirm(), vendor_data_ind(), and zrc_cmd_disc_confirm().
|
static |
References APP_CAPABILITIES, DEV_TYPE_REMOTE_CONTROL, DEV_TYPE_WILDCARD, FUNC_PTR, indicate_fault_behavior(), LED0, LED_On, NUM_SUPPORTED_PROFILES, NWK_SUCCESS, pbp_org_pair_confirm(), pbp_org_pair_request(), and PROFILE_ID_ZRC.
Referenced by nlme_reset_confirm().
|
static |
Push button pairing confirm; target and controller use.
The push button pairing confirm is a callback that provides the status of the push pairing request.
Status | Status of the last pairing transaction |
PairingRef | If pairing was successful, PairingRef contains assigned pairing reference. |
References aplcMinTargetBlackoutPeriod_us, app_timer, FUNC_PTR, indicate_fault_behavior(), nlme_rx_enable_confirm(), nlme_rx_enable_request(), NWK_SUCCESS, nwkcMinActivePeriod, pairing_ref, RX_DURATION_OFF, start_cmd_disc_cb(), SW_TIMEOUT_RELATIVE, and sw_timer_start().
Referenced by nlme_start_confirm().
|
static |
References FUNC_PTR, pairing_ref, zrc_cmd_disc_confirm(), and zrc_cmd_disc_request().
Referenced by pbp_org_pair_confirm().
void vendor_app_alive_req | ( | void | ) |
Vendor-spefic callback; handles reaction to incoming alive request.
Vendor data alive request.
References delay_ms, LED0, LED_Off, and LED_On.
Referenced by vendor_data_ind().
void vendor_data_ind | ( | uint8_t | PairingRef, |
uint16_t | VendorId, | ||
uint8_t | nsduLength, | ||
uint8_t * | nsdu, | ||
uint8_t | RxLinkQuality, | ||
uint8_t | RxFlags | ||
) |
References ALIVE_REQ, ALIVE_RESP, BATTERY_STATUS_REQ, BATTERY_STATUS_RESP, FUNC_PTR, FW_DATA_RESP, FW_VERSION_MAJOR, FW_VERSION_MINOR, FW_VERSION_REQ, FW_VERSION_RESP, FW_VERSION_REV, get_batmon_voltage(), nlde_data_request(), nlme_rx_enable_confirm(), nlme_rx_enable_request(), PGM_READ_WORD, PROFILE_ID_ZRC, RX_FLAG_WITH_SEC, RX_ON_REQ, RX_ON_RESP, TXO_ACK_REQ, TXO_CH_NOT_SPEC, TXO_DST_ADDR_NET, TXO_MULTI_CH, TXO_SEC_REQ, TXO_UNICAST, TXO_VEND_SPEC, VD_NOT_SUPPORTED_ATTRIBUTE, vendor_app_alive_req(), and vendor_data_confirm().
Referenced by main().
|
static |
ZRC command confirm.
The ZRC comand confirm callback provides information about the status of the last command request/transmission.
Status | NWK_SUCCESS if transmission was successful |
PairingRef | Pairing reference |
RcCmd | Sent RC command |
References IDLE, indicate_fault_behavior(), LED0, LED_Off, node_status, and NWK_SUCCESS.
Referenced by app_task().
|
static |
References FUNC_PTR, IDLE, nlme_rx_enable_confirm(), nlme_rx_enable_request(), node_status, nwkcMinActivePeriod, and RX_DURATION_OFF.
Referenced by start_cmd_disc_cb().
|
static |
References IDLE, node_status, PGM_READ_BLOCK, and zrc_cmd_disc_response().
Referenced by main().
uint8_t app_timer |
Referenced by main(), and pbp_org_pair_confirm().
|
static |
Referenced by app_task(), main(), nlme_reset_confirm(), nlme_rx_enable_confirm(), zrc_cmd_confirm(), zrc_cmd_disc_confirm(), and zrc_cmd_disc_indication().
|
static |
Referenced by app_task(), nlme_reset_confirm(), pbp_org_pair_confirm(), and start_cmd_disc_cb().
zrc_indication_callback_t zrc_ind |