This header file contains the interrupt handling definitions.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | pal_trx_irq_flag_clr_awake() (CLEAR_TRX_IRQ_AWAKE()) |
Clears the transceiver AWAKE interrupt. More... | |
#define | pal_trx_irq_flag_clr_cca_ed() (CLEAR_TRX_IRQ_CCA_ED()) |
Clears the transceiver CCA_ED_END interrupt. More... | |
#define | pal_trx_irq_flag_clr_rx_end() (CLEAR_TRX_IRQ_RX_END()) |
Clears the transceiver RX_END interrupt. More... | |
#define | pal_trx_irq_flag_clr_tx_end() (CLEAR_TRX_IRQ_TX_END()) |
Clears the transceiver TX_END interrupt. More... | |
Typedefs | |
typedef void(* | irq_handler_t )(void) |
Functions | |
void | pal_trx_irq_init_awake (FUNC_PTR trx_irq_cb) |
Initializes the transceiver AWAKE interrupt. More... | |
void | pal_trx_irq_init_cca_ed (FUNC_PTR trx_irq_cb) |
Initializes the transceiver CCA ED END interrupt. More... | |
void | pal_trx_irq_init_rx_end (FUNC_PTR trx_irq_cb) |
Initializes the transceiver RX END interrupt. More... | |
void | pal_trx_irq_init_tx_end (FUNC_PTR trx_irq_cb) |
Initializes the transceiver TX END interrupt. More... | |
void | trx_awake_handler_cb (void) |
void | trx_irq_timestamp_handler_cb (void) |
Timestamp interrupt handler. More... | |
void | trx_rx_end_handler_cb (void) |
Transceiver interrupt handler. More... | |
void | trx_tx_end_handler_cb (void) |
Transceiver interrupt handler. More... | |
Variables | |
uint32_t | pal_tx_timestamp |
Timestamp of the last frame transmission (including auto-ACK) More... | |
#define pal_trx_irq_flag_clr_awake | ( | ) | (CLEAR_TRX_IRQ_AWAKE()) |
Clears the transceiver AWAKE interrupt.
Referenced by tal_reset().
#define pal_trx_irq_flag_clr_cca_ed | ( | ) | (CLEAR_TRX_IRQ_CCA_ED()) |
Clears the transceiver CCA_ED_END interrupt.
#define pal_trx_irq_flag_clr_rx_end | ( | ) | (CLEAR_TRX_IRQ_RX_END()) |
Clears the transceiver RX_END interrupt.
Referenced by tal_reset(), and tfa_get_batmon_voltage().
#define pal_trx_irq_flag_clr_tx_end | ( | ) | (CLEAR_TRX_IRQ_TX_END()) |
Clears the transceiver TX_END interrupt.
Referenced by handle_received_frame_irq(), tal_reset(), and tfa_get_batmon_voltage().
typedef void(* irq_handler_t)(void) |
void pal_trx_irq_init_awake | ( | FUNC_PTR | trx_irq_cb | ) |
Initializes the transceiver AWAKE interrupt.
This function sets the microcontroller specific registers responsible for handling the transceiver AWAKE interrupt
trx_irq_cb | Callback function for the transceiver AWAKE interrupt |
References irq_hdl_trx_awake.
Referenced by set_trx_state(), and tal_init().
void pal_trx_irq_init_cca_ed | ( | FUNC_PTR | trx_irq_cb | ) |
Initializes the transceiver CCA ED END interrupt.
This function sets the microcontroller specific registers responsible for handling the transceiver CCA ED END interrupt
trx_irq_cb | Callback function for the transceiver CCA ED END interrupt |
References irq_hdl_trx_cca_ed.
void pal_trx_irq_init_rx_end | ( | FUNC_PTR | trx_irq_cb | ) |
Initializes the transceiver RX END interrupt.
This function sets the microcontroller specific registers responsible for handling the transceiver RX END interrupt
trx_irq_cb | Callback function for the transceiver RX END interrupt |
References irq_hdl_trx_rx_end.
Referenced by tal_init().
void pal_trx_irq_init_tx_end | ( | FUNC_PTR | trx_irq_cb | ) |
Initializes the transceiver TX END interrupt.
This function sets the microcontroller specific registers responsible for handling the transceiver TX END interrupt
trx_irq_cb | Callback function for the transceiver TX END interrupt |
References irq_hdl_trx_tx_end.
Referenced by tal_init().
uint32_t pal_tx_timestamp |
Timestamp of the last frame transmission (including auto-ACK)
Referenced by ISR(), and tx_done_handling().