Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
MAC Symbol Counter Driver(MACSC)

See Quick Start Guide for the MEGARF MACSC Driver.

This is a driver for the AVR MEGARF MAC Symbol Counter Driver(MACSC). It provides functions for enabling, disabling and configuring the module.

Dependencies

This driver depends on the following modules:

Modules

 MAC Symbol Counter (MACSC) interrupt
 management This group provides functions to configure MACSC module interrupts
 

Macros

#define CONCAT(a, b)   a ## b
 String concatenation by preprocessor used to create proper register names. More...
 
#define MACSC_ABSOLUTE_CMP   0
 
#define MACSC_READ32(reg)
 Creates proper subregister names and reads the corresponding values. More...
 
#define MACSC_RELATIVE_CMP   1
 
#define MACSC_WRITE32(reg, val)
 

Typedefs

typedef void(* macsc_callback_t )(void)
 Interrupt event callback function type. More...
 

Enumerations

enum  macsc_cc_channel {
  MACSC_CC1 = 1,
  MACSC_CC2 = 2,
  MACSC_CC3 = 3
}
 
enum  macsc_xtal {
  MACSC_16MHz = 0,
  MACSC_32KHz = 1
}
 MAC SC clock source select. More...
 

Functions

bool is_macsc_backoff_enable (void)
 Check if back-off slot counter is enabled. More...
 
bool is_macsc_enable (void)
 Check if MACSC is enabled. More...
 
void macsc_disable (void)
 Disable MAC SC. More...
 
void macsc_enable (void)
 Enable MAC SC. More...
 
void macsc_enable_cmp_int (enum macsc_cc_channel channel)
 Enables compare interrupts of the MACSC. More...
 
static uint32_t macsc_read32 (volatile uint8_t *hh, volatile uint8_t *hl, volatile uint8_t *lh, volatile uint8_t *ll)
 Reads the 32-bit timer register in the required order of bytes. More...
 
static void macsc_sleep_clk_disable (void)
 Disable 32.768KHz clk using timer 2 async register. More...
 
static void macsc_sleep_clk_enable (void)
 Enable 32.768KHz clk using timer 2 async register. More...
 
void macsc_use_cmp (bool abs_rel, uint32_t cmp, enum macsc_cc_channel channel)
 Usage of Absolute compare mode of the MACSC. More...
 

#define CONCAT (   a,
 
)    a ## b

String concatenation by preprocessor used to create proper register names.

#define MACSC_ABSOLUTE_CMP   0
#define MACSC_READ32 (   reg)
Value:
macsc_read32(&CONCAT(reg, HH), \
&CONCAT(reg, HL), \
&CONCAT(reg, LH), \
&CONCAT(reg, LL))
static uint32_t macsc_read32(volatile uint8_t *hh, volatile uint8_t *hl, volatile uint8_t *lh, volatile uint8_t *ll)
Reads the 32-bit timer register in the required order of bytes.
Definition: macsc_megarf.h:109
#define CONCAT(a, b)
String concatenation by preprocessor used to create proper register names.
Definition: macsc_megarf.h:134

Creates proper subregister names and reads the corresponding values.

Referenced by macsc_read_bts(), macsc_read_count(), and macsc_read_ts().

#define MACSC_RELATIVE_CMP   1
#define MACSC_WRITE32 (   reg,
  val 
)
Value:
do { \
union { uint8_t a[4]; uint32_t v; } \
x; \
x.v = val; \
CONCAT(reg, HH) = x.a[3]; \
CONCAT(reg, HL) = x.a[2]; \
CONCAT(reg, LH) = x.a[1]; \
CONCAT(reg, LL) = x.a[0]; \
} \
while (0)
#define CONCAT(a, b)
String concatenation by preprocessor used to create proper register names.
Definition: macsc_megarf.h:134

Referenced by macsc_use_cmp(), and macsc_write_count().

typedef void(* macsc_callback_t)(void)

Interrupt event callback function type.

The interrupt handler can be configured to do a function callback, the callback function must match the macsc_callback_t type.

Enumerator
MACSC_CC1 
MACSC_CC2 
MACSC_CC3 
enum macsc_xtal

MAC SC clock source select.

uses the SCCKSEL bit in SSCR register to select macsc clk src

If the bit is one,the RTC clock from TOSC1 is selected, otherwise the symbol counter operates with the clock from XTAL1. During transceiver sleep modes the clock falls back to the RTC clock source, regardless of the selected clock. After wakeup, it switches back to the previosly selected clock source.

Enumerator
MACSC_16MHz 
MACSC_32KHz 

bool is_macsc_backoff_enable ( void  )

Check if back-off slot counter is enabled.

check if the back-off slot counter is enabled.

Parameters
none
bool is_macsc_enable ( void  )

Check if MACSC is enabled.

check if the MACSC is enabled.

Parameters
none
void macsc_disable ( void  )

Disable MAC SC.

Disables the MAC SC

Parameters
none

Referenced by cmp3_int_cb().

void macsc_enable ( void  )

Enable MAC SC.

Enables the SC

Parameters
clk_srcselection of clk source,avalable options in macsc_xtal,fixed prescalar
sleep_enableenable RTC as clock source during sleep
auto_tsenable automatic timestamping

Enables the SC

Parameters
none

References cpu_irq_restore(), and cpu_irq_save().

Referenced by sm_sleep().

void macsc_enable_cmp_int ( enum macsc_cc_channel  channel)

Enables compare interrupts of the MACSC.

Parameters
channelCompare channel

References MACSC_CC1, MACSC_CC2, and MACSC_CC3.

Referenced by sm_init().

static uint32_t macsc_read32 ( volatile uint8_t *  hh,
volatile uint8_t *  hl,
volatile uint8_t *  lh,
volatile uint8_t *  ll 
)
inlinestatic

Reads the 32-bit timer register in the required order of bytes.

Parameters
hhhh octet of 32-bit register
hlhl octet of 32-bit register
lhlh octet of 32-bit register
llll octet of 32-bit register
Returns
uint32_t Value of timer register
static void macsc_sleep_clk_disable ( void  )
inlinestatic

Disable 32.768KHz clk using timer 2 async register.

Parameters
none
static void macsc_sleep_clk_enable ( void  )
inlinestatic

Enable 32.768KHz clk using timer 2 async register.

Parameters
none

Referenced by sm_init().

void macsc_use_cmp ( bool  abs_rel,
uint32_t  cmp,
enum macsc_cc_channel  channel 
)

Usage of Absolute compare mode of the MACSC.

Parameters
abs_rel0 for absoulte cmp;1 for relative cmp
cmpcompare value for SCOCRx register
channelCompare channel

Usage of Absolute compare mode of the MACSC.

Parameters
abs_rel0 for absoulte cmp;1 for relative cmp
cmpcompare value for SCOCRx register
channelCompare channel

References MACSC_CC1, MACSC_CC2, MACSC_CC3, and MACSC_WRITE32.

Referenced by sm_sleep().