ATmega256RFR2 Xplained Pro board header file.
This file contains definitions and services related to the features of the ATmega256RFR2 Xplained Pro board.
To use this board, define BOARD= ATMEGA256RFR2_XPLAINED_PRO.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | BOARD_NAME "ATMEGA256RFR2-XPRO" |
#define | MCU_SOC_NAME "ATMEGA256RFR2" |
GPIO Connections of LED | |
LED0 is connected to PORTB pin 4 | |
#define | LED_ON_BOARD IOPORT_CREATE_PIN(PORTB, 4) |
#define | LED0_GPIO LED_ON_BOARD |
#define | LED0 LED0_GPIO |
#define | LED_COUNT 1 |
GPIO Connections of Switch | |
Push button is connected to PORTE pin 4. | |
#define | GPIO_PUSH_BUTTON_ON_BOARD IOPORT_CREATE_PIN(PORTE, 4) |
#define | GPIO_PUSH_BUTTON_0 GPIO_PUSH_BUTTON_ON_BOARD |
#define BOARD_NAME "ATMEGA256RFR2-XPRO" |
#define GPIO_PUSH_BUTTON_0 GPIO_PUSH_BUTTON_ON_BOARD |
#define GPIO_PUSH_BUTTON_ON_BOARD IOPORT_CREATE_PIN(PORTE, 4) |
Referenced by board_init().
#define LED0 LED0_GPIO |
#define LED0_GPIO LED_ON_BOARD |
#define LED_COUNT 1 |
Referenced by appDataInd().
#define LED_ON_BOARD IOPORT_CREATE_PIN(PORTB, 4) |
Referenced by board_init().
#define MCU_SOC_NAME "ATMEGA256RFR2" |