Blood Pressure Sensor Profile declarations.
Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | ADV_DATA_LEN (18) |
ADV_DATA_LEN. More... | |
#define | ADV_TYPE_LEN (0x01) |
ADV_TYPE_LEN. More... | |
#define | BLP_SENSOR_ADV_DATA_COMP_16_UUID_TYPE (0x03) |
HR_SENSOR_ADV_DATA_UUID_TYPE is complete 16 bit uuid type. More... | |
#define | BLP_SENSOR_ADV_DATA_NAME_DATA ("ATMEL-BLP") |
#define | BLP_SENSOR_ADV_DATA_NAME_LEN (9) |
BLP_SENSOR_ADV_DATA_NAME_LEN the length of the device name. More... | |
#define | BLP_SENSOR_ADV_DATA_NAME_TYPE (0x09) |
BLP_SENSOR_ADV_DATA_NAME_TYPE the gap ad data type. More... | |
#define | BLP_SENSOR_ADV_DATA_UUID_LEN (4) |
HR_SENSOR_ADV_DATA_UUID_LEN the total length for hr uuid and dis uuid. More... | |
#define | BLP_SENSOR_ADV_TIMEOUT (655) |
BLP_SENSOR_ADV_TIMEOUT Advertising time-out between 0x0001 and 0x028F in seconds, 0x0000 disables time-out. More... | |
#define | BLP_SENSOR_FAST_ADV (100) |
APP_BLP_SENSOR_FAST_ADV between 0x0020 and 0x4000 in 0.625 ms units (20ms to 10.24s). More... | |
#define | DEVICE_INFORMATION_SERVICE_UUID (0x180A) |
DEVICE_INFORMATION_SERVICE_UUID. More... | |
#define | SCAN_RESP_LEN (10) |
scan_resp_len is the length of the scan response data More... | |
#define | UUID_16_BIT_LEN (0x02) |
Typedefs | |
typedef void(* | blp_indication_callback_t )(bool) |
typedef void(* | blp_notification_callback_t )(bool) |
Functions | |
void | blp_disconnection (void) |
blp_disconnection called by the application to disconnect More... | |
at_ble_status_t | blp_indication_confirmation_handler (void *params) |
blp_indication_confirmation_handler called by ble manager to give the status of notification sent More... | |
at_ble_status_t | blp_notification_confirmation_handler (void *params) |
blp_notification_confirmation_handler called by ble manager to give the status of notification sent More... | |
void | blp_sensor_adv (void) |
blp_sensor_adv adds the advertisement data of the profile and starts advertisement More... | |
at_ble_status_t | blp_sensor_char_changed_handler (void *char_handle) |
blp_sensor_char_changed_handler called by the ble manager after a change in the characteristic More... | |
at_ble_status_t | blp_sensor_connected_state_handler (void *conn_params) |
blp_sensor_connected_state_handler called by ble manager after a change in characteristic More... | |
at_ble_status_t | blp_sensor_disconnect_event_handler (void *disconnect) |
blp_sensor_disconnect_event_handler called by ble manager after disconnection event received More... | |
void | blp_sensor_init (void *param) |
blp_sensor_init initializes and defines the services of the blp profile More... | |
void | blp_sensor_send_indication (uint8_t *blp_data, uint8_t length) |
blp_sensor_send_indication adds the new characteristic value and sends the indication More... | |
void | blp_sensor_send_notification (uint8_t *hr_data, uint8_t length) |
blp_sensor_send_notification disconnects with the peer device called by the application More... | |
void | blp_sensor_service_define (void) |
blp_sensor_service_define defines the services of the profile More... | |
void | blp_sensor_service_init (void) |
blp_sensor_service_init initializes the services of the profile More... | |
void | register_blp_indication_handler (blp_indication_callback_t blp_indication_handler) |
register_blp_indication_handler registers the indication handler passed by the application More... | |
void | register_blp_notification_handler (blp_notification_callback_t blp_notificaton_handler) |
register_blp_notification_handler registers the notification handler passed by the application More... | |
#define ADV_DATA_LEN (18) |
ADV_DATA_LEN.
#define ADV_TYPE_LEN (0x01) |
ADV_TYPE_LEN.
#define BLP_SENSOR_ADV_DATA_COMP_16_UUID_TYPE (0x03) |
HR_SENSOR_ADV_DATA_UUID_TYPE is complete 16 bit uuid type.
#define BLP_SENSOR_ADV_DATA_NAME_DATA ("ATMEL-BLP") |
#define BLP_SENSOR_ADV_DATA_NAME_LEN (9) |
BLP_SENSOR_ADV_DATA_NAME_LEN the length of the device name.
#define BLP_SENSOR_ADV_DATA_NAME_TYPE (0x09) |
BLP_SENSOR_ADV_DATA_NAME_TYPE the gap ad data type.
#define BLP_SENSOR_ADV_DATA_UUID_LEN (4) |
HR_SENSOR_ADV_DATA_UUID_LEN the total length for hr uuid and dis uuid.
#define BLP_SENSOR_ADV_TIMEOUT (655) |
BLP_SENSOR_ADV_TIMEOUT Advertising time-out between 0x0001 and 0x028F in seconds, 0x0000 disables time-out.
Referenced by blp_sensor_adv().
#define BLP_SENSOR_FAST_ADV (100) |
APP_BLP_SENSOR_FAST_ADV between 0x0020 and 0x4000 in 0.625 ms units (20ms to 10.24s).
Referenced by blp_sensor_adv().
#define DEVICE_INFORMATION_SERVICE_UUID (0x180A) |
DEVICE_INFORMATION_SERVICE_UUID.
#define SCAN_RESP_LEN (10) |
scan_resp_len is the length of the scan response data
#define UUID_16_BIT_LEN (0x02) |
typedef void(* blp_indication_callback_t)(bool) |
typedef void(* blp_notification_callback_t)(bool) |
void blp_disconnection | ( | void | ) |
blp_disconnection called by the application to disconnect
References at_ble_disconnect(), AT_BLE_SUCCESS, AT_BLE_TERMINATED_BY_USER, connection_handle, and DBG_LOG.
Referenced by update_blp_sensor_value().
at_ble_status_t blp_indication_confirmation_handler | ( | void * | params | ) |
blp_indication_confirmation_handler called by ble manager to give the status of notification sent
[in] | at_ble_cmd_complete_event_t | address of the cmd completion |
References AT_BLE_SUCCESS, DBG_LOG_DEV, and at_ble_cmd_complete_event_t::status.
at_ble_status_t blp_notification_confirmation_handler | ( | void * | params | ) |
blp_notification_confirmation_handler called by ble manager to give the status of notification sent
[in] | at_ble_cmd_complete_event_t | address of the cmd completion |
References AT_BLE_SUCCESS, DBG_LOG_DEV, and at_ble_cmd_complete_event_t::status.
void blp_sensor_adv | ( | void | ) |
blp_sensor_adv adds the advertisement data of the profile and starts advertisement
blp_sensor_adv adds the advertisement data of the profile and starts advertisement
References AT_BLE_ADV_FP_ANY, AT_BLE_ADV_GEN_DISCOVERABLE, at_ble_adv_start(), AT_BLE_ADV_TYPE_UNDIRECTED, AT_BLE_SUCCESS, BLP_SENSOR_ADV_TIMEOUT, BLP_SENSOR_FAST_ADV, and DBG_LOG.
Referenced by app_disconnected_state_handler(), and main().
at_ble_status_t blp_sensor_char_changed_handler | ( | void * | char_handle | ) |
blp_sensor_char_changed_handler called by the ble manager after a change in the characteristic
[in] | at_ble_characteristic_changed_t | which contains handle of characteristic and new value |
References AT_BLE_SUCCESS, blp_char_change_handler(), BLP_INDICATION_DISABLE, BLP_INDICATION_ENABLE, BLP_NOTIFICATION_DISABLE, BLP_NOTIFICATION_ENABLE, indication_cb, and notification_cb.
at_ble_status_t blp_sensor_connected_state_handler | ( | void * | conn_params | ) |
blp_sensor_connected_state_handler called by ble manager after a change in characteristic
[in] | at_ble_connected_t | which has connection handle and the peer device address |
References AT_BLE_SUCCESS, and connection_handle.
at_ble_status_t blp_sensor_disconnect_event_handler | ( | void * | disconnect | ) |
blp_sensor_disconnect_event_handler called by ble manager after disconnection event received
@param[in] at_ble_disconnected_t which has connection handle and
reason for disconnection
References ALL_UNUSED, and AT_BLE_SUCCESS.
void blp_sensor_init | ( | void * | param | ) |
blp_sensor_init initializes and defines the services of the blp profile
[in] | params | are unused. |
blp_sensor_init initializes and defines the services of the blp profile
[in] | params | are unused. |
References ALL_UNUSED, AT_BLE_SUCCESS, ble_advertisement_data_set(), BLE_GAP_EVENT_TYPE, BLE_GATT_SERVER_EVENT_TYPE, ble_mgr_events_callback_handler(), blp_sensor_service_define(), blp_sensor_service_init(), at_ble_characteristic_t::char_val_handle, at_ble_characteristic_t::client_config_handle, DBG_LOG, DBG_LOG_PTS, at_ble_characteristic_t::init_value, REGISTER_CALL_BACK, hr_gatt_service_handler::serv_chars, dis_gatt_service_handler::serv_chars, hr_gatt_service_handler::serv_handle, and dis_gatt_service_handler::serv_handle.
Referenced by main().
void blp_sensor_send_indication | ( | uint8_t * | blp_data, |
uint8_t | length | ||
) |
blp_sensor_send_indication adds the new characteristic value and sends the indication
[in] | blp | the new blp characteristic value needs to be updated |
[in] | length | length of new characteristic value |
Updating the new characteristic value
Sending the indication for the updated characteristic
References at_ble_characteristic_value_set(), at_ble_indication_send(), AT_BLE_SUCCESS, at_ble_characteristic_t::char_val_handle, connection_handle, DBG_LOG, and hr_gatt_service_handler::serv_chars.
Referenced by app_indication_handler(), and blp_char_indication().
void blp_sensor_send_notification | ( | uint8_t * | blp_data, |
uint8_t | length | ||
) |
blp_sensor_send_notification disconnects with the peer device called by the application
blp_sensor_send_notification disconnects with the peer device called by the application
[in] | blp_data | the new hr characteristic value needs to be updated |
[in] | length | length of new characteristic value |
Updating the new characteristic value
Sending the notification for the updated characteristic
References at_ble_characteristic_value_set(), at_ble_notification_send(), AT_BLE_SUCCESS, at_ble_characteristic_t::char_val_handle, connection_handle, DBG_LOG, and hr_gatt_service_handler::serv_chars.
Referenced by blp_char_notification().
void blp_sensor_service_define | ( | void | ) |
blp_sensor_service_define defines the services of the profile
References AT_BLE_SUCCESS, blp_primary_service_define(), DBG_LOG, and dis_primary_service_define().
Referenced by blp_sensor_init().
void blp_sensor_service_init | ( | void | ) |
blp_sensor_service_init initializes the services of the profile
blp_sensor_service_init initializes the services of the profile
References blp_init_service(), and dis_init_service().
Referenced by blp_sensor_init().
void register_blp_indication_handler | ( | blp_indication_callback_t | blp_indication_handler | ) |
register_blp_indication_handler registers the indication handler passed by the application
[in] | blp_indication_callback_t | address of the indication handler function to be called |
References indication_cb.
Referenced by main().
void register_blp_notification_handler | ( | blp_notification_callback_t | blp_notificaton_handler | ) |
register_blp_notification_handler registers the notification handler passed by the application
[in] | blp_notification_callback_t | address of the notification handler function to be called |
References notification_cb.
Referenced by main().