Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Address Management APIs

This group includes GAP address APIs.

Functions

at_ble_status_t at_ble_addr_get (at_ble_addr_t *address)
 Get device BT Address. More...
 
at_ble_status_t at_ble_addr_set (at_ble_addr_t *address)
 Set device BT Address. More...
 
at_ble_status_t at_ble_random_address_resolve (uint8_t nb_key, at_ble_addr_t *rand_addr, uint8_t *irk_key)
 Handles request of resolving a resolvable random address ,AT_BLE_RESOLV_RAND_ADDR_STATUS event is used to inform which key has been used to perform resolution for the returned address. More...
 

at_ble_status_t at_ble_addr_get ( at_ble_addr_t address)

Get device BT Address.

Parameters
[out]addresspointer to save returned BT Address
Returns
Upon successful completion the function shall return AT_BLE_SUCCESS, Otherwise the function shall return at_ble_status_t

Referenced by ble_set_dev_config().

at_ble_status_t at_ble_addr_set ( at_ble_addr_t address)

Set device BT Address.

Parameters
[in]addressthe new BT address
Precondition
In case of using resolvable random address, at_ble_set_dev_config is used to set device IRK key otherwise default randomness IRK key values will be used.
Note
Returns
Upon successful completion the function shall return AT_BLE_SUCCESS, Otherwise the function shall return at_ble_status_t

Referenced by ble_set_dev_config().

at_ble_status_t at_ble_random_address_resolve ( uint8_t  nb_key,
at_ble_addr_t rand_addr,
uint8_t *  irk_key 
)

Handles request of resolving a resolvable random address ,AT_BLE_RESOLV_RAND_ADDR_STATUS event is used to inform which key has been used to perform resolution for the returned address.

Parameters
[in]nb_keynumber of provided IRK
[in]rand_addrpointer to the random address
[in]irk_keyarray of IRK used for address resolution
Note
  • irk_key argument, should be known after exchanging keys at security level (bonding).
Returns
Upon successful completion the function shall return AT_BLE_SUCCESS, Otherwise the function shall return at_ble_status_t

Referenced by ble_connected_state_handler().