Link Loss Service declarations.
Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.
Data Structures | |
struct | gatt_lls_char_handler |
Macros | |
#define | INVALID_LLS_PARAM (0xff) |
#define | LLS_CHARACTERISTIC_COUNT (1) |
count of characteristics in linkloss service More... | |
#define | LLS_CLIENT 0 |
#define | LLS_INCLUDED_SERVICE_COUNT (0) |
count of included service in Linkloss service More... | |
#define | LLS_SERVER 0 |
Typedefs | |
typedef struct gatt_lls_char_handler | gatt_lls_char_handler_t |
typedef enum linkloss_alert_level | linkloss_alert_level_t |
Enumerations | |
enum | linkloss_alert_level { LLS_NO_ALERT, LLS_MILD_ALERT, LLS_HIGH_ALERT } |
Functions | |
void | init_linkloss_service (gatt_service_handler_t *linkloss_serv) |
Initialize the linkloss service with default values. More... | |
at_ble_status_t | lls_primary_service_define (gatt_service_handler_t *lls_service) |
Defining linkloss service to the attribute data base. More... | |
uint8_t | lls_set_alert_value (at_ble_characteristic_changed_t *change_params, gatt_service_handler_t *lls_handler) |
sets the alert value of the Linkloss service More... | |
#define INVALID_LLS_PARAM (0xff) |
Referenced by lls_set_alert_value(), and pxp_reporter_char_changed_handler().
#define LLS_CHARACTERISTIC_COUNT (1) |
count of characteristics in linkloss service
Referenced by lls_primary_service_define().
#define LLS_CLIENT 0 |
#define LLS_INCLUDED_SERVICE_COUNT (0) |
count of included service in Linkloss service
Referenced by lls_primary_service_define().
#define LLS_SERVER 0 |
typedef struct gatt_lls_char_handler gatt_lls_char_handler_t |
typedef enum linkloss_alert_level linkloss_alert_level_t |
enum linkloss_alert_level |
void init_linkloss_service | ( | gatt_service_handler_t * | linkloss_serv | ) |
Initialize the linkloss service with default values.
[in] | gatt_service_handler_t | the service info which has handle range,uuid and characteristic array fields |
Initialize the linkloss service with default values.
References ALERT_LEVEL_CHAR_UUID, AT_BLE_ATTR_NO_PERMISSIONS, AT_BLE_ATTR_READABLE_NO_AUTHN_NO_AUTHR, AT_BLE_ATTR_READABLE_REQ_AUTHN_NO_AUTHR, AT_BLE_ATTR_WRITABLE_NO_AUTHN_NO_AUTHR, AT_BLE_ATTR_WRITABLE_REQ_AUTHN_NO_AUTHR, AT_BLE_CHAR_READ, AT_BLE_CHAR_WRITE, AT_BLE_UUID_16, LINK_LOSS_SERVICE_UUID, and linkloss_initial_value.
Referenced by pxp_service_init().
at_ble_status_t lls_primary_service_define | ( | gatt_service_handler_t * | lls_service | ) |
Defining linkloss service to the attribute data base.
[in] | gatt_service_handler_t | the service info which has handle range,uuid and characteristic array fields |
Defining linkloss service to the attribute data base.
References at_ble_primary_service_define(), LLS_CHARACTERISTIC_COUNT, and LLS_INCLUDED_SERVICE_COUNT.
Referenced by pxp_service_define().
uint8_t lls_set_alert_value | ( | at_ble_characteristic_changed_t * | change_params, |
gatt_service_handler_t * | lls_handler | ||
) |
sets the alert value of the Linkloss service
[in] | gatt_service_handler_t | the service info which has handle range,uuid and characteristic array fields |
[in] | at_ble_characteristic_changed_t | the information of the characteristic changed. |
sets the alert value of the Linkloss service
References at_ble_characteristic_changed_t::char_handle, at_ble_characteristic_changed_t::char_new_value, DBG_LOG, INVALID_LLS_PARAM, lls_gs_str, and LLS_HIGH_ALERT.
Referenced by pxp_reporter_char_changed_handler().