Immediate Alert Service declarations.
Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.
#include "ble_manager.h"
Macros | |
#define | IAS_CHARACTERISTIC_COUNT (1) |
count of characteristics in immediate alert service More... | |
#define | IAS_CLIENT 0 |
#define | IAS_INCLUDED_SERVICE_COUNT (0) |
count of included service in immediate alert service More... | |
#define | IAS_SERVER 0 |
#define | INVALID_IAS_PARAM (0xff) |
Invalid parameter written. More... | |
Typedefs | |
typedef enum immediate_alert_level | immediate_alert_level_t |
Enumerations | |
enum | immediate_alert_level { IAS_NO_ALERT, IAS_MID_ALERT, IAS_HIGH_ALERT } |
Functions | |
at_ble_status_t | ias_primary_service_define (gatt_service_handler_t *ias_primary_service) |
Defining Immediate alert service to the attribute data base. More... | |
uint8_t | ias_set_alert_value (at_ble_characteristic_changed_t *change_params, gatt_service_handler_t *ias_handler) |
sets the alert value of the immediate alert service More... | |
void | init_immediate_alert_service (gatt_service_handler_t *immediate_alert_serv) |
Initialize the Immediate alert service with default values. More... | |
#define IAS_CHARACTERISTIC_COUNT (1) |
count of characteristics in immediate alert service
Referenced by ias_primary_service_define().
#define IAS_CLIENT 0 |
#define IAS_INCLUDED_SERVICE_COUNT (0) |
count of included service in immediate alert service
Referenced by ias_primary_service_define().
#define IAS_SERVER 0 |
#define INVALID_IAS_PARAM (0xff) |
Invalid parameter written.
Referenced by ias_set_alert_value(), and pxp_reporter_char_changed_handler().
typedef enum immediate_alert_level immediate_alert_level_t |
at_ble_status_t ias_primary_service_define | ( | gatt_service_handler_t * | ias_primary_service | ) |
Defining Immediate alert service to the attribute data base.
[in] | gatt_service_handler_t | the service info which has handle range,uuid and characteristic array fields |
Defining Immediate alert service to the attribute data base.
References at_ble_primary_service_define(), IAS_CHARACTERISTIC_COUNT, and IAS_INCLUDED_SERVICE_COUNT.
Referenced by pxp_service_define().
uint8_t ias_set_alert_value | ( | at_ble_characteristic_changed_t * | change_params, |
gatt_service_handler_t * | ias_handler | ||
) |
sets the alert value of the immediate alert service
[in] | gatt_service_handler_t | the service info which has handle range,uuid and characteristic array fields |
[in] | at_ble_characteristic_changed_t | the information of the characteristic changed. |
sets the alert value of the immediate alert service
References at_ble_characteristic_changed_t::char_handle, at_ble_characteristic_changed_t::char_new_value, and INVALID_IAS_PARAM.
Referenced by pxp_reporter_char_changed_handler().
void init_immediate_alert_service | ( | gatt_service_handler_t * | immediate_alert_serv | ) |
Initialize the Immediate alert service with default values.
[in] | gatt_service_handler_t | the service info which has handle range,uuid and characteristic array fields |
Initialize the Immediate alert service with default values.
References ALERT_LEVEL_CHAR_UUID, AT_BLE_ATTR_NO_PERMISSIONS, AT_BLE_ATTR_WRITABLE_NO_AUTHN_NO_AUTHR, AT_BLE_ATTR_WRITABLE_REQ_AUTHN_NO_AUTHR, AT_BLE_CHAR_WRITE_WITHOUT_RESPONSE, AT_BLE_UUID_16, immediate_alert_initial_value, and IMMEDIATE_ALERT_SERVICE_UUID.
Referenced by pxp_service_init().