Proximity Reporter Profile declarations.
Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.
#include "ble_manager.h"
Macros | |
#define | ADV_DATA_LEN (18) |
ADV_DATA_LEN. More... | |
#define | ADV_TYPE_LEN (0x1) |
ADV_TYPE_LEN. More... | |
#define | APP_PXP_ADV_TIMEOUT (655) |
APP_PXP_ADV_TIMEOUT Advertising time-out between 0x0001 and 0x028F in seconds, 0x0000 disables time-out. More... | |
#define | APP_PXP_FAST_ADV (1600) |
APP_PXP_FAST_ADV between 0x0020 and 0x4000 in 0.625 ms units (20ms to 10.24s). More... | |
#define | IAL_ADV_DATA_UUID_LEN (2) |
IAL_ADV_DATA_UUID_LEN the size of IAL service uuid. More... | |
#define | IAL_ADV_DATA_UUID_TYPE (0x3) |
IAL_ADV_DATA_UUID_TYPE the total sizeof IAL service uuid. More... | |
#define | LL_ADV_DATA_UUID_LEN (2) |
LL_ADV_DATA_UUID_LEN the size of LL service uuid. More... | |
#define | LL_ADV_DATA_UUID_TYPE (0x3) |
LL_ADV_DATA_UUID_TYPE the total sizeof LL service uuid. More... | |
#define | PATHLOSS |
#define | PATHLOSS_VALUE 1 |
PATHLOSS which defines if the user wants pathloss functionality. More... | |
#define | PXP_ADV_DATA_NAME_DATA ("ATMEL-PXP") |
#define | PXP_ADV_DATA_NAME_LEN (9) |
PXP_ADV_DATA_NAME_LEN the length of the device name. More... | |
#define | PXP_ADV_DATA_NAME_TYPE (0x9) |
PXP_ADV_DATA_NAME_TYPE the gap ad data type. More... | |
#define | SCAN_RESP_LEN (10) |
scan_resp_len is the length of the scan response data More... | |
#define | TXP_ADV_DATA_UUID_LEN (2) |
TXP_ADV_DATA_UUID_LEN the size of TXP service uuid. More... | |
#define | TXP_ADV_DATA_UUID_TYPE (0x3) |
TXP_ADV_DATA_UUID_TYPE the total sizeof TXP service uuid. More... | |
Typedefs | |
typedef void(* | reporter_callback_t )(uint8_t) |
typedef void(* | reporter_state_callback_t )(bool) |
Functions | |
void | pxp_reporter_adv (void) |
sets the advertisement data and starts advertisement More... | |
at_ble_status_t | pxp_reporter_char_changed_handler (void *params) |
character changed handler More... | |
at_ble_status_t | pxp_reporter_connected_state_handler (void *params) |
connection state handler More... | |
at_ble_status_t | pxp_reporter_disconnect_event_handler (void *params) |
disconnection event handler More... | |
void | pxp_reporter_init (void *param) |
Initialize the profile, includes all initializations and start up routines of the profiles. More... | |
at_ble_status_t | pxp_service_define (void) |
profile services definition to the attribute data base More... | |
void | pxp_service_init (void) |
Initialize the services of the profile. More... | |
void | register_linkloss_handler (reporter_callback_t linkloss_fn) |
function which register the application alerting function for linkloss to the profile More... | |
void | register_pathloss_handler (reporter_callback_t pathloss_fn) |
function which register the application alerting function for pathloss to the profile More... | |
void | register_state_handler (reporter_state_callback_t state_fn) |
function which register the application state call back handler More... | |
#define ADV_DATA_LEN (18) |
ADV_DATA_LEN.
#define ADV_TYPE_LEN (0x1) |
ADV_TYPE_LEN.
#define APP_PXP_ADV_TIMEOUT (655) |
APP_PXP_ADV_TIMEOUT Advertising time-out between 0x0001 and 0x028F in seconds, 0x0000 disables time-out.
Referenced by pxp_reporter_adv(), and pxp_reporter_disconnect_event_handler().
#define APP_PXP_FAST_ADV (1600) |
APP_PXP_FAST_ADV between 0x0020 and 0x4000 in 0.625 ms units (20ms to 10.24s).
Referenced by pxp_reporter_adv(), and pxp_reporter_disconnect_event_handler().
#define IAL_ADV_DATA_UUID_LEN (2) |
IAL_ADV_DATA_UUID_LEN the size of IAL service uuid.
#define IAL_ADV_DATA_UUID_TYPE (0x3) |
IAL_ADV_DATA_UUID_TYPE the total sizeof IAL service uuid.
#define LL_ADV_DATA_UUID_LEN (2) |
LL_ADV_DATA_UUID_LEN the size of LL service uuid.
#define LL_ADV_DATA_UUID_TYPE (0x3) |
LL_ADV_DATA_UUID_TYPE the total sizeof LL service uuid.
#define PATHLOSS |
#define PATHLOSS_VALUE 1 |
PATHLOSS which defines if the user wants pathloss functionality.
#define PXP_ADV_DATA_NAME_DATA ("ATMEL-PXP") |
#define PXP_ADV_DATA_NAME_LEN (9) |
PXP_ADV_DATA_NAME_LEN the length of the device name.
#define PXP_ADV_DATA_NAME_TYPE (0x9) |
PXP_ADV_DATA_NAME_TYPE the gap ad data type.
#define SCAN_RESP_LEN (10) |
scan_resp_len is the length of the scan response data
#define TXP_ADV_DATA_UUID_LEN (2) |
TXP_ADV_DATA_UUID_LEN the size of TXP service uuid.
#define TXP_ADV_DATA_UUID_TYPE (0x3) |
TXP_ADV_DATA_UUID_TYPE the total sizeof TXP service uuid.
typedef void(* reporter_callback_t)(uint8_t) |
typedef void(* reporter_state_callback_t)(bool) |
void pxp_reporter_adv | ( | void | ) |
sets the advertisement data and starts advertisement
[in] | void |
sets the advertisement data and starts advertisement
References APP_PXP_ADV_TIMEOUT, APP_PXP_FAST_ADV, AT_BLE_ADV_FP_ANY, AT_BLE_ADV_GEN_DISCOVERABLE, at_ble_adv_start(), AT_BLE_ADV_TYPE_UNDIRECTED, AT_BLE_SUCCESS, ble_advertisement_data_set(), and DBG_LOG.
Referenced by pxp_reporter_init().
at_ble_status_t pxp_reporter_char_changed_handler | ( | void * | params | ) |
character changed handler
[in] | at_ble_characteristic_changed_t | which includes handle,new value |
character changed handler
References AT_BLE_SUCCESS, ias_set_alert_value(), INVALID_IAS_PARAM, INVALID_LLS_PARAM, linkloss_current_alert_level, lls_set_alert_value(), pathloss_alert_value, and pathloss_cb.
at_ble_status_t pxp_reporter_connected_state_handler | ( | void * | params | ) |
connection state handler
[in] | at_ble_connected_t | which includes the connection parameters like handle |
connection state handler
References ALL_UNUSED, at_ble_characteristic_value_get(), AT_BLE_SUCCESS, connected_cb, DBG_LOG, linkloss_current_alert_level, and pathloss_alert_value.
at_ble_status_t pxp_reporter_disconnect_event_handler | ( | void * | params | ) |
disconnection event handler
[in] | at_ble_disconencted_t | which includes the connection parameters like handle,reason for disconnection |
disconnection event handler
References ALL_UNUSED, APP_PXP_ADV_TIMEOUT, APP_PXP_FAST_ADV, AT_BLE_ADV_FP_ANY, AT_BLE_ADV_GEN_DISCOVERABLE, at_ble_adv_start(), AT_BLE_ADV_TYPE_UNDIRECTED, AT_BLE_SUCCESS, DBG_LOG, linkloss_cb, and linkloss_current_alert_level.
void pxp_reporter_init | ( | void * | param | ) |
Initialize the profile, includes all initializations and start up routines of the profiles.
[in] | void |
Initialize the profile, includes all initializations and start up routines of the profiles.
References ALL_UNUSED, BLE_GAP_EVENT_TYPE, BLE_GATT_SERVER_EVENT_TYPE, ble_mgr_events_callback_handler(), pxp_reporter_adv(), pxp_service_define(), pxp_service_init(), and REGISTER_CALL_BACK.
Referenced by main().
at_ble_status_t pxp_service_define | ( | void | ) |
profile services definition to the attribute data base
[in] | void |
profile services definition to the attribute data base
References AT_BLE_SUCCESS, DBG_LOG, DBG_LOG_DEV, ias_primary_service_define(), lls_primary_service_define(), and txps_primary_service_define().
Referenced by pxp_reporter_init().
void pxp_service_init | ( | void | ) |
Initialize the services of the profile.
[in] | void |
Initialize the services of the profile.
Initializing the mandatory linkloss service of proximity reporter
Initializing the optional services for pathloss feature of proximity reporter
References init_immediate_alert_service(), init_linkloss_service(), and init_tx_power_service().
Referenced by pxp_reporter_init().
void register_linkloss_handler | ( | reporter_callback_t | linkloss_fn | ) |
function which register the application alerting function for linkloss to the profile
[in] | call | back function of the application for linkloss |
function which register the application alerting function for linkloss to the profile
References linkloss_cb.
Referenced by main().
void register_pathloss_handler | ( | reporter_callback_t | pathloss_fn | ) |
function which register the application alerting function for pathloss to the profile
[in] | call | back function of the application for pathloss |
function which register the application alerting function for pathloss to the profile
References pathloss_cb.
Referenced by main().
void register_state_handler | ( | reporter_state_callback_t | state_fn | ) |
function which register the application state call back handler
[in] | call | back function of the application for connection state |
References connected_cb.
Referenced by main().