NV component implementation.
Copyright (c) 2018 Microchip Technology Inc. and its subsidiaries.
#include "S_Nv_Bindings.h"
#include "S_Nv_Init.h"
#include "S_Nv.h"
#include "pdsDataServer.h"
#include "D_Nv.h"
#include "assert.h"
#include <compiler.h>
#include "wlPdsMemIds.h"
#include "string.h"
#include "sysTimer.h"
Data Structures | |
struct | BlockHeader_t |
struct | BlockHeaderSNv1_t |
struct | Item_t |
Structure used to store where to find an item. More... | |
struct | SectorHeader_t |
16 byte sector header used in flash located at the start of the active sector. More... | |
struct | SectorHeaderSnv1_t |
16 byte sector header used in flash located at the start of the active sector. More... | |
Macros | |
#define | BLOCK_HEADER_SIZE ((uint16_t) sizeof(BlockHeader_t)) |
The size of the block header. More... | |
#define | COMPACT_ITEM_DELAY_MS 3000u |
Delay before performing a compact item operation. More... | |
#define | COMPACT_ITEM_THRESHOLD 100u |
Perform a compact item operation if the number of partial writes is larger than this. More... | |
#define | COMPACT_SECTOR_DELAY_MS 10000u |
Delay before performing a preemptive compact operation. More... | |
#define | COMPID "S_Nv" |
#define | ERASE_SECTOR_DELAY_MS 7000u |
Delay before erasing a sector. More... | |
#define | EVENT_COMPACT_ITEM 2u |
#define | EVENT_COMPACT_SECTOR 1u |
#define | EVENT_ERASE_SECTOR 0u |
Timer event used to erase a sector. More... | |
#define | FIRST_SECTOR D_NV_FIRST_SECTOR |
#define | INITIAL_SECTOR_SEQUENCE_NUMBER 0xFFFFFFFEuL |
The sequence number to use for the initial sector. More... | |
#define | ITEMS_AREA_START_ADDRESS NVMCTRL_ROW_SIZE |
#define | MAX_ITEM_COUNT PDS_MAX_ID |
The maximum number of items. More... | |
#define | MAX_ITEM_LENGTH 2048u |
The maxumum length of an item. More... | |
#define | PERSISTENT_NV_ITEMS_APPLICATION 0xFFFu |
#define | PREEMPTIVE_COMPACT_SECTOR_THRESHOLD (MAX_ITEM_LENGTH + BLOCK_HEADER_SIZE) |
Perform a compact sector operation with a delay if the sector has less free space than this. More... | |
#define | ROW_SIZE NVMCTRL_ROW_SIZE |
#define | SECTOR_COUNT D_NV_SECTOR_COUNT |
#define | SECTOR_HEADER_SIZE ((uint16_t) sizeof(SectorHeader_t)) |
The size of the sector header. More... | |
#define | SECTOR_SIZE D_NV_SECTOR_SIZE |
Typedefs | |
typedef struct BlockHeader_t | BlockHeader_t |
typedef struct BlockHeaderSNv1_t | BlockHeaderSNv1_t |
typedef struct Item_t | Item_t |
Structure used to store where to find an item. More... | |
typedef struct SectorHeader_t | SectorHeader_t |
16 byte sector header used in flash located at the start of the active sector. More... | |
typedef struct SectorHeaderSnv1_t | SectorHeaderSnv1_t |
16 byte sector header used in flash located at the start of the active sector. More... | |
Enumerations | |
enum | ItemAlignment_t { ITEM_NO_ALIGNMENT, ITEM_16BYTE_ALIGNMENT, ITEM_64BYTE_ALIGNMENT } |
Enumerations for Snv Item alignments. More... | |
enum | SnvRevisioin_t { SNV_REV_1 = 1, SNV_REV_2 } |
Enumerations for Snv revisions. More... | |
Functions | |
static S_Nv_ReturnValue_t | CompactItem (void) |
static void | compactItemTimerFired (struct SYS_Timer_t *timer) |
Compact item timer callback. More... | |
static bool | CompactSector (void) |
static void | CompactSectorIfNeeded (uint16_t immediateThreshold) |
static void | compactSectorTimerFired (struct SYS_Timer_t *timer) |
Compact sector timer callback. More... | |
static uint16_t | ComputeCrc (uint8_t *pData, uint16_t length, uint16_t crc) |
static uint16_t | ComputeDataCrc (uint8_t sourceSector, uint16_t blockPointer, BlockHeader_t *pBlockHeader) |
static uint16_t | ComputeHeaderCrc (BlockHeader_t *pBlockHeader) |
static uint16_t | ComputeHeaderCrcSnv1 (BlockHeaderSNv1_t *pBlockHeader) |
static uint16_t | ComputeSectorHeaderCrc (SectorHeader_t *pSectorHeader) |
static Item_t * | CreateItemCache (uint16_t id) |
Return a pointer to a cache for a new item. More... | |
static void | DeleteItemCache (uint16_t id) |
Removes the specified item from the cache array. More... | |
static bool | EraseSector (void) |
static void | eraseSectorTimerFired (struct SYS_Timer_t *timer) |
Erase sector timer callback. More... | |
static uint16_t | FindItem (uint16_t id) |
Return a pointer to the last written block for the item. More... | |
static Item_t * | FindItemCache (uint16_t id) |
Return a pointer to the cache for the item. More... | |
static bool | GatherData (uint8_t sourceSector, uint16_t lastBlockPointer, uint16_t offset, uint16_t length, void *pData) |
Gather data from an item for a read or compact operation. More... | |
static bool | IsEmpty (uint8_t *pData, uint16_t length) |
Check if the RAM buffer contains all 0xFF values (flash erased) More... | |
static bool | IsPersistent (uint16_t id) |
static void | LoadSector (SnvRevisioin_t revisionNumber) |
static bool | PowerSupplyTooLow () |
Check the power supply. More... | |
void | S_Nv_CompactSector_Impl (void) |
S_Nv_ReturnValue_t | S_Nv_Delete_Impl (S_Nv_ItemId_t id) |
Interface function, see S_Nv_Delete. More... | |
void | S_Nv_EarlyInit (void) |
Initializes the internal flash service for early access. More... | |
S_Nv_ReturnValue_t | S_Nv_EraseAll_Impl (bool includingPersistentItems) |
Interface function, see S_Nv_EraseAll. More... | |
void | S_Nv_Init (void) |
Initializes the component and tells which items are persistent against S_Nv_EraseAll(FALSE). More... | |
bool | S_Nv_IsItemAvailable_Impl (S_Nv_ItemId_t id) |
Interface function, see S_Nv_IsItemAvailable. More... | |
S_Nv_ReturnValue_t | S_Nv_ItemInit_Impl (S_Nv_ItemId_t id, uint16_t itemLength, void *pDefaultData) |
Interface function, see S_Nv_ItemInit. More... | |
uint16_t | S_Nv_ItemLength_Impl (S_Nv_ItemId_t id) |
Interface function, see S_Nv_ItemLength. More... | |
S_Nv_ReturnValue_t | S_Nv_Read_Impl (S_Nv_ItemId_t id, uint16_t offset, uint16_t dataLength, void *pData) |
Interface function, see S_Nv_Read. More... | |
void | S_Nv_SetPowerSupplyCheckingFunction_Impl (S_Nv_PowerSupplyCheckingFunction_t pf) |
Interface function, see S_Nv_SetPowerSupplyCheckingFunction. More... | |
S_Nv_ReturnValue_t | S_Nv_Write_Impl (S_Nv_ItemId_t id, uint16_t offset, uint16_t dataLength, void *pData) |
Interface function, see S_Nv_Write. More... | |
static bool | SmartCompacting (uint8_t *compactBlock, uint16_t curItemLength) |
static void | UpdateSectorHead (uint16_t increment, ItemAlignment_t itemAlignment) |
Update the sector head with increment as per Alignement. More... | |
static bool | WriteAndCheck (uint16_t offset, uint8_t *pData, uint16_t length) |
static bool | WriteBlockHeader (BlockHeader_t *pBlockHeader) |
static bool | WriteDataBlockAndHeader (BlockHeader_t *pBlockHeader, uint8_t *pData) |
static bool | WriteSectorHeader (uint32_t sequenceNumber) |
Variables | |
static uint16_t | compactBlockOffset = 0u |
static SYS_Timer_t | compactItemTimer |
static SYS_Timer_t | compactSectorTimer |
static uint16_t | currentCompactLength = 0u |
static uint8_t | dataBlock [ROW_SIZE] |
static SYS_Timer_t | eraseSectorTimer |
static uint16_t | s_compactItemId = 0x0000u |
The item to perform a compact operation on and the length of this item. More... | |
static uint16_t | s_compactItemLength = 0x0000u |
static bool | s_earlyInitDone = false |
Check if the early init function is called already. More... | |
static Item_t | s_itemCache [MAX_ITEM_COUNT] |
static uint8_t | s_itemCount = 0u |
The number of read, and thus cached, items. More... | |
static uint16_t | s_nextPageAddressAfterCompact |
static const uint16_t | s_persistentItems [] = {PERSISTENT_NV_ITEMS_APPLICATION} |
static S_Nv_PowerSupplyCheckingFunction_t | s_powerSupplyCheckingFunction = NULL |
Callback function called before changing flash contents. More... | |
static uint8_t | s_sector |
The active sector. More... | |
static uint16_t | s_sectorHead |
Location of the first unprogrammed byte in the active sector. More... | |
static uint8_t | s_sectorToErase = 0xFFu |
The sector to erase in the EVENT_ERASE_SECTOR handler. More... | |
#define BLOCK_HEADER_SIZE ((uint16_t) sizeof(BlockHeader_t)) |
The size of the block header.
same for Snv rev1
Referenced by CompactItem(), CompactSector(), GatherData(), LoadSector(), S_Nv_Delete_Impl(), S_Nv_ItemInit_Impl(), S_Nv_ItemLength_Impl(), S_Nv_Write_Impl(), WriteBlockHeader(), and WriteDataBlockAndHeader().
#define COMPACT_ITEM_DELAY_MS 3000u |
Delay before performing a compact item operation.
Referenced by S_Nv_Write_Impl().
#define COMPACT_ITEM_THRESHOLD 100u |
Perform a compact item operation if the number of partial writes is larger than this.
Referenced by S_Nv_Write_Impl().
#define COMPACT_SECTOR_DELAY_MS 10000u |
Delay before performing a preemptive compact operation.
Referenced by CompactSectorIfNeeded().
#define COMPID "S_Nv" |
#define ERASE_SECTOR_DELAY_MS 7000u |
Delay before erasing a sector.
Referenced by S_Nv_Init().
#define EVENT_COMPACT_ITEM 2u |
#define EVENT_COMPACT_SECTOR 1u |
#define EVENT_ERASE_SECTOR 0u |
Timer event used to erase a sector.
#define FIRST_SECTOR D_NV_FIRST_SECTOR |
Referenced by CompactSector(), S_Nv_EarlyInit(), and S_Nv_EraseAll_Impl().
#define INITIAL_SECTOR_SEQUENCE_NUMBER 0xFFFFFFFEuL |
The sequence number to use for the initial sector.
Referenced by S_Nv_EarlyInit().
#define ITEMS_AREA_START_ADDRESS NVMCTRL_ROW_SIZE |
Referenced by EraseSector(), and LoadSector().
#define MAX_ITEM_COUNT PDS_MAX_ID |
The maximum number of items.
Referenced by CreateItemCache(), and S_Nv_ItemInit_Impl().
#define MAX_ITEM_LENGTH 2048u |
The maxumum length of an item.
Referenced by S_Nv_ItemInit_Impl().
#define PERSISTENT_NV_ITEMS_APPLICATION 0xFFFu |
#define PREEMPTIVE_COMPACT_SECTOR_THRESHOLD (MAX_ITEM_LENGTH + BLOCK_HEADER_SIZE) |
Perform a compact sector operation with a delay if the sector has less free space than this.
Referenced by CompactSectorIfNeeded().
#define ROW_SIZE NVMCTRL_ROW_SIZE |
Referenced by CompactItem(), CompactSector(), SmartCompacting(), and WriteDataBlockAndHeader().
#define SECTOR_COUNT D_NV_SECTOR_COUNT |
Referenced by CompactSector(), S_Nv_EarlyInit(), and S_Nv_EraseAll_Impl().
#define SECTOR_HEADER_SIZE ((uint16_t) sizeof(SectorHeader_t)) |
The size of the sector header.
Referenced by CompactSector(), S_Nv_EarlyInit(), and WriteSectorHeader().
#define SECTOR_SIZE D_NV_SECTOR_SIZE |
Referenced by CompactSectorIfNeeded(), EraseSector(), and LoadSector().
typedef struct BlockHeader_t BlockHeader_t |
typedef struct BlockHeaderSNv1_t BlockHeaderSNv1_t |
typedef struct SectorHeader_t SectorHeader_t |
16 byte sector header used in flash located at the start of the active sector.
typedef struct SectorHeaderSnv1_t SectorHeaderSnv1_t |
16 byte sector header used in flash located at the start of the active sector.
enum ItemAlignment_t |
enum SnvRevisioin_t |
|
static |
References BLOCK_HEADER_SIZE, BlockHeader_t::blockLength, BlockHeader_t::blockOffset, CompactSectorIfNeeded(), D_Nv_Read, dataBlock, FindItemCache(), GatherData(), ITEM_64BYTE_ALIGNMENT, BlockHeader_t::itemLength, Item_t::lastBlock, PowerSupplyTooLow(), BlockHeader_t::previousBlock, ROW_SIZE, s_compactItemId, s_compactItemLength, S_Nv_ReturnValue_Failure, S_Nv_ReturnValue_Ok, S_Nv_ReturnValue_PowerSupplyTooLow, s_sector, s_sectorHead, UpdateSectorHead(), WriteAndCheck(), and BlockHeader_t::writeCount.
Referenced by compactItemTimerFired(), and S_Nv_ItemInit_Impl().
|
static |
|
static |
References BLOCK_HEADER_SIZE, BlockHeader_t::blockLength, BlockHeader_t::blockOffset, compactBlockOffset, ComputeDataCrc(), ComputeHeaderCrc(), currentCompactLength, D_Nv_Read, dataBlock, BlockHeader_t::dataCrc, EraseSector(), FIRST_SECTOR, GatherData(), BlockHeader_t::headerCrc, ITEM_64BYTE_ALIGNMENT, ITEM_NO_ALIGNMENT, BlockHeader_t::itemLength, Item_t::lastBlock, BlockHeader_t::previousBlock, ROW_SIZE, s_compactItemId, s_compactItemLength, s_itemCount, s_nextPageAddressAfterCompact, s_sector, s_sectorHead, s_sectorToErase, SECTOR_COUNT, SECTOR_HEADER_SIZE, SectorHeader_t::sequenceNumber, SmartCompacting(), SYS_TimerStart(), SYS_TimerStop(), UpdateSectorHead(), WriteAndCheck(), BlockHeader_t::writeCount, and WriteSectorHeader().
Referenced by CompactSectorIfNeeded(), compactSectorTimerFired(), LoadSector(), S_Nv_CompactSector_Impl(), and S_Nv_EraseAll_Impl().
|
static |
References COMPACT_SECTOR_DELAY_MS, CompactSector(), compactSectorTimerFired(), SYS_Timer_t::handler, SYS_Timer_t::interval, SYS_Timer_t::mode, PREEMPTIVE_COMPACT_SECTOR_THRESHOLD, s_sectorHead, SECTOR_SIZE, SYS_TIMER_INTERVAL_MODE, SYS_TimerStarted(), and SYS_Timer_t::timeout.
Referenced by CompactItem(), S_Nv_Delete_Impl(), S_Nv_ItemInit_Impl(), and S_Nv_Write_Impl().
|
static |
Compact sector timer callback.
References CompactSector(), and PowerSupplyTooLow().
Referenced by CompactSectorIfNeeded().
|
static |
Referenced by ComputeDataCrc(), ComputeHeaderCrc(), ComputeHeaderCrcSnv1(), ComputeSectorHeaderCrc(), and WriteDataBlockAndHeader().
|
static |
References BlockHeader_t::blockLength, BlockHeader_t::blockOffset, ComputeCrc(), dataBlock, and GatherData().
Referenced by CompactSector(), and LoadSector().
|
static |
References ComputeCrc(), and BlockHeader_t::headerCrc.
Referenced by CompactSector(), LoadSector(), WriteBlockHeader(), and WriteDataBlockAndHeader().
|
static |
References ComputeCrc(), BlockHeaderSNv1_t::headerCrc, and BlockHeaderSNv1_t::isActive.
Referenced by LoadSector().
|
static |
References ComputeCrc(), and SectorHeader_t::headerCrc.
Referenced by S_Nv_EarlyInit(), and WriteSectorHeader().
|
static |
Return a pointer to a cache for a new item.
id | The id to create cache for |
References FindItemCache(), Item_t::id, MAX_ITEM_COUNT, and s_itemCount.
Referenced by LoadSector(), and S_Nv_ItemInit_Impl().
|
static |
Removes the specified item from the cache array.
id | The id to delete the cache for |
References FindItemCache(), and s_itemCount.
Referenced by LoadSector(), S_Nv_Delete_Impl(), and S_Nv_EraseAll_Impl().
|
static |
References D_Nv_EraseSector, D_Nv_IsEmpty, ITEMS_AREA_START_ADDRESS, s_sector, s_sectorHead, and SECTOR_SIZE.
Referenced by CompactSector(), and S_Nv_EarlyInit().
|
static |
Erase sector timer callback.
References D_Nv_EraseSector, PowerSupplyTooLow(), and s_sectorToErase.
Referenced by S_Nv_Init().
|
static |
Return a pointer to the last written block for the item.
id | The id to find |
References FindItemCache(), and Item_t::lastBlock.
Referenced by S_Nv_Delete_Impl(), S_Nv_IsItemAvailable_Impl(), S_Nv_ItemInit_Impl(), S_Nv_ItemLength_Impl(), and S_Nv_Read_Impl().
|
static |
Return a pointer to the cache for the item.
id | The id to find |
References Item_t::id, Item_t::lastBlock, and s_itemCount.
Referenced by CompactItem(), CreateItemCache(), DeleteItemCache(), FindItem(), LoadSector(), and S_Nv_Write_Impl().
|
static |
Gather data from an item for a read or compact operation.
sourceSector | |
lastBlockPointer | Pointer to the last block written for the item |
offset | The start of the range of bytes to copy from the item |
length | The size of the range of bytes to copy from the item |
pData | Pointer to destination buffer in RAM for a read operation. NULL for a compact operation. |
This function is used by both the read and the compact operation.
References BLOCK_HEADER_SIZE, BlockHeader_t::blockLength, BlockHeader_t::blockOffset, D_Nv_Read, and BlockHeader_t::previousBlock.
Referenced by CompactItem(), CompactSector(), ComputeDataCrc(), and S_Nv_Read_Impl().
|
static |
Check if the RAM buffer contains all 0xFF values (flash erased)
pData | The buffer to check |
length | The length of the buffer |
Referenced by LoadSector().
|
static |
References s_persistentItems.
Referenced by S_Nv_EraseAll_Impl().
|
static |
References BLOCK_HEADER_SIZE, BlockHeaderSNv1_t::blockLength, BlockHeader_t::blockLength, CompactSector(), ComputeDataCrc(), ComputeHeaderCrc(), ComputeHeaderCrcSnv1(), CreateItemCache(), D_Nv_Read, BlockHeader_t::dataCrc, DeleteItemCache(), FindItemCache(), BlockHeaderSNv1_t::headerCrc, BlockHeader_t::headerCrc, BlockHeaderSNv1_t::id, BlockHeader_t::id, BlockHeaderSNv1_t::isActive, IsEmpty(), ITEM_16BYTE_ALIGNMENT, ITEM_64BYTE_ALIGNMENT, ITEM_NO_ALIGNMENT, BlockHeaderSNv1_t::itemLength, BlockHeader_t::itemLength, ITEMS_AREA_START_ADDRESS, Item_t::lastBlock, SectorHeader_t::nextPageAddressAfterCompact, s_sector, s_sectorHead, SECTOR_SIZE, SNV_REV_1, SNV_REV_2, and UpdateSectorHead().
Referenced by S_Nv_EarlyInit().
|
static |
Check the power supply.
References s_powerSupplyCheckingFunction.
Referenced by CompactItem(), compactSectorTimerFired(), eraseSectorTimerFired(), S_Nv_Delete_Impl(), S_Nv_EraseAll_Impl(), S_Nv_ItemInit_Impl(), and S_Nv_Write_Impl().
void S_Nv_CompactSector_Impl | ( | void | ) |
References CompactSector().
S_Nv_ReturnValue_t S_Nv_Delete_Impl | ( | S_Nv_ItemId_t | id | ) |
Interface function, see S_Nv_Delete.
References BLOCK_HEADER_SIZE, BlockHeader_t::blockLength, BlockHeader_t::blockOffset, CompactSectorIfNeeded(), DeleteItemCache(), FindItem(), BlockHeader_t::id, BlockHeader_t::itemLength, PowerSupplyTooLow(), BlockHeader_t::previousBlock, S_Nv_ReturnValue_DoesNotExist, S_Nv_ReturnValue_Failure, S_Nv_ReturnValue_Ok, S_Nv_ReturnValue_PowerSupplyTooLow, WriteBlockHeader(), and BlockHeader_t::writeCount.
void S_Nv_EarlyInit | ( | void | ) |
Initializes the internal flash service for early access.
References ComputeSectorHeaderCrc(), D_Nv_Read, EraseSector(), FIRST_SECTOR, SectorHeader_t::headerCrc, INITIAL_SECTOR_SEQUENCE_NUMBER, SectorHeaderSnv1_t::isActive, LoadSector(), s_earlyInitDone, s_itemCount, s_nextPageAddressAfterCompact, s_sector, SECTOR_COUNT, SECTOR_HEADER_SIZE, SectorHeader_t::sequenceNumber, SectorHeader_t::sequenceParity, SectorHeader_t::signature, SNV_REV_1, SNV_REV_2, and WriteSectorHeader().
Referenced by S_Nv_Init().
S_Nv_ReturnValue_t S_Nv_EraseAll_Impl | ( | bool | includingPersistentItems | ) |
Interface function, see S_Nv_EraseAll.
Important: EraseAll leaves the file system in a non-working state if persistent items are also deleted. This is because all sectors are deleted without initializing a new one or even clearing the cache, so reinitialization of the driver is needed.
References CompactSector(), D_Nv_EraseSector, DeleteItemCache(), FIRST_SECTOR, Item_t::id, IsPersistent(), PowerSupplyTooLow(), s_itemCount, S_Nv_ReturnValue_Ok, S_Nv_ReturnValue_PowerSupplyTooLow, and SECTOR_COUNT.
void S_Nv_Init | ( | void | ) |
Initializes the component and tells which items are persistent against S_Nv_EraseAll(FALSE).
References ERASE_SECTOR_DELAY_MS, eraseSectorTimerFired(), SYS_Timer_t::handler, SYS_Timer_t::interval, SYS_Timer_t::mode, s_earlyInitDone, S_Nv_EarlyInit(), SYS_TIMER_INTERVAL_MODE, and SYS_Timer_t::timeout.
Referenced by PDS_Init().
bool S_Nv_IsItemAvailable_Impl | ( | S_Nv_ItemId_t | id | ) |
Interface function, see S_Nv_IsItemAvailable.
Important: This will check whether the item is found in the storage area
References FindItem().
S_Nv_ReturnValue_t S_Nv_ItemInit_Impl | ( | S_Nv_ItemId_t | id, |
uint16_t | itemLength, | ||
void * | pDefaultData | ||
) |
Interface function, see S_Nv_ItemInit.
References BLOCK_HEADER_SIZE, BlockHeader_t::blockLength, BlockHeader_t::blockOffset, CompactItem(), CompactSectorIfNeeded(), CreateItemCache(), FindItem(), BlockHeader_t::id, BlockHeader_t::itemLength, Item_t::lastBlock, MAX_ITEM_COUNT, MAX_ITEM_LENGTH, PowerSupplyTooLow(), BlockHeader_t::previousBlock, s_compactItemId, s_compactItemLength, s_itemCount, S_Nv_ItemLength(), S_Nv_Read(), S_Nv_ReturnValue_DidNotExist, S_Nv_ReturnValue_Failure, S_Nv_ReturnValue_Ok, S_Nv_ReturnValue_PowerSupplyTooLow, s_sectorHead, BlockHeader_t::writeCount, and WriteDataBlockAndHeader().
uint16_t S_Nv_ItemLength_Impl | ( | S_Nv_ItemId_t | id | ) |
Interface function, see S_Nv_ItemLength.
References BLOCK_HEADER_SIZE, D_Nv_Read, FindItem(), BlockHeader_t::itemLength, and s_sector.
S_Nv_ReturnValue_t S_Nv_Read_Impl | ( | S_Nv_ItemId_t | id, |
uint16_t | offset, | ||
uint16_t | dataLength, | ||
void * | pData | ||
) |
Interface function, see S_Nv_Read.
References FindItem(), GatherData(), S_Nv_ReturnValue_BeyondEnd, S_Nv_ReturnValue_DoesNotExist, S_Nv_ReturnValue_Ok, and s_sector.
void S_Nv_SetPowerSupplyCheckingFunction_Impl | ( | S_Nv_PowerSupplyCheckingFunction_t | pf | ) |
Interface function, see S_Nv_SetPowerSupplyCheckingFunction.
References s_powerSupplyCheckingFunction.
S_Nv_ReturnValue_t S_Nv_Write_Impl | ( | S_Nv_ItemId_t | id, |
uint16_t | offset, | ||
uint16_t | dataLength, | ||
void * | pData | ||
) |
Interface function, see S_Nv_Write.
References BLOCK_HEADER_SIZE, BlockHeader_t::blockLength, BlockHeader_t::blockOffset, COMPACT_ITEM_DELAY_MS, COMPACT_ITEM_THRESHOLD, compactItemTimerFired(), CompactSectorIfNeeded(), D_Nv_Read, FindItemCache(), SYS_Timer_t::handler, BlockHeader_t::id, SYS_Timer_t::interval, BlockHeader_t::itemLength, Item_t::lastBlock, SYS_Timer_t::mode, PowerSupplyTooLow(), BlockHeader_t::previousBlock, s_compactItemId, s_compactItemLength, S_Nv_ReturnValue_BeyondEnd, S_Nv_ReturnValue_DoesNotExist, S_Nv_ReturnValue_Failure, S_Nv_ReturnValue_Ok, S_Nv_ReturnValue_PowerSupplyTooLow, s_sector, s_sectorHead, SYS_TIMER_INTERVAL_MODE, SYS_TimerStarted(), SYS_Timer_t::timeout, BlockHeader_t::writeCount, and WriteDataBlockAndHeader().
|
static |
References compactBlockOffset, currentCompactLength, dataBlock, ITEM_NO_ALIGNMENT, ROW_SIZE, s_sectorHead, UpdateSectorHead(), and WriteAndCheck().
Referenced by CompactSector().
|
static |
Update the sector head with increment as per Alignement.
increment | The length updated |
References ITEM_16BYTE_ALIGNMENT, ITEM_64BYTE_ALIGNMENT, ITEM_NO_ALIGNMENT, and s_sectorHead.
Referenced by CompactItem(), CompactSector(), LoadSector(), SmartCompacting(), WriteBlockHeader(), and WriteDataBlockAndHeader().
|
static |
References D_Nv_IsEqual, D_Nv_Write, and s_sector.
Referenced by CompactItem(), CompactSector(), SmartCompacting(), WriteBlockHeader(), WriteDataBlockAndHeader(), and WriteSectorHeader().
|
static |
References BLOCK_HEADER_SIZE, ComputeHeaderCrc(), D_Nv_IsEmpty, dataBlock, BlockHeader_t::dataCrc, BlockHeader_t::headerCrc, ITEM_64BYTE_ALIGNMENT, s_sector, s_sectorHead, UpdateSectorHead(), and WriteAndCheck().
Referenced by S_Nv_Delete_Impl().
|
static |
References BLOCK_HEADER_SIZE, BlockHeader_t::blockLength, ComputeCrc(), ComputeHeaderCrc(), dataBlock, BlockHeader_t::dataCrc, BlockHeader_t::headerCrc, ITEM_64BYTE_ALIGNMENT, MIN, ROW_SIZE, s_sectorHead, UpdateSectorHead(), and WriteAndCheck().
Referenced by S_Nv_ItemInit_Impl(), and S_Nv_Write_Impl().
|
static |
References ComputeSectorHeaderCrc(), SectorHeader_t::headerCrc, SectorHeader_t::nextPageAddressAfterCompact, s_nextPageAddressAfterCompact, SECTOR_HEADER_SIZE, SectorHeader_t::sequenceNumber, SectorHeader_t::sequenceParity, SectorHeader_t::signature, and WriteAndCheck().
Referenced by CompactSector(), and S_Nv_EarlyInit().
|
static |
Referenced by CompactSector(), and SmartCompacting().
|
static |
|
static |
|
static |
Referenced by CompactSector(), and SmartCompacting().
|
static |
Referenced by CompactItem(), CompactSector(), ComputeDataCrc(), SmartCompacting(), WriteBlockHeader(), and WriteDataBlockAndHeader().
|
static |
|
static |
The item to perform a compact operation on and the length of this item.
Referenced by CompactItem(), CompactSector(), S_Nv_ItemInit_Impl(), and S_Nv_Write_Impl().
|
static |
Referenced by CompactItem(), CompactSector(), S_Nv_ItemInit_Impl(), and S_Nv_Write_Impl().
Check if the early init function is called already.
Referenced by S_Nv_EarlyInit(), and S_Nv_Init().
|
static |
|
static |
The number of read, and thus cached, items.
Referenced by CompactSector(), CreateItemCache(), DeleteItemCache(), FindItemCache(), S_Nv_EarlyInit(), S_Nv_EraseAll_Impl(), and S_Nv_ItemInit_Impl().
|
static |
Referenced by CompactSector(), S_Nv_EarlyInit(), and WriteSectorHeader().
|
static |
Referenced by IsPersistent().
|
static |
Callback function called before changing flash contents.
Referenced by PowerSupplyTooLow(), and S_Nv_SetPowerSupplyCheckingFunction_Impl().
|
static |
The active sector.
Referenced by CompactItem(), CompactSector(), EraseSector(), LoadSector(), S_Nv_EarlyInit(), S_Nv_ItemLength_Impl(), S_Nv_Read_Impl(), S_Nv_Write_Impl(), WriteAndCheck(), and WriteBlockHeader().
|
static |
Location of the first unprogrammed byte in the active sector.
Referenced by CompactItem(), CompactSector(), CompactSectorIfNeeded(), EraseSector(), LoadSector(), S_Nv_ItemInit_Impl(), S_Nv_Write_Impl(), SmartCompacting(), UpdateSectorHead(), WriteBlockHeader(), and WriteDataBlockAndHeader().
|
static |
The sector to erase in the EVENT_ERASE_SECTOR handler.
Referenced by CompactSector(), and eraseSectorTimerFired().