Data Structures | |
struct | ip64_addrmap_entry |
Macros | |
#define | FLAGS_NONE 0 |
#define | FLAGS_RECYCLABLE 1 |
Functions | |
struct ip64_addrmap_entry * | ip64_addrmap_create (const uip_ip6addr_t *ip6addr, uint16_t ip6port, const uip_ip4addr_t *ip4addr, uint16_t ip4port, uint8_t protocol) |
Create a new address mapping from an IPv6 address/port, an IPv4 address/port, and a protocol number. More... | |
void | ip64_addrmap_init (void) |
Initialize the ip64_addrmap module. More... | |
struct ip64_addrmap_entry * | ip64_addrmap_list (void) |
Obtain the list of all address mappings. More... | |
struct ip64_addrmap_entry * | ip64_addrmap_lookup (const uip_ip6addr_t *ip6addr, uint16_t ip6port, const uip_ip4addr_t *ip4addr, uint16_t ip4port, uint8_t protocol) |
Look up an address mapping from inside the IPv6 network, given the IPv6 address/port, the IPv4 address/port, and the protocol. More... | |
struct ip64_addrmap_entry * | ip64_addrmap_lookup_port (uint16_t mappedport, uint8_t protocol) |
Look up an address mapping from the outside IPv4 network, given the mapped port number and protocol. More... | |
void | ip64_addrmap_set_lifetime (struct ip64_addrmap_entry *e, clock_time_t lifetime) |
Set the lifetime of an address mapping. More... | |
void | ip64_addrmap_set_recycleble (struct ip64_addrmap_entry *e) |
Mark an address mapping to be recyclable. More... | |
#define FLAGS_NONE 0 |
Referenced by ip64_addrmap_create().
#define FLAGS_RECYCLABLE 1 |
Referenced by ip64_addrmap_set_recycleble(), and recycle().
struct ip64_addrmap_entry* ip64_addrmap_create | ( | const uip_ip6addr_t * | ip6addr, |
uint16_t | ip6port, | ||
const uip_ip4addr_t * | ip4addr, | ||
uint16_t | ip4port, | ||
uint8_t | protocol | ||
) |
Create a new address mapping from an IPv6 address/port, an IPv4 address/port, and a protocol number.
References check_age(), ip64_addrmap_entry::flags, FLAGS_NONE, increase_mapped_port(), ip64_addrmap_entry::ip4addr, ip64_addrmap_entry::ip4port, ip64_addrmap_entry::ip6addr, ip64_addrmap_entry::ip6port, list_add(), list_head(), list_item_next(), ip64_addrmap_entry::mapped_port, mapped_port, memb_alloc(), n, NULL, ip64_addrmap_entry::protocol, recycle(), ip64_addrmap_entry::timer, and timer_set().
Referenced by ip64_6to4().
void ip64_addrmap_init | ( | void | ) |
Initialize the ip64_addrmap module.
References FIRST_MAPPED_PORT, list_init(), mapped_port, and memb_init().
struct ip64_addrmap_entry* ip64_addrmap_list | ( | void | ) |
Obtain the list of all address mappings.
References list_head().
struct ip64_addrmap_entry* ip64_addrmap_lookup | ( | const uip_ip6addr_t * | ip6addr, |
uint16_t | ip6port, | ||
const uip_ip4addr_t * | ip4addr, | ||
uint16_t | ip4port, | ||
uint8_t | protocol | ||
) |
Look up an address mapping from inside the IPv6 network, given the IPv6 address/port, the IPv4 address/port, and the protocol.
References check_age(), ip64_addrmap_entry::ip4addr, ip64_addrmap_entry::ip4port, ip64_addrmap_entry::ip6addr, ip64_addrmap_entry::ip6port, list_head(), list_item_next(), NULL, printf, ip64_addrmap_entry::protocol, uip_htons(), uip_ip4addr_cmp, and uip_ip6addr_cmp.
Referenced by ip64_6to4().
struct ip64_addrmap_entry* ip64_addrmap_lookup_port | ( | uint16_t | mappedport, |
uint8_t | protocol | ||
) |
Look up an address mapping from the outside IPv4 network, given the mapped port number and protocol.
References check_age(), list_head(), list_item_next(), ip64_addrmap_entry::mapped_port, NULL, printf, and ip64_addrmap_entry::protocol.
Referenced by ip64_4to6().
void ip64_addrmap_set_lifetime | ( | struct ip64_addrmap_entry * | e, |
clock_time_t | lifetime | ||
) |
Set the lifetime of an address mapping.
References NULL, ip64_addrmap_entry::timer, and timer_set().
Referenced by ip64_6to4().
void ip64_addrmap_set_recycleble | ( | struct ip64_addrmap_entry * | e | ) |
Mark an address mapping to be recyclable.
References ip64_addrmap_entry::flags, FLAGS_RECYCLABLE, and NULL.
Referenced by ip64_6to4().