Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Serial Line IP (SLIP) protocol

The SLIP protocol is a very simple way to transmit IP packets over a serial line.

It does not provide any framing or error control, and is therefore not very widely used today.

This SLIP implementation requires two functions for accessing the serial device: slipdev_char_poll() and slipdev_char_put(). These must be implemented specifically for the system on which the SLIP protocol is to be run.

Files

file  slipdev.c
 SLIP protocol implementation.
 
file  slipdev.h
 SLIP header file.
 

Macros

#define SLIP_END   0300
 
#define SLIP_ESC   0333
 
#define SLIP_ESC_END   0334
 
#define SLIP_ESC_ESC   0335
 

Functions

uint8_t slipdev_char_poll (uint8_t *c)
 Poll the serial device for a character. More...
 
void slipdev_char_put (uint8_t c)
 Put a character on the serial device. More...
 
void slipdev_init (void)
 Initialize the SLIP module. More...
 
uint16_t slipdev_poll (void)
 Poll the SLIP device for an available packet. More...
 
uint8_t slipdev_send (void)
 Send the packet in the uip_buf and uip_appdata buffers using the SLIP protocol. More...
 

Variables

static uint8_t lastc
 
static uint16_t len
 
static uint8_t slip_buf [UIP_BUFSIZE]
 
static uint16_t tmplen
 

#define SLIP_END   0300

Referenced by slipdev_poll(), and slipdev_send().

#define SLIP_ESC   0333

Referenced by slipdev_poll(), and slipdev_send().

#define SLIP_ESC_END   0334

Referenced by slipdev_poll(), and slipdev_send().

#define SLIP_ESC_ESC   0335

Referenced by slipdev_poll(), and slipdev_send().

uint8_t slipdev_char_poll ( uint8_t *  c)

Poll the serial device for a character.

This function is used by the SLIP implementation to poll the serial device for a character. It must be implemented specifically for the system on which the SLIP implementation is to be run.

The function should return immediately regardless if a character is available or not. If a character is available it should be placed at the memory location pointed to by the pointer supplied by the argument c.

Parameters
cA pointer to a byte that is filled in by the function with the received character, if available.
Return values
0If no character is available.
Non-zeroIf a character is available.

Referenced by slipdev_poll().

void slipdev_char_put ( uint8_t  c)

Put a character on the serial device.

This function is used by the SLIP implementation to put a character on the serial device. It must be implemented specifically for the system on which the SLIP implementation is to be run.

Parameters
cThe character to be put on the serial device.

Referenced by slipdev_send().

void slipdev_init ( void  )

Initialize the SLIP module.

This function does not initialize the underlying RS232 device, but only the SLIP part.

References lastc, and len.

uint16_t slipdev_poll ( void  )

Poll the SLIP device for an available packet.

This function will poll the SLIP device to see if a packet is available. It uses a buffer in which all avaliable bytes from the RS232 interface are read into. When a full packet has been read into the buffer, the packet is copied into the uip_buf buffer and the length of the packet is returned.

Returns
The length of the packet placed in the uip_buf buffer, or zero if no packet is available.

References c, lastc, len, slip_buf, SLIP_END, SLIP_ESC, SLIP_ESC_END, SLIP_ESC_ESC, slipdev_char_poll(), tmplen, uip_buf, UIP_BUFSIZE, and UIP_LLH_LEN.

uint8_t slipdev_send ( void  )

Send the packet in the uip_buf and uip_appdata buffers using the SLIP protocol.

The first 40 bytes of the packet (the IP and TCP headers) are read from the uip_buf buffer, and the following bytes (the application data) are read from the uip_appdata buffer.

Returns
This function will always return 0.

References c, i, SLIP_END, SLIP_ESC, SLIP_ESC_END, SLIP_ESC_ESC, slipdev_char_put(), uip_appdata, uip_buf, uip_len, UIP_LLH_LEN, and UIP_TCPIP_HLEN.

uint8_t lastc
static

Referenced by slipdev_init(), and slipdev_poll().

uint8_t slip_buf[UIP_BUFSIZE]
static

Referenced by slipdev_poll().

uint16_t tmplen
static

Referenced by slipdev_poll().