Data Structures | |
struct | _sics_frag |
struct | sicslowpan_addr_context |
The header for fragments. More... | |
struct | sicslowpan_nh_compressor |
The structure of a next header compressor. More... | |
Files | |
file | sicslowpan.c |
6lowpan implementation (RFC4944 and draft-ietf-6lowpan-hc-06) | |
file | sicslowpan.h |
Header file for the 6lowpan implementation (RFC4944 and draft-hui-6lowpan-hc-01) | |
Macros | |
#define | _DEBUG_ DEBUG_NONE |
FOR HC-06 COMPLIANCE TODO: -Add compression options to UDP, currently only supports both ports compressed or both ports elided. More... | |
#define | COMPRESSION_THRESHOLD SICSLOWPAN_CONF_COMPRESSION_THRESHOLD |
Some MAC layers need a minimum payload, which is configurable through the SICSLOWPAN_CONF_MIN_MAC_PAYLOAD option. More... | |
#define | FRAG_IN_DEBUG DEBUG_NONE |
#define | FRAG_OUT_DEBUG DEBUG_NONE |
#define | GET16(ptr, index) (((uint16_t)((ptr)[index] << 8)) | ((ptr)[(index) + 1])) |
#define | MAC_MAX_PAYLOAD SICSLOWPAN_CONF_MAC_MAX_PAYLOAD |
Size of the 802.15.4 payload (127byte - 25 for MAC header) More... | |
#define | PRINTF(...) |
#define | PRINTFI(...) |
#define | PRINTFO(...) |
#define | PRINTPACKETBUF() |
#define | PRINTSICSLOWPANBUF() |
#define | PRINTUIPBUF() |
#define | SET16(ptr, index, value) |
#define | SICSLOWPAN_COMPRESSION SICSLOWPAN_CONF_COMPRESSION |
#define | SICSLOWPAN_MAX_MAC_TRANSMISSIONS SICSLOWPAN_CONF_MAX_MAC_TRANSMISSIONS |
#define | SICSLOWPAN_NHC_EXT_HDR 0xE0 |
#define | SICSLOWPAN_NHC_MASK 0xF0 |
#define | UIP_LOG(m) |
#define | USE_FRAMER_HDRLEN 1 |
Functions | |
void | rime_sniffer_add (struct rime_sniffer *s) |
void | rime_sniffer_remove (struct rime_sniffer *s) |
static void | set_packet_attrs (void) |
int | sicslowpan_get_last_rssi (void) |
void | sicslowpan_init (void) |
Variables | |
static struct rime_sniffer * | callback = NULL |
static int | last_rssi |
struct network_driver | sicslowpan_driver |
Pointers in the packetbuf buffer | |
#define | PACKETBUF_FRAG_PTR (packetbuf_ptr) |
#define | PACKETBUF_FRAG_DISPATCH_SIZE 0 /* 16 bit */ |
#define | PACKETBUF_FRAG_TAG 2 /* 16 bit */ |
#define | PACKETBUF_FRAG_OFFSET 4 /* 8 bit */ |
#define | PACKETBUF_HC1_DISPATCH 0 /* 8 bit */ |
#define | PACKETBUF_HC1_ENCODING 1 /* 8 bit */ |
#define | PACKETBUF_HC1_TTL 2 /* 8 bit */ |
#define | PACKETBUF_HC1_HC_UDP_DISPATCH 0 /* 8 bit */ |
#define | PACKETBUF_HC1_HC_UDP_HC1_ENCODING 1 /* 8 bit */ |
#define | PACKETBUF_HC1_HC_UDP_UDP_ENCODING 2 /* 8 bit */ |
#define | PACKETBUF_HC1_HC_UDP_TTL 3 /* 8 bit */ |
#define | PACKETBUF_HC1_HC_UDP_PORTS 4 /* 8 bit */ |
#define | PACKETBUF_HC1_HC_UDP_CHKSUM 5 /* 16 bit */ |
Pointers in the sicslowpan and uip buffer | |
#define | SICSLOWPAN_IP_BUF ((struct uip_ip_hdr *)&sicslowpan_buf[UIP_LLH_LEN]) |
#define | SICSLOWPAN_UDP_BUF ((struct uip_udp_hdr *)&sicslowpan_buf[UIP_LLIPH_LEN]) |
#define | UIP_IP_BUF ((struct uip_ip_hdr *)&uip_buf[UIP_LLH_LEN]) |
#define | UIP_UDP_BUF ((struct uip_udp_hdr *)&uip_buf[UIP_LLIPH_LEN]) |
#define | UIP_TCP_BUF ((struct uip_tcp_hdr *)&uip_buf[UIP_LLIPH_LEN]) |
#define | UIP_ICMP_BUF ((struct uip_icmp_hdr *)&uip_buf[UIP_LLIPH_LEN]) |
General variables | |
static uint8_t * | packetbuf_ptr |
A pointer to the packetbuf buffer. More... | |
static uint8_t | uncomp_hdr_len |
uncomp_hdr_len is the length of the headers before compression (if HC2 is used this includes the UDP header in addition to the IP header). More... | |
static int | last_tx_status |
the result of the last transmitted fragment More... | |
Fragmentation related variables | |
typedef struct _sics_frag | sics_frag_t |
static uip_buf_t | sicslowpan_aligned_buf |
The buffer used for the 6lowpan reassembly. More... | |
static uint16_t | sicslowpan_len |
The total length of the IPv6 packet in the sicslowpan_buf. More... | |
static uint16_t | my_tag |
Datagram tag to be put in the fragments I send. More... | |
uip_buf_t | sicslowpanbuf [NUM_REASM_BUFS] |
uint8_t | sics_used_buf [NUM_REASM_BUFS] |
static sics_frag_t | sics_frag_attr [NUM_REASM_BUFS] |
static struct ctimer | reasm_ct |
static void | sics_frag_buf_init (void) |
static void | reasm_timer_callback (void *ptr) |
#define | sicslowpan_buf (sicslowpan_aligned_buf.u8) |
HC06 specific variables | |
static struct sicslowpan_addr_context | addr_contexts [SICSLOWPAN_CONF_MAX_ADDR_CONTEXTS] |
Addresses contexts for IPHC. More... | |
static struct sicslowpan_addr_context * | context |
pointer to an address context. More... | |
static uint8_t * | hc06_ptr |
pointer to the byte where to write next inline field. More... | |
const uint8_t | unc_llconf [] = {0x0f,0x28,0x22,0x20} |
const uint8_t | unc_ctxconf [] = {0x00,0x88,0x82,0x80} |
const uint8_t | unc_mxconf [] = {0x0f, 0x25, 0x23, 0x21} |
const uint8_t | llprefix [] = {0xfe, 0x80} |
static const uint8_t | ttl_values [] = {0, 1, 64, 255} |
HC06 related functions | |
static struct sicslowpan_addr_context * | addr_context_lookup_by_prefix (uip_ipaddr_t *ipaddr) |
find the context corresponding to prefix ipaddr More... | |
static struct sicslowpan_addr_context * | addr_context_lookup_by_number (uint8_t number) |
find the context with the given number More... | |
static uint8_t | compress_addr_64 (uint8_t bitpos, uip_ipaddr_t *ipaddr, uip_lladdr_t *lladdr) |
static void | uncompress_addr (uip_ipaddr_t *ipaddr, uint8_t const prefix[], uint8_t pref_post_count, uip_lladdr_t *lladdr) |
static void | compress_hdr_hc06 (linkaddr_t *link_destaddr, uint8_t *tx_hdr_len) |
Compress IP/UDP header. More... | |
static void | uncompress_hdr_hc06 (uint16_t ip_len, uint8_t *uip_buff, uint8_t *rx_hdr_len) |
Uncompress HC06 (i.e., IPHC and LOWPAN_UDP) headers and put them in sicslowpan_buf. More... | |
IPv6 dispatch "compression" function | |
static void | compress_hdr_ipv6 (linkaddr_t *link_destaddr, uint8_t *tx_hdr_len) |
Input/output functions common to all compression schemes | |
static void | packet_sent (void *ptr, int status, int transmissions) |
Callback function for the MAC packet sent callback. More... | |
static void | send_packet (linkaddr_t *dest) |
This function is called by the 6lowpan code to send out a packet. More... | |
static uint8_t | output (const uip_lladdr_t *localdest) |
Take an IP packet and format it to be sent on an 802.15.4 network using 6lowpan. More... | |
static void | input (void) |
Process a received 6lowpan packet. More... | |
General sicslowpan defines | |
#define | SICSLOWPAN_UDP_4_BIT_PORT_MIN 0xF0B0 |
#define | SICSLOWPAN_UDP_4_BIT_PORT_MAX 0xF0BF /* F0B0 + 15 */ |
#define | SICSLOWPAN_UDP_8_BIT_PORT_MIN 0xF000 |
#define | SICSLOWPAN_UDP_8_BIT_PORT_MAX 0xF0FF /* F000 + 255 */ |
6lowpan compressions | |
#define | SICSLOWPAN_COMPRESSION_IPV6 0 |
#define | SICSLOWPAN_COMPRESSION_HC1 1 |
#define | SICSLOWPAN_COMPRESSION_HC06 2 |
6lowpan dispatches | |
#define | SICSLOWPAN_DISPATCH_NALP 0x00 /* 00xxxxxx */ |
#define | SICSLOWPAN_DISPATCH_IPV6 0x41 /* 01000001 = 65 */ |
#define | SICSLOWPAN_DISPATCH_HC1 0x42 /* 01000010 = 66 */ |
#define | SICSLOWPAN_DISPATCH_IPHC 0x60 /* 011xxxxx = ... */ |
#define | SICSLOWPAN_DISPATCH_FRAG1 0xc0 /* 11000xxx */ |
#define | SICSLOWPAN_DISPATCH_FRAGN 0xe0 /* 11100xxx */ |
HC1 encoding | |
#define | SICSLOWPAN_HC1_NH_UDP 0x02 |
#define | SICSLOWPAN_HC1_NH_TCP 0x06 |
#define | SICSLOWPAN_HC1_NH_ICMP6 0x04 |
HC_UDP encoding (works together with HC1) | |
#define | SICSLOWPAN_HC_UDP_ALL_C 0xE0 |
IPHC encoding | |
#define | SICSLOWPAN_IPHC_FL_C 0x10 |
#define | SICSLOWPAN_IPHC_TC_C 0x08 |
#define | SICSLOWPAN_IPHC_NH_C 0x04 |
#define | SICSLOWPAN_IPHC_TTL_1 0x01 |
#define | SICSLOWPAN_IPHC_TTL_64 0x02 |
#define | SICSLOWPAN_IPHC_TTL_255 0x03 |
#define | SICSLOWPAN_IPHC_TTL_I 0x00 |
#define | SICSLOWPAN_IPHC_CID 0x80 |
#define | SICSLOWPAN_IPHC_SAC 0x40 |
#define | SICSLOWPAN_IPHC_SAM_00 0x00 |
#define | SICSLOWPAN_IPHC_SAM_01 0x10 |
#define | SICSLOWPAN_IPHC_SAM_10 0x20 |
#define | SICSLOWPAN_IPHC_SAM_11 0x30 |
#define | SICSLOWPAN_IPHC_SAM_BIT 4 |
#define | SICSLOWPAN_IPHC_M 0x08 |
#define | SICSLOWPAN_IPHC_DAC 0x04 |
#define | SICSLOWPAN_IPHC_DAM_00 0x00 |
#define | SICSLOWPAN_IPHC_DAM_01 0x01 |
#define | SICSLOWPAN_IPHC_DAM_10 0x02 |
#define | SICSLOWPAN_IPHC_DAM_11 0x03 |
#define | SICSLOWPAN_IPHC_DAM_BIT 0 |
#define | SICSLOWPAN_IPHC_ADDR_CONTEXT_LL 0 |
#define | SICSLOWPAN_IPHC_MCAST_RANGE 0xA0 |
LOWPAN_UDP encoding (works together with IPHC) | |
#define | SICSLOWPAN_NHC_UDP_MASK 0xF8 |
#define | SICSLOWPAN_NHC_UDP_ID 0xF0 |
#define | SICSLOWPAN_NHC_UDP_CHECKSUMC 0x04 |
#define | SICSLOWPAN_NHC_UDP_CHECKSUMI 0x00 |
#define | SICSLOWPAN_NHC_UDP_CS_P_00 0xF0 /* all inline */ |
#define | SICSLOWPAN_NHC_UDP_CS_P_01 0xF1 /* source 16bit inline, dest = 0xF0 + 8 bit inline */ |
#define | SICSLOWPAN_NHC_UDP_CS_P_10 0xF2 /* source = 0xF0 + 8bit inline, dest = 16 bit inline */ |
#define | SICSLOWPAN_NHC_UDP_CS_P_11 0xF3 /* source & dest = 0xF0B + 4bit inline */ |
The 6lowpan "headers" length | |
#define | SICSLOWPAN_IPV6_HDR_LEN 1 /*one byte*/ |
#define | SICSLOWPAN_HC1_HDR_LEN 3 |
#define | SICSLOWPAN_HC1_HC_UDP_HDR_LEN 7 |
#define | SICSLOWPAN_FRAG1_HDR_LEN 4 |
#define | SICSLOWPAN_FRAGN_HDR_LEN 5 |
Address compressibility test functions | |
#define | sicslowpan_is_iid_16_bit_compressable(a) |
check whether we can compress the IID in address 'a' to 16 bits. More... | |
#define | sicslowpan_is_mcast_addr_decompressable(a) |
check whether the 9-bit group-id of the compressed multicast address is known. More... | |
#define | sicslowpan_is_mcast_addr_compressable(a) |
check whether the 112-bit group-id of the multicast address is mappable to a 9-bit group-id It is true if the group is the all nodes or all routers group. More... | |
#define | sicslowpan_is_mcast_addr_compressable48(a) |
#define | sicslowpan_is_mcast_addr_compressable32(a) |
#define | sicslowpan_is_mcast_addr_compressable8(a) |
#define _DEBUG_ DEBUG_NONE |
FOR HC-06 COMPLIANCE TODO: -Add compression options to UDP, currently only supports both ports compressed or both ports elided.
-Verify TC/FL compression works
-Add stateless multicast option
#define COMPRESSION_THRESHOLD SICSLOWPAN_CONF_COMPRESSION_THRESHOLD |
Some MAC layers need a minimum payload, which is configurable through the SICSLOWPAN_CONF_MIN_MAC_PAYLOAD option.
Referenced by output().
#define FRAG_IN_DEBUG DEBUG_NONE |
#define FRAG_OUT_DEBUG DEBUG_NONE |
#define GET16 | ( | ptr, | |
index | |||
) | (((uint16_t)((ptr)[index] << 8)) | ((ptr)[(index) + 1])) |
Referenced by input().
#define MAC_MAX_PAYLOAD SICSLOWPAN_CONF_MAC_MAX_PAYLOAD |
Size of the 802.15.4 payload (127byte - 25 for MAC header)
Referenced by output().
#define PACKETBUF_FRAG_PTR (packetbuf_ptr) |
#define PACKETBUF_HC1_DISPATCH 0 /* 8 bit */ |
Referenced by input().
#define PACKETBUF_HC1_ENCODING 1 /* 8 bit */ |
#define PACKETBUF_HC1_HC_UDP_CHKSUM 5 /* 16 bit */ |
#define PACKETBUF_HC1_HC_UDP_DISPATCH 0 /* 8 bit */ |
#define PACKETBUF_HC1_HC_UDP_HC1_ENCODING 1 /* 8 bit */ |
#define PACKETBUF_HC1_HC_UDP_PORTS 4 /* 8 bit */ |
#define PACKETBUF_HC1_HC_UDP_TTL 3 /* 8 bit */ |
#define PACKETBUF_HC1_HC_UDP_UDP_ENCODING 2 /* 8 bit */ |
#define PACKETBUF_HC1_TTL 2 /* 8 bit */ |
#define PRINTF | ( | ... | ) |
Referenced by compress_hdr_hc06(), input(), packet_sent(), uncompress_addr(), and uncompress_hdr_hc06().
#define PRINTFI | ( | ... | ) |
Referenced by input(), and reasm_timer_callback().
#define PRINTFO | ( | ... | ) |
Referenced by output().
#define PRINTPACKETBUF | ( | ) |
#define PRINTSICSLOWPANBUF | ( | ) |
#define PRINTUIPBUF | ( | ) |
#define SET16 | ( | ptr, | |
index, | |||
value | |||
) |
Referenced by output().
#define sicslowpan_buf (sicslowpan_aligned_buf.u8) |
Referenced by input(), and uncompress_hdr_hc06().
#define SICSLOWPAN_COMPRESSION SICSLOWPAN_CONF_COMPRESSION |
#define SICSLOWPAN_COMPRESSION_HC06 2 |
#define SICSLOWPAN_COMPRESSION_HC1 1 |
#define SICSLOWPAN_COMPRESSION_IPV6 0 |
#define SICSLOWPAN_DISPATCH_HC1 0x42 /* 01000010 = 66 */ |
Referenced by input().
#define SICSLOWPAN_DISPATCH_IPHC 0x60 /* 011xxxxx = ... */ |
Referenced by compress_hdr_hc06(), and input().
#define SICSLOWPAN_DISPATCH_IPV6 0x41 /* 01000001 = 65 */ |
Referenced by compress_hdr_ipv6(), and input().
#define SICSLOWPAN_DISPATCH_NALP 0x00 /* 00xxxxxx */ |
#define SICSLOWPAN_HC1_HC_UDP_HDR_LEN 7 |
#define SICSLOWPAN_HC1_HDR_LEN 3 |
#define SICSLOWPAN_HC1_NH_ICMP6 0x04 |
#define SICSLOWPAN_HC1_NH_TCP 0x06 |
#define SICSLOWPAN_HC1_NH_UDP 0x02 |
#define SICSLOWPAN_HC_UDP_ALL_C 0xE0 |
#define SICSLOWPAN_IP_BUF ((struct uip_ip_hdr *)&sicslowpan_buf[UIP_LLH_LEN]) |
Referenced by input(), and uncompress_hdr_hc06().
#define SICSLOWPAN_IPHC_ADDR_CONTEXT_LL 0 |
#define SICSLOWPAN_IPHC_CID 0x80 |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_IPHC_DAC 0x04 |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_IPHC_DAM_00 0x00 |
Referenced by compress_hdr_hc06().
#define SICSLOWPAN_IPHC_DAM_01 0x01 |
Referenced by compress_hdr_hc06().
#define SICSLOWPAN_IPHC_DAM_10 0x02 |
Referenced by compress_hdr_hc06().
#define SICSLOWPAN_IPHC_DAM_11 0x03 |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_IPHC_DAM_BIT 0 |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_IPHC_FL_C 0x10 |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_IPHC_M 0x08 |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_IPHC_MCAST_RANGE 0xA0 |
#define SICSLOWPAN_IPHC_NH_C 0x04 |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_IPHC_SAC 0x40 |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_IPHC_SAM_00 0x00 |
Referenced by compress_hdr_hc06().
#define SICSLOWPAN_IPHC_SAM_01 0x10 |
#define SICSLOWPAN_IPHC_SAM_10 0x20 |
#define SICSLOWPAN_IPHC_SAM_11 0x30 |
Referenced by uncompress_hdr_hc06().
#define SICSLOWPAN_IPHC_SAM_BIT 4 |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_IPHC_TC_C 0x08 |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_IPHC_TTL_1 0x01 |
Referenced by compress_hdr_hc06().
#define SICSLOWPAN_IPHC_TTL_255 0x03 |
Referenced by compress_hdr_hc06().
#define SICSLOWPAN_IPHC_TTL_64 0x02 |
Referenced by compress_hdr_hc06().
#define SICSLOWPAN_IPHC_TTL_I 0x00 |
Referenced by uncompress_hdr_hc06().
#define SICSLOWPAN_IPV6_HDR_LEN 1 /*one byte*/ |
Referenced by compress_hdr_ipv6(), and input().
#define sicslowpan_is_iid_16_bit_compressable | ( | a | ) |
check whether we can compress the IID in address 'a' to 16 bits.
This is used for unicast addresses only, and is true if the address is on the format <PREFIX>::0000:00ff:fe00:XXXX NOTE: we currently assume 64-bits prefixes
Referenced by compress_addr_64().
#define sicslowpan_is_mcast_addr_compressable | ( | a | ) |
check whether the 112-bit group-id of the multicast address is mappable to a 9-bit group-id It is true if the group is the all nodes or all routers group.
#define sicslowpan_is_mcast_addr_compressable32 | ( | a | ) |
Referenced by compress_hdr_hc06().
#define sicslowpan_is_mcast_addr_compressable48 | ( | a | ) |
Referenced by compress_hdr_hc06().
#define sicslowpan_is_mcast_addr_compressable8 | ( | a | ) |
Referenced by compress_hdr_hc06().
#define sicslowpan_is_mcast_addr_decompressable | ( | a | ) |
check whether the 9-bit group-id of the compressed multicast address is known.
It is true if the 9-bit group is the all nodes or all routers group.
a | is typed uint8_t * |
#define SICSLOWPAN_MAX_MAC_TRANSMISSIONS SICSLOWPAN_CONF_MAX_MAC_TRANSMISSIONS |
Referenced by output().
#define SICSLOWPAN_NHC_EXT_HDR 0xE0 |
#define SICSLOWPAN_NHC_MASK 0xF0 |
#define SICSLOWPAN_NHC_UDP_CHECKSUMC 0x04 |
Referenced by uncompress_hdr_hc06().
#define SICSLOWPAN_NHC_UDP_CHECKSUMI 0x00 |
#define SICSLOWPAN_NHC_UDP_CS_P_00 0xF0 /* all inline */ |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_NHC_UDP_CS_P_01 0xF1 /* source 16bit inline, dest = 0xF0 + 8 bit inline */ |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_NHC_UDP_CS_P_10 0xF2 /* source = 0xF0 + 8bit inline, dest = 16 bit inline */ |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_NHC_UDP_CS_P_11 0xF3 /* source & dest = 0xF0B + 4bit inline */ |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_NHC_UDP_ID 0xF0 |
Referenced by uncompress_hdr_hc06().
#define SICSLOWPAN_NHC_UDP_MASK 0xF8 |
Referenced by uncompress_hdr_hc06().
#define SICSLOWPAN_UDP_4_BIT_PORT_MAX 0xF0BF /* F0B0 + 15 */ |
#define SICSLOWPAN_UDP_4_BIT_PORT_MIN 0xF0B0 |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_UDP_8_BIT_PORT_MAX 0xF0FF /* F000 + 255 */ |
#define SICSLOWPAN_UDP_8_BIT_PORT_MIN 0xF000 |
Referenced by compress_hdr_hc06(), and uncompress_hdr_hc06().
#define SICSLOWPAN_UDP_BUF ((struct uip_udp_hdr *)&sicslowpan_buf[UIP_LLIPH_LEN]) |
#define UIP_ICMP_BUF ((struct uip_icmp_hdr *)&uip_buf[UIP_LLIPH_LEN]) |
Referenced by set_packet_attrs().
#define UIP_IP_BUF ((struct uip_ip_hdr *)&uip_buf[UIP_LLH_LEN]) |
Referenced by compress_hdr_hc06(), compress_hdr_ipv6(), input(), output(), and set_packet_attrs().
#define UIP_LOG | ( | m | ) |
#define UIP_TCP_BUF ((struct uip_tcp_hdr *)&uip_buf[UIP_LLIPH_LEN]) |
Referenced by output(), and set_packet_attrs().
#define UIP_UDP_BUF ((struct uip_udp_hdr *)&uip_buf[UIP_LLIPH_LEN]) |
Referenced by compress_hdr_hc06(), and set_packet_attrs().
#define USE_FRAMER_HDRLEN 1 |
typedef struct _sics_frag sics_frag_t |
|
static |
find the context with the given number
References addr_contexts, i, NULL, SICSLOWPAN_CONF_MAX_ADDR_CONTEXTS, and sicslowpan_addr_context::used.
Referenced by uncompress_hdr_hc06().
|
static |
find the context corresponding to prefix ipaddr
References addr_contexts, i, NULL, sicslowpan_addr_context::prefix, SICSLOWPAN_CONF_MAX_ADDR_CONTEXTS, uip_ipaddr_prefixcmp, and sicslowpan_addr_context::used.
Referenced by compress_hdr_hc06().
|
static |
References hc06_ptr, sicslowpan_is_iid_16_bit_compressable, uip_ip6addr_t::u16, and uip_is_addr_mac_addr_based.
Referenced by compress_hdr_hc06().
|
static |
Compress IP/UDP header.
This function is called by the 6lowpan code to create a compressed 6lowpan packet in the packetbuf buffer from a full IPv6 packet in the uip_buf buffer.
HC-06 (draft-ietf-6lowpan-hc, version 6)
http://tools.ietf.org/html/draft-ietf-6lowpan-hc-06
For LOWPAN_UDP compression, we either compress both ports or none. General format with LOWPAN_UDP compression is
* 1 2 3 * 0 1 2 3 4 5 6 7 8 9 0 1 2 3 4 5 6 7 8 9 0 1 2 3 4 5 6 7 8 9 0 1 * +-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ * |0|1|1|TF |N|HLI|C|S|SAM|M|D|DAM| SCI | DCI | comp. IPv6 hdr| * +-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ * | compressed IPv6 fields ..... | * +-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ * | LOWPAN_UDP | non compressed UDP fields ... | * +-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ * | L4 data ... | * +-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ *
link_destaddr | L2 destination address, needed to compress IP dest |
References addr_context_lookup_by_prefix(), compress_addr_64(), hc06_ptr, NULL, sicslowpan_addr_context::number, packetbuf_ptr, PRINTF, SICSLOWPAN_DISPATCH_IPHC, SICSLOWPAN_IPHC_CID, SICSLOWPAN_IPHC_DAC, SICSLOWPAN_IPHC_DAM_00, SICSLOWPAN_IPHC_DAM_01, SICSLOWPAN_IPHC_DAM_10, SICSLOWPAN_IPHC_DAM_11, SICSLOWPAN_IPHC_DAM_BIT, SICSLOWPAN_IPHC_FL_C, SICSLOWPAN_IPHC_M, SICSLOWPAN_IPHC_NH_C, SICSLOWPAN_IPHC_SAC, SICSLOWPAN_IPHC_SAM_00, SICSLOWPAN_IPHC_SAM_BIT, SICSLOWPAN_IPHC_TC_C, SICSLOWPAN_IPHC_TTL_1, SICSLOWPAN_IPHC_TTL_255, SICSLOWPAN_IPHC_TTL_64, sicslowpan_is_mcast_addr_compressable32, sicslowpan_is_mcast_addr_compressable48, sicslowpan_is_mcast_addr_compressable8, SICSLOWPAN_NHC_UDP_CS_P_00, SICSLOWPAN_NHC_UDP_CS_P_01, SICSLOWPAN_NHC_UDP_CS_P_10, SICSLOWPAN_NHC_UDP_CS_P_11, SICSLOWPAN_UDP_4_BIT_PORT_MIN, SICSLOWPAN_UDP_8_BIT_PORT_MIN, UIP_IP_BUF, UIP_IPH_LEN, uip_is_addr_link_local, uip_is_addr_mcast, uip_is_addr_unspecified, uip_lladdr, UIP_PROTO_UDP, UIP_UDP_BUF, UIP_UDPH_LEN, and uncomp_hdr_len.
Referenced by output().
|
static |
References packetbuf_ptr, SICSLOWPAN_DISPATCH_IPV6, SICSLOWPAN_IPV6_HDR_LEN, UIP_IP_BUF, UIP_IPH_LEN, and uncomp_hdr_len.
Referenced by output().
|
static |
Process a received 6lowpan packet.
r | The MAC layer |
The 6lowpan packet is put in packetbuf by the MAC. If its a frag1 or a non-fragmented packet we first uncompress the IP header. The 6lowpan payload and possibly the uncompressed IP header are then copied in siclowpan_buf. If the IP packet is complete it is copied to uip_buf and the IP layer is called.
References _sics_frag::frag_send_addr, _sics_frag::frag_size, _sics_frag::frag_tag, GET16, i, rime_sniffer::input_callback, last_rssi, linkaddr_copy(), LINKADDR_SIZE, NUM_REASM_BUFS, packetbuf_addr(), PACKETBUF_ADDR_SENDER, packetbuf_attr(), PACKETBUF_ATTR_RSSI, packetbuf_datalen(), packetbuf_dataptr(), PACKETBUF_FRAG_DISPATCH_SIZE, PACKETBUF_FRAG_OFFSET, PACKETBUF_FRAG_PTR, PACKETBUF_FRAG_TAG, PACKETBUF_HC1_DISPATCH, packetbuf_ptr, printf, PRINTF, PRINTFI, _sics_frag::processed_ip_len, REASSEMBLY_TIMEOUT, RIMESTATS_ADD, set_packet_attrs(), sics_used_buf, sicslowpan_buf, SICSLOWPAN_DISPATCH_FRAG1, SICSLOWPAN_DISPATCH_FRAGN, SICSLOWPAN_DISPATCH_HC1, SICSLOWPAN_DISPATCH_IPHC, SICSLOWPAN_DISPATCH_IPV6, SICSLOWPAN_FRAG1_HDR_LEN, SICSLOWPAN_FRAGN_HDR_LEN, SICSLOWPAN_IP_BUF, SICSLOWPAN_IPV6_HDR_LEN, sicslowpan_len, tcpip_input(), timer_expired(), timer_set(), linkaddr_t::u8, uip_buf_t::u8, UIP_IP_BUF, UIP_IPH_LEN, uip_len, UIP_LLH_LEN, uncomp_hdr_len, and uncompress_hdr_hc06().
|
static |
Take an IP packet and format it to be sent on an 802.15.4 network using 6lowpan.
localdest | The MAC address of the destination |
The IP packet is initially in uip_buf. Its header is compressed and if necessary it is fragmented. The resulting packet/fragments are put in packetbuf and delivered to the 802.15.4 MAC.
References compress_hdr_hc06(), compress_hdr_ipv6(), COMPRESSION_THRESHOLD, framer::create, delay_ms, last_tx_status, linkaddr_copy(), linkaddr_null, MAC_MAX_PAYLOAD, MAC_TX_COLLISION, MAC_TX_ERR, MAC_TX_ERR_FATAL, my_tag, NETSTACK_FRAMER, NULL, PACKETBUF_ADDR_RECEIVER, PACKETBUF_ATTR_MAX_MAC_TRANSMISSIONS, PACKETBUF_ATTR_PACKET_TYPE, PACKETBUF_ATTR_PACKET_TYPE_STREAM, PACKETBUF_ATTR_PACKET_TYPE_STREAM_END, packetbuf_clear(), packetbuf_dataptr(), PACKETBUF_FRAG_DISPATCH_SIZE, PACKETBUF_FRAG_OFFSET, PACKETBUF_FRAG_PTR, PACKETBUF_FRAG_TAG, packetbuf_ptr, packetbuf_set_addr(), packetbuf_set_attr(), packetbuf_set_datalen(), printf, PRINTFO, queuebuf_free(), queuebuf_new_from_packetbuf(), queuebuf_to_packetbuf(), RIMESTATS_ADD, send_packet(), SET16, set_packet_attrs(), SICSLOWPAN_DISPATCH_FRAG1, SICSLOWPAN_DISPATCH_FRAGN, SICSLOWPAN_FRAG1_HDR_LEN, SICSLOWPAN_FRAGN_HDR_LEN, SICSLOWPAN_MAX_MAC_TRANSMISSIONS, TCP_ACK, TCP_CTL, TCP_FIN, UIP_IP_BUF, uip_len, UIP_PROTO_TCP, UIP_TCP_BUF, and uncomp_hdr_len.
Referenced by sicslowpan_init().
|
static |
Callback function for the MAC packet sent callback.
References last_tx_status, NULL, rime_sniffer::output_callback, PRINTF, status, and uip_ds6_link_neighbor_callback().
Referenced by send_packet().
|
static |
References ctimer_reset(), i, NUM_REASM_BUFS, PRINTFI, reasm_ct, sics_used_buf, and timer_expired().
Referenced by sicslowpan_init().
void rime_sniffer_add | ( | struct rime_sniffer * | s | ) |
References s.
void rime_sniffer_remove | ( | struct rime_sniffer * | s | ) |
References NULL.
|
static |
This function is called by the 6lowpan code to send out a packet.
dest | the link layer destination address of the packet |
References NETSTACK_MAC, NULL, packet_sent(), PACKETBUF_ADDR_RECEIVER, PACKETBUF_ADDR_SENDER, PACKETBUF_ATTR_RELIABLE, packetbuf_set_addr(), packetbuf_set_attr(), mac_driver::send, uip_lladdr, and wdt_reset_count().
Referenced by output().
|
static |
|
static |
References NUM_REASM_BUFS, and sics_used_buf.
Referenced by sicslowpan_init().
int sicslowpan_get_last_rssi | ( | void | ) |
References last_rssi.
void sicslowpan_init | ( | void | ) |
|
static |
References hc06_ptr, PRINT6ADDR, PRINTF, uip_ip6addr_t::u8, and uip_ds6_set_addr_iid().
Referenced by uncompress_hdr_hc06().
|
static |
Uncompress HC06 (i.e., IPHC and LOWPAN_UDP) headers and put them in sicslowpan_buf.
This function is called by the input function when the dispatch is HC06. We process the packet in the packetbuf buffer, uncompress the header fields, and copy the result in the sicslowpan buffer. At the end of the decompression, packetbuf_hdr_len and uncompressed_hdr_len are set to the appropriate values
ip_len | Equal to 0 if the packet is not a fragment (IP length is then inferred from the L2 length), non 0 if the packet is a 1st fragment. |
References addr_context_lookup_by_number(), uip_ip_hdr::destipaddr, uip_udp_hdr::destport, uip_ip_hdr::flow, hc06_ptr, len, uip_ip_hdr::len, llprefix, NULL, PACKETBUF_ADDR_RECEIVER, PACKETBUF_ADDR_SENDER, packetbuf_datalen(), packetbuf_ptr, sicslowpan_addr_context::prefix, PRINTF, uip_ip_hdr::proto, sicslowpan_buf, SICSLOWPAN_IP_BUF, SICSLOWPAN_IPHC_CID, SICSLOWPAN_IPHC_DAC, SICSLOWPAN_IPHC_DAM_11, SICSLOWPAN_IPHC_DAM_BIT, SICSLOWPAN_IPHC_FL_C, SICSLOWPAN_IPHC_M, SICSLOWPAN_IPHC_NH_C, SICSLOWPAN_IPHC_SAC, SICSLOWPAN_IPHC_SAM_11, SICSLOWPAN_IPHC_SAM_BIT, SICSLOWPAN_IPHC_TC_C, SICSLOWPAN_IPHC_TTL_I, SICSLOWPAN_NHC_UDP_CHECKSUMC, SICSLOWPAN_NHC_UDP_CS_P_00, SICSLOWPAN_NHC_UDP_CS_P_01, SICSLOWPAN_NHC_UDP_CS_P_10, SICSLOWPAN_NHC_UDP_CS_P_11, SICSLOWPAN_NHC_UDP_ID, SICSLOWPAN_NHC_UDP_MASK, SICSLOWPAN_UDP_4_BIT_PORT_MIN, SICSLOWPAN_UDP_8_BIT_PORT_MIN, uip_ip_hdr::srcipaddr, uip_udp_hdr::srcport, uip_ip_hdr::tcflow, uip_ip_hdr::ttl, ttl_values, uip_udp_hdr::udpchksum, uip_udp_hdr::udplen, UIP_IPH_LEN, UIP_LLH_LEN, UIP_LLIPH_LEN, UIP_PROTO_UDP, UIP_UDPH_LEN, unc_ctxconf, unc_llconf, unc_mxconf, uncomp_hdr_len, uncompress_addr(), and uip_ip_hdr::vtc.
Referenced by input().
|
static |
Addresses contexts for IPHC.
Referenced by addr_context_lookup_by_number(), addr_context_lookup_by_prefix(), and sicslowpan_init().
|
static |
|
static |
pointer to an address context.
|
static |
pointer to the byte where to write next inline field.
Referenced by compress_addr_64(), compress_hdr_hc06(), uncompress_addr(), and uncompress_hdr_hc06().
|
static |
Referenced by input(), and sicslowpan_get_last_rssi().
|
static |
the result of the last transmitted fragment
Referenced by output(), and packet_sent().
const uint8_t llprefix[] = {0xfe, 0x80} |
Referenced by uncompress_hdr_hc06().
|
static |
Datagram tag to be put in the fragments I send.
Referenced by output().
|
static |
A pointer to the packetbuf buffer.
We initialize it to the beginning of the packetbuf buffer, then access different fields by updating the offset packetbuf_hdr_len.
Referenced by compress_hdr_hc06(), compress_hdr_ipv6(), input(), output(), and uncompress_hdr_hc06().
|
static |
Referenced by reasm_timer_callback(), and sicslowpan_init().
|
static |
uint8_t sics_used_buf[NUM_REASM_BUFS] |
Referenced by input(), reasm_timer_callback(), and sics_frag_buf_init().
|
static |
The buffer used for the 6lowpan reassembly.
This buffer contains only the IPv6 packet (no MAC header, 6lowpan, etc). It has a fix size as we do not use dynamic memory allocation.
struct network_driver sicslowpan_driver |
|
static |
The total length of the IPv6 packet in the sicslowpan_buf.
Referenced by input().
uip_buf_t sicslowpanbuf[NUM_REASM_BUFS] |
|
static |
Referenced by uncompress_hdr_hc06().
const uint8_t unc_ctxconf[] = {0x00,0x88,0x82,0x80} |
Referenced by uncompress_hdr_hc06().
const uint8_t unc_llconf[] = {0x0f,0x28,0x22,0x20} |
Referenced by uncompress_hdr_hc06().
const uint8_t unc_mxconf[] = {0x0f, 0x25, 0x23, 0x21} |
Referenced by uncompress_hdr_hc06().
|
static |
uncomp_hdr_len is the length of the headers before compression (if HC2 is used this includes the UDP header in addition to the IP header).
Referenced by compress_hdr_hc06(), compress_hdr_ipv6(), input(), output(), and uncompress_hdr_hc06().