Copyright (C) 2006-2010, Brainspark B.V.
This file is part of PolarSSL (http://www.polarssl.org) Lead Maintainer: Paul Bakker <polarssl_maintainer at polarssl.org>
All rights reserved.
This program is free software; you can redistribute it and/or modify it under the terms of the GNU General Public License as published by the Free Software Foundation; either version 2 of the License, or (at your option) any later version.
This program is distributed in the hope that it will be useful, but WITHOUT ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details.
You should have received a copy of the GNU General Public License along with this program; if not, write to the Free Software Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.
Data Structures | |
struct | arc4_context |
ARC4 context structure. More... | |
Functions | |
int | arc4_crypt (arc4_context *ctx, int length, const unsigned char *input, unsigned char *output) |
ARC4 cipher function. More... | |
int | arc4_self_test (int verbose) |
void | arc4_setup (arc4_context *ctx, const unsigned char *key, int keylen) |
ARC4 key schedule. More... | |
int arc4_crypt | ( | arc4_context * | ctx, |
int | length, | ||
const unsigned char * | input, | ||
unsigned char * | output | ||
) |
ARC4 cipher function.
ctx | ARC4 context |
length | length of the input data |
input | buffer holding the input data |
output | buffer for the output data |
Referenced by main().
int arc4_self_test | ( | int | verbose | ) |
Referenced by main().
void arc4_setup | ( | arc4_context * | ctx, |
const unsigned char * | key, | ||
int | keylen | ||
) |
ARC4 key schedule.
ctx | ARC4 context to be initialized |
key | the secret key |
keylen | length of the key |
Referenced by main().