Microchip® Advanced Software Framework

rsa.h File Reference

Copyright (C) 2006-2010, Brainspark B.V.

This file is part of PolarSSL (http://www.polarssl.org) Lead Maintainer: Paul Bakker <polarssl_maintainer at polarssl.org>

All rights reserved.

This program is free software; you can redistribute it and/or modify it under the terms of the GNU General Public License as published by the Free Software Foundation; either version 2 of the License, or (at your option) any later version.

This program is distributed in the hope that it will be useful, but WITHOUT ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details.

You should have received a copy of the GNU General Public License along with this program; if not, write to the Free Software Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.

#include "polarssl/bignum.h"

Data Structures

struct  rsa_context
 RSA context structure. More...
 

Macros

#define ASN1_HASH_MDX
 
#define ASN1_HASH_SHA1
 
#define ASN1_HASH_SHA2X
 
#define ASN1_STR_CONSTRUCTED_SEQUENCE   "\x30"
 
#define ASN1_STR_NULL   "\x05"
 
#define ASN1_STR_OCTET_STRING   "\x04"
 
#define ASN1_STR_OID   "\x06"
 
#define OID_COUNTRY_US   "\x86\x48"
 
#define OID_DIGEST_ALG_MDX   "\x2A\x86\x48\x86\xF7\x0D\x02\x00"
 
#define OID_HASH_ALG_SHA1   "\x2b\x0e\x03\x02\x1a"
 
#define OID_HASH_ALG_SHA2X   "\x60\x86\x48\x01\x65\x03\x04\x02\x00"
 
#define OID_ISO_IDENTIFIED_ORG   "\x2b"
 
#define OID_ISO_MEMBER_BODIES   "\x2a"
 
#define OID_OIW_SECSIG_SHA1   "\x0e\x03\x02\x1a"
 
#define OID_RSA_DATA_SECURITY   "\x86\xf7\x0d"
 
#define POLARSSL_ERR_RSA_BAD_INPUT_DATA   -0x0400
 
#define POLARSSL_ERR_RSA_INVALID_PADDING   -0x0410
 
#define POLARSSL_ERR_RSA_KEY_CHECK_FAILED   -0x0430
 
#define POLARSSL_ERR_RSA_KEY_GEN_FAILED   -0x0420
 
#define POLARSSL_ERR_RSA_OUTPUT_TOO_LARGE   -0x0470
 
#define POLARSSL_ERR_RSA_PRIVATE_FAILED   -0x0450
 
#define POLARSSL_ERR_RSA_PUBLIC_FAILED   -0x0440
 
#define POLARSSL_ERR_RSA_RNG_FAILED   -0x0480
 
#define POLARSSL_ERR_RSA_VERIFY_FAILED   -0x0460
 
#define RSA_CRYPT   2
 
#define RSA_PKCS_V15   0
 
#define RSA_PKCS_V21   1
 
#define RSA_PRIVATE   1
 
#define RSA_PUBLIC   0
 
#define RSA_SIGN   1
 
#define SIG_RSA_MD2   2
 
#define SIG_RSA_MD4   3
 
#define SIG_RSA_MD5   4
 
#define SIG_RSA_RAW   0
 
#define SIG_RSA_SHA1   5
 
#define SIG_RSA_SHA224   14
 
#define SIG_RSA_SHA256   11
 
#define SIG_RSA_SHA384   12
 
#define SIG_RSA_SHA512   13
 

Functions

int rsa_check_privkey (const rsa_context *ctx)
 Check a private RSA key. More...
 
int rsa_check_pubkey (const rsa_context *ctx)
 Check a public RSA key. More...
 
void rsa_free (rsa_context *ctx)
 Free the components of an RSA key. More...
 
int rsa_gen_key (rsa_context *ctx, int(*f_rng)(void *), void *p_rng, int nbits, int exponent)
 Generate an RSA keypair. More...
 
void rsa_init (rsa_context *ctx, int padding, int hash_id)
 Initialize an RSA context. More...
 
int rsa_pkcs1_decrypt (rsa_context *ctx, int mode, int *olen, const unsigned char *input, unsigned char *output, int output_max_len)
 Do an RSA operation, then remove the message padding. More...
 
int rsa_pkcs1_encrypt (rsa_context *ctx, int(*f_rng)(void *), void *p_rng, int mode, int ilen, const unsigned char *input, unsigned char *output)
 Add the message padding, then do an RSA operation. More...
 
int rsa_pkcs1_sign (rsa_context *ctx, int mode, int hash_id, int hashlen, const unsigned char *hash, unsigned char *sig)
 Do a private RSA to sign a message digest. More...
 
int rsa_pkcs1_verify (rsa_context *ctx, int mode, int hash_id, int hashlen, const unsigned char *hash, unsigned char *sig)
 Do a public RSA and check the message digest. More...
 
int rsa_private (rsa_context *ctx, const unsigned char *input, unsigned char *output)
 Do an RSA private key operation. More...
 
int rsa_public (rsa_context *ctx, const unsigned char *input, unsigned char *output)
 Do an RSA public key operation. More...
 
int rsa_self_test (int verbose)
 Checkup routine. More...
 

#define ASN1_HASH_MDX
Value:
( \
)
#define ASN1_STR_CONSTRUCTED_SEQUENCE
Definition: rsa.h:65
#define ASN1_STR_NULL
Definition: rsa.h:66
#define ASN1_STR_OCTET_STRING
Definition: rsa.h:68
#define ASN1_STR_OID
Definition: rsa.h:67
#define ASN1_HASH_SHA1
Value:
#define ASN1_STR_CONSTRUCTED_SEQUENCE
Definition: rsa.h:65
#define ASN1_STR_NULL
Definition: rsa.h:66
#define ASN1_STR_OCTET_STRING
Definition: rsa.h:68
#define ASN1_STR_OID
Definition: rsa.h:67
#define ASN1_HASH_SHA2X
Value:
#define ASN1_STR_CONSTRUCTED_SEQUENCE
Definition: rsa.h:65
#define ASN1_STR_NULL
Definition: rsa.h:66
#define ASN1_STR_OCTET_STRING
Definition: rsa.h:68
#define ASN1_STR_OID
Definition: rsa.h:67
#define ASN1_STR_CONSTRUCTED_SEQUENCE   "\x30"
#define ASN1_STR_NULL   "\x05"
#define ASN1_STR_OCTET_STRING   "\x04"
#define ASN1_STR_OID   "\x06"
#define OID_COUNTRY_US   "\x86\x48"
#define OID_DIGEST_ALG_MDX   "\x2A\x86\x48\x86\xF7\x0D\x02\x00"
#define OID_HASH_ALG_SHA1   "\x2b\x0e\x03\x02\x1a"
#define OID_HASH_ALG_SHA2X   "\x60\x86\x48\x01\x65\x03\x04\x02\x00"
#define OID_ISO_IDENTIFIED_ORG   "\x2b"
#define OID_ISO_MEMBER_BODIES   "\x2a"
#define OID_OIW_SECSIG_SHA1   "\x0e\x03\x02\x1a"
#define OID_RSA_DATA_SECURITY   "\x86\xf7\x0d"
#define POLARSSL_ERR_RSA_BAD_INPUT_DATA   -0x0400
#define POLARSSL_ERR_RSA_INVALID_PADDING   -0x0410
#define POLARSSL_ERR_RSA_KEY_CHECK_FAILED   -0x0430
#define POLARSSL_ERR_RSA_KEY_GEN_FAILED   -0x0420
#define POLARSSL_ERR_RSA_OUTPUT_TOO_LARGE   -0x0470
#define POLARSSL_ERR_RSA_PRIVATE_FAILED   -0x0450
#define POLARSSL_ERR_RSA_PUBLIC_FAILED   -0x0440
#define POLARSSL_ERR_RSA_RNG_FAILED   -0x0480
#define POLARSSL_ERR_RSA_VERIFY_FAILED   -0x0460
#define RSA_CRYPT   2
#define RSA_PKCS_V15   0

Referenced by main().

#define RSA_PKCS_V21   1
#define RSA_PRIVATE   1
#define RSA_PUBLIC   0
#define RSA_SIGN   1
#define SIG_RSA_MD2   2
#define SIG_RSA_MD4   3
#define SIG_RSA_MD5   4
#define SIG_RSA_RAW   0
#define SIG_RSA_SHA1   5
#define SIG_RSA_SHA224   14
#define SIG_RSA_SHA256   11
#define SIG_RSA_SHA384   12
#define SIG_RSA_SHA512   13

int rsa_check_privkey ( const rsa_context ctx)

Check a private RSA key.

Parameters
ctxRSA context to be checked
Returns
0 if successful, or an POLARSSL_ERR_RSA_XXX error code
int rsa_check_pubkey ( const rsa_context ctx)

Check a public RSA key.

Parameters
ctxRSA context to be checked
Returns
0 if successful, or an POLARSSL_ERR_RSA_XXX error code
void rsa_free ( rsa_context ctx)

Free the components of an RSA key.

Parameters
ctxRSA Context to free

Referenced by main().

int rsa_gen_key ( rsa_context ctx,
int(*)(void *)  f_rng,
void *  p_rng,
int  nbits,
int  exponent 
)

Generate an RSA keypair.

Parameters
ctxRSA context that will hold the key
f_rngRNG function
p_rngRNG parameter
nbitssize of the public key in bits
exponentpublic exponent (e.g., 65537)
Note
rsa_init() must be called beforehand to setup the RSA context.
Returns
0 if successful, or an POLARSSL_ERR_RSA_XXX error code

Referenced by main().

void rsa_init ( rsa_context ctx,
int  padding,
int  hash_id 
)

Initialize an RSA context.

Parameters
ctxRSA context to be initialized
paddingRSA_PKCS_V15 or RSA_PKCS_V21
hash_idRSA_PKCS_V21 hash identifier
Note
The hash_id parameter is actually ignored when using RSA_PKCS_V15 padding.
Currently, RSA_PKCS_V21 padding is not supported.

Referenced by main().

int rsa_pkcs1_decrypt ( rsa_context ctx,
int  mode,
int *  olen,
const unsigned char *  input,
unsigned char *  output,
int  output_max_len 
)

Do an RSA operation, then remove the message padding.

Parameters
ctxRSA context
modeRSA_PUBLIC or RSA_PRIVATE
inputbuffer holding the encrypted data
outputbuffer that will hold the plaintext
olenwill contain the plaintext length
output_max_lenmaximum length of the output buffer
Returns
0 if successful, or an POLARSSL_ERR_RSA_XXX error code
Note
The output buffer must be as large as the size of ctx->N (eg. 128 bytes if RSA-1024 is used) otherwise an error is thrown.

Referenced by RSA_private_decrypt(), and RSA_public_decrypt().

int rsa_pkcs1_encrypt ( rsa_context ctx,
int(*)(void *)  f_rng,
void *  p_rng,
int  mode,
int  ilen,
const unsigned char *  input,
unsigned char *  output 
)

Add the message padding, then do an RSA operation.

Parameters
ctxRSA context
f_rngRNG function
p_rngRNG parameter
modeRSA_PUBLIC or RSA_PRIVATE
ilencontains the plaintext length
inputbuffer holding the data to be encrypted
outputbuffer that will hold the ciphertext
Returns
0 if successful, or an POLARSSL_ERR_RSA_XXX error code
Note
The output buffer must be as large as the size of ctx->N (eg. 128 bytes if RSA-1024 is used).

Referenced by RSA_private_encrypt(), and RSA_public_encrypt().

int rsa_pkcs1_sign ( rsa_context ctx,
int  mode,
int  hash_id,
int  hashlen,
const unsigned char *  hash,
unsigned char *  sig 
)

Do a private RSA to sign a message digest.

Parameters
ctxRSA context
modeRSA_PUBLIC or RSA_PRIVATE
hash_idSIG_RSA_RAW, SIG_RSA_MD{2,4,5} or SIG_RSA_SHA{1,224,256,384,512}
hashlenmessage digest length (for SIG_RSA_RAW only)
hashbuffer holding the message digest
sigbuffer that will hold the ciphertext
Returns
0 if the signing operation was successful, or an POLARSSL_ERR_RSA_XXX error code
Note
The "sig" buffer must be as large as the size of ctx->N (eg. 128 bytes if RSA-1024 is used).
int rsa_pkcs1_verify ( rsa_context ctx,
int  mode,
int  hash_id,
int  hashlen,
const unsigned char *  hash,
unsigned char *  sig 
)

Do a public RSA and check the message digest.

Parameters
ctxpoints to an RSA public key
modeRSA_PUBLIC or RSA_PRIVATE
hash_idSIG_RSA_RAW, SIG_RSA_MD{2,4,5} or SIG_RSA_SHA{1,224,256,384,512}
hashlenmessage digest length (for SIG_RSA_RAW only)
hashbuffer holding the message digest
sigbuffer holding the ciphertext
Returns
0 if the verify operation was successful, or an POLARSSL_ERR_RSA_XXX error code
Note
The "sig" buffer must be as large as the size of ctx->N (eg. 128 bytes if RSA-1024 is used).
int rsa_private ( rsa_context ctx,
const unsigned char *  input,
unsigned char *  output 
)

Do an RSA private key operation.

Parameters
ctxRSA context
inputinput buffer
outputoutput buffer
Returns
0 if successful, or an POLARSSL_ERR_RSA_XXX error code
Note
The input and output buffers must be large enough (eg. 128 bytes if RSA-1024 is used).

Referenced by main().

int rsa_public ( rsa_context ctx,
const unsigned char *  input,
unsigned char *  output 
)

Do an RSA public key operation.

Parameters
ctxRSA context
inputinput buffer
outputoutput buffer
Returns
0 if successful, or an POLARSSL_ERR_RSA_XXX error code
Note
This function does NOT take care of message padding. Also, be sure to set input[0] = 0 or assure that input is smaller than N.
The input and output buffers must be large enough (eg. 128 bytes if RSA-1024 is used).

Referenced by main().

int rsa_self_test ( int  verbose)

Checkup routine.

Returns
0 if successful, or 1 if the test failed

Referenced by main().