Microchip® Advanced Software Framework

avr32/applications/uc3_a3_xplained-demo/touch_api.h File Reference
#include <stdint.h>
#include <stdbool.h>
#include "touch_config.h"

Data Structures

struct  qt_lib_sig_info_t
 This will be used to get the library information from the library. More...
 
struct  tag_qt_touch_lib_config_data_t
 post processing configuration data that is received from the debug interface. More...
 
struct  tag_qt_touch_lib_measure_data_t
 measured touch data that is sent for the debugging and fine tunning. More...
 
struct  tag_qt_touch_status_t
 The state of the library sensors. More...
 
struct  tag_sensor_t
 

Macros

#define BURST_FUNC_NAME   BURST_JOIN( _STATIC_PORT_PIN_CONF_, QTOUCH_SNS_PORT_COUNT, INTRABURST_1, INTRABURST_2, _POWER_OPTIMIZATION_ )
 
#define BURST_JOIN(static_flag, num_ports, intra1, intra2, pow_opt)   JOIN3( static_flag, num_ports, intra1, intra2, pow_opt )
 
#define CALCULATE_MASKS   NULL
 
#define CONCAT(A, B, C)   JOIN1( A, B, C )
 
#define DEF_QT_DI   4u
 
#define DEF_QT_DRIFT_HOLD_TIME   20 /* 4s */
 
#define DEF_QT_MAX_ON_DURATION   0 /* disabled */
 
#define DEF_QT_NEG_DRIFT_RATE   20 /* 4s per LSB */
 
#define DEF_QT_POS_DRIFT_RATE   5 /* 1s per LSB */
 
#define DEF_QT_POS_RECAL_DELAY   3u
 
#define DEF_QT_RECAL_THRESHOLD   RECAL_50 /* recal threshold = 50% of detect */
 
#define JOIN(x, y)   x ## y
 
#define JOIN1(A, B, C)   A ## B ## C
 
#define JOIN3(a, b, c, d, e)   burst_ ## a ## _ ## b ## _ ## c ## d ## _ ## e
 
#define qt_init_sensing()   qt_init_sensing_with_burst( BURST_FUNC_NAME ,CALCULATE_MASKS)
 
#define QT_MAX_NUM_ROTORS_SLIDERS   8
 
#define QT_NUM_SENSOR_STATE_BYTES   ( ( QT_NUM_CHANNELS + 7u ) / 8u )
 
#define QTLIB_BURST_AGAIN   (uint16_t) 0x0100
 
#define QTLIB_CHANNEL_REF_CHANGE   (uint16_t) 0x0008
 
#define QTLIB_IN_DETECT   (uint16_t) 0x0001
 
#define QTLIB_NO_ACTIVITY   (uint16_t) 0x0000
 
#define QTLIB_RESOLVE_CAL   (uint16_t) 0x0200
 
#define QTLIB_RESOLVE_DI   (uint16_t) 0x0800
 
#define QTLIB_RESOLVE_FILTERIN   (uint16_t) 0x0400
 
#define QTLIB_RESOLVE_POS_RECAL   (uint16_t) 0x1000
 
#define QTLIB_ROTOR_SLIDER_POS_CHANGE   (uint16_t) 0x0004
 
#define QTLIB_STATUS_CHANGE   (uint16_t) 0x0002
 
#define REG(REGISTER, SIDE)   JOIN( REGISTER, SIDE )
 
#define SNS1   SNS
 
#define SNSK1   SNSK
 
#define TICKS_PER_MS   500u
 
#define TOUCH_DATA_T   uint8_t
 

Typedefs

typedef enum tag_aks_group_t aks_group_t
 
typedef enum tag_channel_t channel_t
 
typedef enum tag_hysteresis_t hysteresis_t
 
typedef struct qt_lib_sig_info_t qt_lib_siginfo_t
 
typedef struct
tag_qt_touch_lib_config_data_t 
qt_touch_lib_config_data_t
 
typedef struct
tag_qt_touch_lib_measure_data_t 
qt_touch_lib_measure_data_t
 
typedef struct
tag_qt_touch_status_t 
qt_touch_status_t
 
typedef enum tag_recal_threshold_t recal_threshold_t
 
typedef enum tag_resolution_t resolution_t
 
typedef struct tag_sensor_t sensor_t
 
typedef enum tag_sensor_type_t sensor_type_t
 
typedef uint8_t threshold_t
 

Enumerations

enum  tag_aks_group_t {
  NO_AKS_GROUP,
  AKS_GROUP_1,
  AKS_GROUP_2,
  AKS_GROUP_3,
  AKS_GROUP_4,
  AKS_GROUP_5,
  AKS_GROUP_6,
  AKS_GROUP_7,
  NO_AKS_GROUP,
  AKS_GROUP_1,
  AKS_GROUP_2,
  AKS_GROUP_3,
  AKS_GROUP_4,
  AKS_GROUP_5,
  AKS_GROUP_6,
  AKS_GROUP_7
}
 
enum  tag_channel_t {
  CHANNEL_0,
  CHANNEL_1,
  CHANNEL_2,
  CHANNEL_3,
  CHANNEL_4,
  CHANNEL_5,
  CHANNEL_6,
  CHANNEL_7,
  CHANNEL_8,
  CHANNEL_9,
  CHANNEL_10,
  CHANNEL_11,
  CHANNEL_12,
  CHANNEL_13,
  CHANNEL_14,
  CHANNEL_15,
  CHANNEL_16,
  CHANNEL_17,
  CHANNEL_18,
  CHANNEL_19,
  CHANNEL_20,
  CHANNEL_21,
  CHANNEL_22,
  CHANNEL_23,
  CHANNEL_24,
  CHANNEL_25,
  CHANNEL_26,
  CHANNEL_27,
  CHANNEL_28,
  CHANNEL_29,
  CHANNEL_30,
  CHANNEL_31
}
 
enum  tag_hysteresis_t {
  HYST_50,
  HYST_25,
  HYST_12_5,
  HYST_6_25,
  HYST_50,
  HYST_25,
  HYST_12_5,
  HYST_6_25
}
 
enum  tag_recal_threshold_t {
  RECAL_100,
  RECAL_50,
  RECAL_25,
  RECAL_12_5,
  RECAL_6_25,
  RECAL_100 = 0,
  RECAL_50,
  RECAL_25,
  RECAL_12_5,
  RECAL_6_25
}
 
enum  tag_resolution_t {
  RES_1_BIT,
  RES_2_BIT,
  RES_3_BIT,
  RES_4_BIT,
  RES_5_BIT,
  RES_6_BIT,
  RES_7_BIT,
  RES_8_BIT,
  RES_1_BIT,
  RES_2_BIT,
  RES_3_BIT,
  RES_4_BIT,
  RES_5_BIT,
  RES_6_BIT,
  RES_7_BIT,
  RES_8_BIT
}
 
enum  tag_sensor_type_t {
  SENSOR_TYPE_UNASSIGNED,
  SENSOR_TYPE_KEY,
  SENSOR_TYPE_ROTOR,
  SENSOR_TYPE_SLIDER,
  SENSOR_TYPE_UNASSIGNED,
  SENSOR_TYPE_KEY,
  SENSOR_TYPE_ROTOR,
  SENSOR_TYPE_SLIDER
}
 

Functions

void BURST_FUNC_NAME (TOUCH_DATA_T mask_index)
 
void calc_masks (void)
 
void qt_calibrate_sensing (void)
 
void qt_enable_key (channel_t channel, aks_group_t aks_group, threshold_t detect_threshold, hysteresis_t detect_hysteresis)
 
void qt_enable_rotor (channel_t from_channel, channel_t to_channel, aks_group_t aks_group, threshold_t detect_threshold, hysteresis_t detect_hysteresis, resolution_t angle_resolution, uint8_t angle_hysteresis)
 
void qt_enable_slider (channel_t from_channel, channel_t to_channel, aks_group_t aks_group, threshold_t detect_threshold, hysteresis_t detect_hysteresis, resolution_t position_resolution, uint8_t position_hysteresis)
 
void qt_get_library_sig (qt_lib_siginfo_t *lib_sig_ptr)
 
int16_t qt_get_sensor_delta (uint8_t sensor)
 
void qt_init_sensing_with_burst (void(*burst_function)(TOUCH_DATA_T mask_index), void(*calculate_masks)(void))
 
uint16_t qt_measure_sensors (uint16_t current_time_ms)
 
void qt_reset_sensing (void)
 

Variables

void(* burst_proc )(TOUCH_DATA_T mask_index)
 
uint16_t lib_status_flags
 
qt_touch_lib_config_data_t qt_config_data
 
void(* qt_filter_callback )(void)
 
qt_touch_lib_measure_data_t qt_measure_data
 
uint16_t qt_measurement_period_msec
 
sensor_t sensors [QT_NUM_CHANNELS]
 

#define BURST_FUNC_NAME   BURST_JOIN( _STATIC_PORT_PIN_CONF_, QTOUCH_SNS_PORT_COUNT, INTRABURST_1, INTRABURST_2, _POWER_OPTIMIZATION_ )
#define BURST_JOIN (   static_flag,
  num_ports,
  intra1,
  intra2,
  pow_opt 
)    JOIN3( static_flag, num_ports, intra1, intra2, pow_opt )
#define CALCULATE_MASKS   NULL
#define CONCAT (   A,
  B,
  C 
)    JOIN1( A, B, C )
#define DEF_QT_DI   4u

Referenced by qt_set_parameters().

#define DEF_QT_DRIFT_HOLD_TIME   20 /* 4s */

Referenced by qt_set_parameters().

#define DEF_QT_MAX_ON_DURATION   0 /* disabled */

Referenced by qt_set_parameters().

#define DEF_QT_NEG_DRIFT_RATE   20 /* 4s per LSB */

Referenced by qt_set_parameters().

#define DEF_QT_POS_DRIFT_RATE   5 /* 1s per LSB */

Referenced by qt_set_parameters().

#define DEF_QT_POS_RECAL_DELAY   3u

Referenced by qt_set_parameters().

#define DEF_QT_RECAL_THRESHOLD   RECAL_50 /* recal threshold = 50% of detect */

Referenced by qt_set_parameters().

#define JOIN (   x,
 
)    x ## y
#define JOIN1 (   A,
  B,
  C 
)    A ## B ## C
#define JOIN3 (   a,
  b,
  c,
  d,
 
)    burst_ ## a ## _ ## b ## _ ## c ## d ## _ ## e
#define qt_init_sensing ( )    qt_init_sensing_with_burst( BURST_FUNC_NAME ,CALCULATE_MASKS)

Referenced by touch_init().

#define QT_MAX_NUM_ROTORS_SLIDERS   8

Referenced by Transmit_State().

#define QT_NUM_SENSOR_STATE_BYTES   ( ( QT_NUM_CHANNELS + 7u ) / 8u )

Referenced by Transmit_State().

#define QTLIB_BURST_AGAIN   (uint16_t) 0x0100

Referenced by touch_handler().

#define QTLIB_CHANNEL_REF_CHANGE   (uint16_t) 0x0008

Referenced by QDebug_SendData().

#define QTLIB_IN_DETECT   (uint16_t) 0x0001
#define QTLIB_NO_ACTIVITY   (uint16_t) 0x0000
#define QTLIB_RESOLVE_CAL   (uint16_t) 0x0200
#define QTLIB_RESOLVE_DI   (uint16_t) 0x0800
#define QTLIB_RESOLVE_FILTERIN   (uint16_t) 0x0400
#define QTLIB_RESOLVE_POS_RECAL   (uint16_t) 0x1000
#define QTLIB_ROTOR_SLIDER_POS_CHANGE   (uint16_t) 0x0004

Referenced by QDebug_SendData().

#define QTLIB_STATUS_CHANGE   (uint16_t) 0x0002

Referenced by QDebug_SendData().

#define REG (   REGISTER,
  SIDE 
)    JOIN( REGISTER, SIDE )
#define SNS1   SNS
#define SNSK1   SNSK
#define TICKS_PER_MS   500u

Referenced by Transmit_Global_Config().

#define TOUCH_DATA_T   uint8_t

typedef enum tag_channel_t channel_t
typedef struct tag_sensor_t sensor_t
typedef uint8_t threshold_t

Enumerator
NO_AKS_GROUP 
AKS_GROUP_1 
AKS_GROUP_2 
AKS_GROUP_3 
AKS_GROUP_4 
AKS_GROUP_5 
AKS_GROUP_6 
AKS_GROUP_7 
NO_AKS_GROUP 
AKS_GROUP_1 
AKS_GROUP_2 
AKS_GROUP_3 
AKS_GROUP_4 
AKS_GROUP_5 
AKS_GROUP_6 
AKS_GROUP_7 
Enumerator
CHANNEL_0 
CHANNEL_1 
CHANNEL_2 
CHANNEL_3 
CHANNEL_4 
CHANNEL_5 
CHANNEL_6 
CHANNEL_7 
CHANNEL_8 
CHANNEL_9 
CHANNEL_10 
CHANNEL_11 
CHANNEL_12 
CHANNEL_13 
CHANNEL_14 
CHANNEL_15 
CHANNEL_16 
CHANNEL_17 
CHANNEL_18 
CHANNEL_19 
CHANNEL_20 
CHANNEL_21 
CHANNEL_22 
CHANNEL_23 
CHANNEL_24 
CHANNEL_25 
CHANNEL_26 
CHANNEL_27 
CHANNEL_28 
CHANNEL_29 
CHANNEL_30 
CHANNEL_31 
Enumerator
HYST_50 
HYST_25 
HYST_12_5 
HYST_6_25 
HYST_50 
HYST_25 
HYST_12_5 
HYST_6_25 
Enumerator
RECAL_100 
RECAL_50 
RECAL_25 
RECAL_12_5 
RECAL_6_25 
RECAL_100 
RECAL_50 
RECAL_25 
RECAL_12_5 
RECAL_6_25 
Enumerator
RES_1_BIT 
RES_2_BIT 
RES_3_BIT 
RES_4_BIT 
RES_5_BIT 
RES_6_BIT 
RES_7_BIT 
RES_8_BIT 
RES_1_BIT 
RES_2_BIT 
RES_3_BIT 
RES_4_BIT 
RES_5_BIT 
RES_6_BIT 
RES_7_BIT 
RES_8_BIT 
Enumerator
SENSOR_TYPE_UNASSIGNED 
SENSOR_TYPE_KEY 
SENSOR_TYPE_ROTOR 
SENSOR_TYPE_SLIDER 
SENSOR_TYPE_UNASSIGNED 
SENSOR_TYPE_KEY 
SENSOR_TYPE_ROTOR 
SENSOR_TYPE_SLIDER 

void BURST_FUNC_NAME ( TOUCH_DATA_T  mask_index)
void calc_masks ( void  )
void qt_calibrate_sensing ( void  )
void qt_enable_key ( channel_t  channel,
aks_group_t  aks_group,
threshold_t  detect_threshold,
hysteresis_t  detect_hysteresis 
)

Referenced by touch_init().

void qt_enable_rotor ( channel_t  from_channel,
channel_t  to_channel,
aks_group_t  aks_group,
threshold_t  detect_threshold,
hysteresis_t  detect_hysteresis,
resolution_t  angle_resolution,
uint8_t  angle_hysteresis 
)
void qt_enable_slider ( channel_t  from_channel,
channel_t  to_channel,
aks_group_t  aks_group,
threshold_t  detect_threshold,
hysteresis_t  detect_hysteresis,
resolution_t  position_resolution,
uint8_t  position_hysteresis 
)

Referenced by touch_init().

void qt_get_library_sig ( qt_lib_siginfo_t lib_sig_ptr)

Referenced by QDebug_Init().

int16_t qt_get_sensor_delta ( uint8_t  sensor)
void qt_init_sensing_with_burst ( void(*)(TOUCH_DATA_T mask_index)  burst_function,
void(*)(void)  calculate_masks 
)
uint16_t qt_measure_sensors ( uint16_t  current_time_ms)

Referenced by touch_handler().

void qt_reset_sensing ( void  )

void(* burst_proc)(TOUCH_DATA_T mask_index)
uint16_t lib_status_flags
void(* qt_filter_callback)(void)

Referenced by qt_set_parameters().

qt_touch_lib_measure_data_t qt_measure_data
uint16_t qt_measurement_period_msec