UC3-A3 Xplained Application Touch functions.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include "board.h"
#include "gpio.h"
#include "sysclk.h"
#include "tc.h"
#include "uc3-a3_xplained_demo.h"
#include "touch_api.h"
#include "QDebug.h"
#include "QDebugTransport.h"
Macros | |
#define | _DEBUG_INTERFACE_ |
#define | TOUCH_MEASUREMENT_PERIOD_MS 25 |
#define | TOUCH_MEASUREMENT_TC (&AVR32_TC1) |
#define | TOUCH_MEASUREMENT_TC_CHANNEL 0 |
#define | TOUCH_MEASUREMENT_TC_IRQ AVR32_TC1_IRQ0 |
#define | TOUCH_MEASUREMENT_TC_IRQ_GROUP AVR32_TC1_IRQ_GROUP |
Functions | |
static void | init_timer (void) |
Initializes the touch measurement timer. More... | |
ISR (tc_irq, TOUCH_MEASUREMENT_TC_IRQ_GROUP, AVR32_INTC_INT0) | |
Touch measurement timer interrupt. More... | |
static void | qt_set_parameters (void) |
Initializes the touch library configuration. More... | |
void | touch_handler (void) |
Measure touch sensors and do appropriate action. More... | |
void | touch_init (void) |
Initialize touch sensors. More... | |
Variables | |
static volatile uint16_t | current_time_ms = 0 |
Current time in ms. More... | |
uint16_t | measurement_period_ms = TOUCH_MEASUREMENT_PERIOD_MS |
Time measurement period in ms. More... | |
static volatile bool | time_to_measure_touch = true |
Touch measurement flag. More... | |
#define _DEBUG_INTERFACE_ |
#define TOUCH_MEASUREMENT_PERIOD_MS 25 |
#define TOUCH_MEASUREMENT_TC (&AVR32_TC1) |
Referenced by init_timer(), and ISR().
#define TOUCH_MEASUREMENT_TC_CHANNEL 0 |
Referenced by init_timer(), and ISR().
#define TOUCH_MEASUREMENT_TC_IRQ AVR32_TC1_IRQ0 |
Referenced by init_timer().
#define TOUCH_MEASUREMENT_TC_IRQ_GROUP AVR32_TC1_IRQ_GROUP |
|
static |
Initializes the touch measurement timer.
We need a timer that triggers approx. every millisecond. The touch library seems to need this as time-base.
Software trigger effect on TIOB.
External event effect on TIOB.
RC compare effect on TIOB.
RB compare effect on TIOB.
Software trigger effect on TIOA.
External event effect on TIOA.
RC compare effect on TIOA: toggle.
RA compare effect on TIOA: toggle.
Waveform selection
External event trigger enable.
External event selection.
External event edge selection.
Counter disable when RC compare.
Counter clock stopped with RC compare.
Burst signal selection.
Clock inversion selection.
Internal source clock 3 (fPBA / 8).
References tc_waveform_opt_t::channel, Disable_global_interrupt, Enable_global_interrupt, tc_interrupt_t::etrgs, INTC_register_interrupt(), sysclk_enable_peripheral_clock(), sysclk_get_pba_hz(), TC_CLOCK_SOURCE_TC3, tc_configure_interrupts(), TC_EVT_EFFECT_NOOP, tc_init_waveform(), tc_interrupt, tc_irq(), TC_SEL_NO_EDGE, tc_start(), TC_WAVEFORM_SEL_UP_MODE_RC_TRIGGER, tc_write_rc(), TOUCH_MEASUREMENT_TC, TOUCH_MEASUREMENT_TC_CHANNEL, and TOUCH_MEASUREMENT_TC_IRQ.
Referenced by touch_init().
ISR | ( | tc_irq | , |
TOUCH_MEASUREMENT_TC_IRQ_GROUP | , | ||
AVR32_INTC_INT0 | |||
) |
Touch measurement timer interrupt.
Initiates periodically touch measurements. Triggers every 1ms and will set the flag time_to_measure_touch every TOUCH_MEASUREMENT_PERIOD_MS ms.
References current_time_ms, measurement_period_ms, tc_read_sr(), time_to_measure_touch, TOUCH_MEASUREMENT_TC, and TOUCH_MEASUREMENT_TC_CHANNEL.
|
static |
Initializes the touch library configuration.
Sets the correct configuration for the QTouch library.
References DEF_QT_DI, DEF_QT_DRIFT_HOLD_TIME, DEF_QT_MAX_ON_DURATION, DEF_QT_NEG_DRIFT_RATE, DEF_QT_POS_DRIFT_RATE, DEF_QT_POS_RECAL_DELAY, DEF_QT_RECAL_THRESHOLD, NULL, qt_config_data, tag_qt_touch_lib_config_data_t::qt_di, tag_qt_touch_lib_config_data_t::qt_drift_hold_time, qt_filter_callback, tag_qt_touch_lib_config_data_t::qt_max_on_duration, tag_qt_touch_lib_config_data_t::qt_neg_drift_rate, tag_qt_touch_lib_config_data_t::qt_pos_drift_rate, tag_qt_touch_lib_config_data_t::qt_pos_recal_delay, and tag_qt_touch_lib_config_data_t::qt_recal_threshold.
Referenced by touch_init().
void touch_handler | ( | void | ) |
Measure touch sensors and do appropriate action.
References current_time_ms, QDebug_ProcessCommands(), QDebug_SendData(), qt_measure_data, qt_measure_sensors(), tag_qt_touch_lib_measure_data_t::qt_touch_status, QTLIB_BURST_AGAIN, tag_qt_touch_status_t::rotor_slider_values, tag_qt_touch_status_t::sensor_states, tc_write_rb(), and time_to_measure_touch.
Referenced by main().
void touch_init | ( | void | ) |
Initialize touch sensors.
The touch channels are connected on the GPIO controller 4 which is a part of port X
Touch Button: GPIO 98 SNSK1 CHANNEL1_SNS 99 SNS1 CHANNEL1_SNSK
Touch Slider: 100 SNS0 CHANNEL2_SNS 101 SNSK0 CHANNEL2_SNSK 102 SNS1 CHANNEL3_SNS 103 SNSK1 CHANNEL3_SNSK 104 SNS2 CHANNEL4_SNS 105 SNSK2 CHANNEL4_SNSK
References CHANNEL_1, CHANNEL_2, CHANNEL_4, HYST_12_5, init_timer(), NO_AKS_GROUP, QDebug_Init(), QDebug_ProcessCommands(), qt_enable_key(), qt_enable_slider(), qt_init_sensing, qt_set_parameters(), RES_8_BIT, and sysclk_enable_peripheral_clock().
Referenced by main().
|
static |
Current time in ms.
This is required for the touch library. The time is updated in the timer ISR so this must be volatile.
Referenced by ISR(), and touch_handler().
uint16_t measurement_period_ms = TOUCH_MEASUREMENT_PERIOD_MS |
Time measurement period in ms.
Needs to be global since it is required for the QDebug module.
Referenced by ISR(), Set_Measurement_Period(), and Transmit_Global_Config().
Touch measurement flag.
Indicates when a new touch measurement should be done. This is set in the timer ISR so this must be volatile.
Referenced by ISR(), and touch_handler().