Common Sensor Service Compass Calibration Example.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include <stdio.h>
#include <asf.h>
#include <led.h>
Macros | |
#define | ALL_LEDS (LED1 | LED2 | LED3 | LED4) |
#define | NUM_BLINK_LEDS (4) |
#define | PROMPT_LED LED4 /* Blink while waiting for user input */ |
#define | SWITCH_PRESSED gpio_pin_is_low(GPIO_PUSH_BUTTON_0) |
Functions | |
int | main (void) |
Compass / magnetometer calibration application. More... | |
static void | prompt_user (char *prompt_string) |
User prompt routine. More... | |
Variables | |
static const uint32_t | led_array [NUM_BLINK_LEDS] = {LED1, LED2, LED3, LED4} |
#define ALL_LEDS (LED1 | LED2 | LED3 | LED4) |
Referenced by main(), and prompt_user().
#define NUM_BLINK_LEDS (4) |
Referenced by main().
Referenced by prompt_user().
#define SWITCH_PRESSED gpio_pin_is_low(GPIO_PUSH_BUTTON_0) |
Referenced by prompt_user().
int main | ( | void | ) |
Compass / magnetometer calibration application.
This application illustrates the use of the sensor_calibrate() function for compass/magnetometer calibration. It prompts the user (via serial output) to manipulate the sensor board and press a button to continue.
The calibration process is used to correct for fixed magnetic forces present on the board where the compass is mounted. If uncorrected, these fixed forces will prevent accurate measurement of the actual external magnetic forces (e.g. magnetic North).
The calibration sequence requires three steps. During each step, the board is placed in a specific orientation, and the user presses the button on the board to trigger a compass sensor reading.
The three orientations are:
After Step 3 is completed, the calibration values for the sensor are calculated and are written to non-volatile (flash) memory on the microcontroller. These values will continue to be used for future compass heading readings.
References ALL_LEDS, delay_ms, sensor_data_t::heading, led_array, MANUAL_CALIBRATE, NULL, NUM_BLINK_LEDS, prompt_user(), sensor_data_t::scaled, sensor_attach(), sensor_calibrate(), SENSOR_ERR_IO, sensor_get_heading(), sensor_platform_init(), and SENSOR_TYPE_COMPASS.
|
static |
User prompt routine.
This routine prompts the user to press the button and then waits for him to do so.
References ALL_LEDS, delay_ms, PROMPT_LED, and SWITCH_PRESSED.
Referenced by main().
|
static |
Referenced by main().