lwIP Operating System abstraction
#include "lwip/opt.h"
#include "lwip/sys.h"
#include "lwip/def.h"
#include "lwip/memp.h"
#include "lwip/tcpip.h"
Data Structures | |
struct | sswt_cb |
Struct used for sys_sem_wait_timeout() to tell wether the time has run out or the semaphore has really become available. More... | |
Functions | |
static void | sswt_handler (void *arg) |
Timeout handler function for sys_sem_wait_timeout() More... | |
void | sys_mbox_fetch (sys_mbox_t mbox, void **msg) |
Wait (forever) for a message to arrive in an mbox. More... | |
void | sys_msleep (u32_t ms) |
Sleep for some ms. More... | |
void | sys_sem_wait (sys_sem_t sem) |
Wait (forever) for a semaphore to become available. More... | |
int | sys_sem_wait_timeout (sys_sem_t sem, u32_t timeout) |
Wait for a semaphore with timeout (specified in ms) More... | |
void | sys_timeout (u32_t msecs, sys_timeout_handler h, void *arg) |
Create a one-shot timer (aka timeout). More... | |
void | sys_untimeout (sys_timeout_handler h, void *arg) |
Go through timeout list (for this task only) and remove the first matching entry, even though the timeout has not triggered yet. More... | |
|
static |
Timeout handler function for sys_sem_wait_timeout()
arg | struct sswt_cb* used to signal a semaphore and end waiting. |
References sswt_cb::psem, sys_sem_signal(), and sswt_cb::timeflag.
Referenced by sys_sem_wait_timeout().
void sys_mbox_fetch | ( | sys_mbox_t | mbox, |
void ** | msg | ||
) |
Wait (forever) for a message to arrive in an mbox.
While waiting, timeouts (for this thread) are processed.
mbox | the mbox to fetch the message from |
msg | the place to store the message |
References sys_timeo::arg, arg, sys_timeo::h, LOCK_TCPIP_CORE, LWIP_DEBUGF, memp_free(), sys_timeo::next, sys_timeouts::next, NULL, sys_arch_mbox_fetch(), SYS_ARCH_TIMEOUT, sys_arch_timeouts(), SYS_DEBUG, sys_timeo::time, and UNLOCK_TCPIP_CORE.
void sys_msleep | ( | u32_t | ms | ) |
Sleep for some ms.
Timeouts are processed while sleeping.
ms | number of milliseconds to sleep |
References sys_sem_free(), sys_sem_new(), and sys_sem_wait_timeout().
void sys_sem_wait | ( | sys_sem_t | sem | ) |
Wait (forever) for a semaphore to become available.
While waiting, timeouts (for this thread) are processed.
sem | semaphore to wait for |
References sys_timeo::arg, arg, sys_timeo::h, LWIP_DEBUGF, memp_free(), sys_timeo::next, sys_timeouts::next, NULL, sys_arch_sem_wait(), SYS_ARCH_TIMEOUT, sys_arch_timeouts(), SYS_DEBUG, and sys_timeo::time.
int sys_sem_wait_timeout | ( | sys_sem_t | sem, |
u32_t | timeout | ||
) |
Wait for a semaphore with timeout (specified in ms)
sem | semaphore to wait |
timeout | timeout in ms (0: wait forever) |
References sswt_cb::psem, sswt_handler(), sys_sem_wait, sys_timeout(), sys_untimeout(), and sswt_cb::timeflag.
Referenced by sys_msleep().
void sys_timeout | ( | u32_t | msecs, |
sys_timeout_handler | h, | ||
void * | arg | ||
) |
Create a one-shot timer (aka timeout).
Timeouts are processed in the following cases:
msecs | time in milliseconds after that the timer should expire |
h | callback function to call when msecs have elapsed |
arg | argument to pass to the callback function |
References sys_timeo::arg, arg, sys_timeo::h, LWIP_ASSERT, LWIP_DEBUGF, memp_malloc(), sys_timeo::next, sys_timeouts::next, NULL, sys_arch_timeouts(), SYS_DEBUG, sys_timeo::time, and U32_F.
Referenced by sys_sem_wait_timeout(), and tcpip_thread().
void sys_untimeout | ( | sys_timeout_handler | h, |
void * | arg | ||
) |
Go through timeout list (for this task only) and remove the first matching entry, even though the timeout has not triggered yet.
h | callback function that would be called by the timeout |
arg | callback argument that would be passed to h |
References sys_timeo::arg, sys_timeo::h, LWIP_ASSERT, memp_free(), sys_timeo::next, sys_timeouts::next, NULL, sys_arch_timeouts(), and sys_timeo::time.
Referenced by sys_sem_wait_timeout(), and tcpip_thread().