Data Structures | |
union | Navauto_mov_bitfield_status |
struct | Navauto_mov_state |
Structure to store the status from function navauto_mov() More... | |
Macros | |
Definition of the directory limitations of the file list | |
#define | NAVAUTO_MODE_DISKS 0 |
#define | NAVAUTO_MODE_DISK 1 |
#define | NAVAUTO_MODE_DIRONLY 2 |
#define | NAVAUTO_MODE_DIRSUB 3 |
#define | NAVAUTO_MODE_NB 4 |
Definition of the random states | |
#define | NAVAUTO_RAND_OFF 0 |
#define | NAVAUTO_RAND_ON 1 |
Status list of function navauto_mov() | |
#define | NAVAUTO_MOV_OK 0 |
#define | NAVAUTO_MOV_OK_LOOP 1 |
#define | NAVAUTO_MOV_EMPTY 2 |
#define | NAVAUTO_MOV_DISKNOPRESENT 3 |
#define | NAVAUTO_MOV_DISKERROR 4 |
Typedefs | |
typedef uint8_t | Navauto_mode |
Structure to store the directory limitation of the file list. More... | |
typedef uint8_t | Navauto_rand |
Structure to store the random state. More... | |
Enumerations | |
enum | navauto_mov_options_t { NAVAUTO_MOV_OPTS_NONE = 0, NAVAUTO_MOV_OPTS_STAY_CURRENT_DIR = 1 } |
Functions | |
uint16_t | navauto_close (void) |
This function closes the file list. More... | |
Navauto_mode | navauto_getmode (void) |
This function returns the directory limitation of the file list. More... | |
uint16_t | navauto_getnb (void) |
This function returns the file list size. More... | |
uint16_t | navauto_getpos (void) |
This function returns the current position in the file list. More... | |
Navauto_rand | navauto_getrand (void) |
This function returns the random state used. More... | |
void | navauto_init (const FS_STRING sz_filterext) |
This function initializes the file extension filter used to create the file list. More... | |
Navauto_mov_state | navauto_mov (bool b_direction, navauto_mov_options_t options) |
This function jumps to the next or previous file in file list. More... | |
bool | navauto_open (bool b_playlist, uint16_t pos) |
This function opens a file list at the current position in navigator. More... | |
bool | navauto_setmode (Navauto_mode exp_mode) |
This function sets the directory limitation of the file list. More... | |
bool | navauto_setpos (uint16_t u16_pos) |
This function selects a new position in file list. More... | |
void | navauto_setrand (Navauto_rand rand) |
This function changes the random state. More... | |
#define NAVAUTO_MODE_DIRONLY 2 |
#define NAVAUTO_MODE_DIRSUB 3 |
#define NAVAUTO_MODE_DISK 1 |
#define NAVAUTO_MODE_DISKS 0 |
#define NAVAUTO_MODE_NB 4 |
#define NAVAUTO_MOV_DISKERROR 4 |
Referenced by navauto_mov_playlist().
#define NAVAUTO_MOV_DISKNOPRESENT 3 |
#define NAVAUTO_MOV_EMPTY 2 |
Referenced by navauto_mov_explorer(), navauto_mov_explorer_is_file(), and navauto_mov_explorer_new_dir().
#define NAVAUTO_MOV_OK 0 |
#define NAVAUTO_MOV_OK_LOOP 1 |
#define NAVAUTO_RAND_OFF 0 |
#define NAVAUTO_RAND_ON 1 |
typedef uint8_t Navauto_mode |
Structure to store the directory limitation of the file list.
typedef uint8_t Navauto_rand |
Structure to store the random state.
uint16_t navauto_close | ( | void | ) |
This function closes the file list.
@return If a play list file is open then it is the last position in the file list else it is the directory level corresponding at the last selected file
//! At the end of this routine, the selected file of current navigator is : //! - the play list file (in case of a play list file has been opened) //! - the last selected file (in other case) //!
References g_navauto_b_playlist, g_navauto_u16_dir_level, g_navauto_u16_pos, and pl_main_close().
Referenced by ai_usb_ms_audio_context_restore(), ai_usb_ms_audio_ctrl_resume(), ai_usb_ms_audio_nav_eof_occur(), ai_usb_ms_audio_nav_mov(), ai_usb_ms_audio_nav_playfile(), and ai_usb_ms_specific_audio_nav_playlist_play_link().
Navauto_mode navauto_getmode | ( | void | ) |
This function returns the directory limitation of the file list.
@return Used navigation mode (NAVAUTO_MODE_DISKS, NAVAUTO_MODE_DIRONLY, NAVAUTO_MODE_DIRSUB)
//! This parameter is ignored then a play list file is selected //!
References g_navauto_exp_mode.
Referenced by ai_usb_ms_audio_context_save(), and ai_usb_ms_audio_nav_expmode_get().
uint16_t navauto_getnb | ( | void | ) |
This function returns the file list size.
References g_navauto_u16_nb.
Referenced by ai_usb_ms_audio_nav_nb().
uint16_t navauto_getpos | ( | void | ) |
This function returns the current position in the file list.
References g_navauto_u16_pos.
Referenced by ai_usb_ms_audio_nav_getpos(), and ai_usb_ms_specific_audio_nav_playlist_play_link().
Navauto_rand navauto_getrand | ( | void | ) |
This function returns the random state used.
References g_navauto_rand.
Referenced by ai_usb_ms_specific_audio_nav_playlist_play_link(), navauto_open(), and navauto_setpos().
void navauto_init | ( | const FS_STRING | sz_filterext | ) |
This function initializes the file extension filter used to create the file list.
@param sz_filterext file extension filter
//! This parameter is ignored then a play list file is selected //!
References g_navauto_filter, g_navauto_u16_dir_level_root, and g_navauto_u16_nb.
Referenced by ai_usb_ms_init_drive().
Navauto_mov_state navauto_mov | ( | bool | b_direction, |
navauto_mov_options_t | options | ||
) |
This function jumps to the next or previous file in file list.
@param b_direction jump direction (FS_FIND_NEXT or FS_FIND_PREV) @param options jump direction (FS_FIND_NEXT or FS_FIND_PREV) @return the status of the action
//! When the random is ON, the direction is ignored //!
References g_navauto_b_playlist, navauto_mov_explorer(), and navauto_mov_playlist().
Referenced by ai_usb_ms_audio_nav_eof_occur(), ai_usb_ms_audio_nav_mov(), navauto_open(), and navauto_setpos().
This function opens a file list at the current position in navigator.
b_playlist | if true then the current selected file is a play list file to open else create a file list with files included in a disk part |
pos | If b_playlist true, then position in the play list to start else folder level of the current position |
References FS_FIND_NEXT, FS_FIND_PREV, g_navauto_b_playlist, g_navauto_filter, g_navauto_u16_dir_level, g_navauto_u16_dir_level_root, g_navauto_u16_nb, g_navauto_u16_pos, index, nav_dir_gotoparent(), nav_file_checkext(), nav_filelist_reset(), nav_filelist_set(), nav_filelist_validpos(), nav_getindex(), nav_gotoindex(), navauto_getrand(), navauto_mov(), navauto_mov_explorer(), navauto_mov_explorer_reset(), NAVAUTO_MOV_OK, NAVAUTO_MOV_OK_LOOP, NAVAUTO_MOV_OPTS_NONE, navauto_rand_init(), NAVAUTO_RAND_OFF, navauto_setrand(), pl_main_open(), pl_nav_getnbfile(), pl_nav_setpos(), state, status, Navauto_mov_state::status, Fs_index::u16_entry_pos_sel_file, Fs_index::u32_cluster_sel_dir, and Fs_index::u8_lun.
Referenced by ai_usb_ms_audio_context_restore(), ai_usb_ms_audio_ctrl_resume(), ai_usb_ms_audio_nav_playfile(), ai_usb_ms_specific_audio_nav_playlist_play_link(), and navauto_setmode().
bool navauto_setmode | ( | Navauto_mode | exp_mode | ) |
This function sets the directory limitation of the file list.
@param exp_mode mode to select (NAVAUTO_MODE_DISKS, NAVAUTO_MODE_DIRONLY, NAVAUTO_MODE_DIRSUB) @return true, mode changed @return false, mode can't be changed (note: the selected file must be close)
//! This parameter is ignored then a play list file is selected //! When the mode change, the folder level is reseted at the current position. //!
References g_navauto_b_playlist, g_navauto_exp_mode, and navauto_open().
Referenced by ai_usb_ms_audio_context_restore(), and ai_usb_ms_audio_nav_expmode_set().
bool navauto_setpos | ( | uint16_t | u16_pos | ) |
This function selects a new position in file list.
u16_pos | new position to select |
References FS_FIND_NEXT, FS_FIND_PREV, g_navauto_u16_pos, navauto_getrand(), navauto_mov(), NAVAUTO_MOV_OK, NAVAUTO_MOV_OPTS_NONE, navauto_setrand(), state, and Navauto_mov_state::status.
Referenced by ai_usb_ms_audio_nav_setpos().
void navauto_setrand | ( | Navauto_rand | rand | ) |
This function changes the random state.
rand | random mode to use |
References g_navauto_rand, g_navauto_rand_tab, g_navauto_u16_pos, and navauto_rand_init().
Referenced by ai_usb_ms_audio_nav_shuffle_set(), ai_usb_ms_new_connection(), ai_usb_ms_specific_audio_nav_playlist_play_link(), navauto_open(), and navauto_setpos().