#include <string.h>
#include <stdio.h>
#include "compiler.h"
#include "s_pushb.h"
#include "gpio.h"
#include "FreeRTOS.h"
Macros | |
#define | PB1_POSITION GPIO_PUSH_BUTTON_0 |
#define | PB2_POSITION GPIO_PUSH_BUTTON_1 |
#define | PB3_POSITION GPIO_PUSH_BUTTON_2 |
#define | PUSHB_EVENT_PRESS true |
#define | PUSHB_EVENT_RELEASE false |
#define | SENSOR_PB1_CONFIG_FILE "CFG/PB1.TXT" |
#define | SENSOR_PB2_CONFIG_FILE "CFG/PB2.TXT" |
#define | SENSOR_PB3_CONFIG_FILE "CFG/PB3.TXT" |
Functions | |
bool | b_pushb1_get_value (char *buf) |
Get a pushbutton current state. More... | |
bool | b_pushb2_get_value (char *buf) |
Get a pushbutton current state. More... | |
bool | b_pushb3_get_value (char *buf) |
Get a pushbutton current state. More... | |
Variables | |
const signed portCHAR * | acpc_pushb_events [2] |
static bool | b_pushb1 = PUSHB_EVENT_RELEASE |
static bool | b_pushb2 = PUSHB_EVENT_RELEASE |
static bool | b_pushb3 = PUSHB_EVENT_RELEASE |
#define PB1_POSITION GPIO_PUSH_BUTTON_0 |
Referenced by b_pushb1_get_value().
#define PB2_POSITION GPIO_PUSH_BUTTON_1 |
Referenced by b_pushb2_get_value().
#define PB3_POSITION GPIO_PUSH_BUTTON_2 |
Referenced by b_pushb3_get_value().
#define PUSHB_EVENT_PRESS true |
Pushbutton events.
Referenced by b_pushb1_get_value(), b_pushb2_get_value(), and b_pushb3_get_value().
#define PUSHB_EVENT_RELEASE false |
Referenced by b_pushb1_get_value(), b_pushb2_get_value(), and b_pushb3_get_value().
#define SENSOR_PB1_CONFIG_FILE "CFG/PB1.TXT" |
#define SENSOR_PB2_CONFIG_FILE "CFG/PB2.TXT" |
#define SENSOR_PB3_CONFIG_FILE "CFG/PB3.TXT" |
bool b_pushb1_get_value | ( | char * | buf | ) |
Get a pushbutton current state.
buf | char buffer in which the push button state is stored. |
References acpc_pushb_events, b_pushb1, gpio_get_pin_value(), PB1_POSITION, PUSHB_EVENT_PRESS, PUSHB_EVENT_RELEASE, and sprintf().
Referenced by device_full_custom_task().
bool b_pushb2_get_value | ( | char * | buf | ) |
Get a pushbutton current state.
buf | char buffer in which the push button state is stored. |
References acpc_pushb_events, b_pushb2, gpio_get_pin_value(), PB2_POSITION, PUSHB_EVENT_PRESS, PUSHB_EVENT_RELEASE, and sprintf().
Referenced by device_full_custom_task().
bool b_pushb3_get_value | ( | char * | buf | ) |
Get a pushbutton current state.
buf | char buffer in which the push button state is stored. |
References acpc_pushb_events, b_pushb3, gpio_get_pin_value(), PB3_POSITION, PUSHB_EVENT_PRESS, PUSHB_EVENT_RELEASE, and sprintf().
const signed portCHAR* acpc_pushb_events[2] |
Pushbutton events string.
Referenced by b_pushb1_get_value(), b_pushb2_get_value(), and b_pushb3_get_value().
|
static |
Pushbutton events emulation.
Referenced by b_pushb1_get_value().
|
static |
Referenced by b_pushb2_get_value().
|
static |
Referenced by b_pushb3_get_value().