Microchip® Advanced Software Framework

s_temperature.c File Reference
#include <string.h>
#include <stdio.h>
#include "compiler.h"
#include "s_temperature.h"
#include "board.h"
#include "gpio.h"
#include "adc.h"

Functions

bool b_temperature_get_value (char *buf)
 Get the current temperature value. More...
 

Variables

static volatile avr32_adc_t * adc = (volatile avr32_adc_t *) &AVR32_ADC
 
const unsigned short temperature_code []
 The following table give the correspondence between the ADC code and the temperature Each elements of the table corresponds to an ADC code value. More...
 

bool b_temperature_get_value ( char *  buf)

Get the current temperature value.

Parameters
bufchar buffer in which the temperature value is stored.
Returns
true upon success, false if error.

References adc, adc_disable(), adc_enable(), adc_get_value(), adc_start(), index, sprintf(), and temperature_code.

Referenced by device_full_custom_task().

volatile avr32_adc_t* adc = (volatile avr32_adc_t *) &AVR32_ADC
static

ADC cell.

Referenced by b_light_get_value(), and b_temperature_get_value().

const unsigned short temperature_code[]
Initial value:
={
0x3B4,0x3B0,0x3AB,0x3A6,0x3A0,0x39A,0x394,0x38E,0x388,0x381,0x37A,0x373,
0x36B,0x363,0x35B,0x353,0x34A,0x341,0x338,0x32F,0x325,0x31B,0x311,0x307,
0x2FC,0x2F1,0x2E6,0x2DB,0x2D0,0x2C4,0x2B8,0x2AC,0x2A0,0x294,0x288,0x27C,
0x26F,0x263,0x256,0x24A,0x23D,0x231,0x225,0x218,0x20C,0x200,0x1F3,0x1E7,
0x1DB,0x1CF,0x1C4,0x1B8,0x1AC,0x1A1,0x196,0x18B,0x180,0x176,0x16B,0x161,
0x157,0x14D,0x144,0x13A,0x131,0x128,0x11F,0x117,0x10F,0x106,0xFE,0xF7,
0xEF,0xE8,0xE1,0xDA,0xD3,0xCD,0xC7,0xC0,0xBA,0xB5,0xAF,0xAA,0xA4,0x9F,
0x9A,0x96,0x91,0x8C,0x88,0x84,0x80,0x7C,0x78,0x74,0x71,0x6D,0x6A,0x67,
0x64,0x61,0x5E,0x5B,0x58,0x55,0x53,0x50,0x4E,0x4C,0x49,0x47,0x45,0x43,
0x41,0x3F,0x3D,0x3C,0x3A,0x38}

The following table give the correspondence between the ADC code and the temperature Each elements of the table corresponds to an ADC code value.

The index in the table give the corresponding temperature (inC) with the following formula : Tempeature=index-20. table[O] corresponds to -20C temperature code The following table gives the ADC code for VCC=3.3V and Aref=AVcc

Referenced by b_temperature_get_value().