Microchip® Advanced Software Framework

 All Data Structures Namespaces Files Functions Variables Typedefs Enumerations Enumerator Friends Macros Groups Pages

In this section you can find all the projects related to the Peripheral Event Controller (PEVC) Driver.

Example(s)

PEVC Example 1 for uc3c_ek

PEVC example using the "AST - period event 0" as an event source and the "PDCA - start of transfer channel 0" as a triggered event that sends a character to a USART output.

PEVC Example 2 for uc3c_ek

PEVC example using "the generic clock GCLK7" as an event source and the "PDCA - start of transfer channel 0" as a triggered event that sends a character to a USART output.

PEVC Example 3 for uc3c_ek

PEVC example using the "PAD_EVT[15:0] - change on input pins" as an event source and the "PDCA - start of transfer channel 0" as a triggered event that sends a character to a USART output.