#include "sau.h"
Functions | |
bool | sau_configure_channels (const sau_map_t sau_map, uint32_t size) |
Configs specific HSB memories for a set of channels. More... | |
void | sau_disable_channel (unsigned char channel_num) |
void | sau_enable_channel (unsigned char channel_num) |
void | sau_lock_channels (U8 unlock_HSB_cycles, U8 unlock_key) |
Lock SAU channels. More... | |
uint32_t | sau_read_channel (unsigned char channel_num) |
Read the HSB memory value by the SAU channel. More... | |
bool | sau_unlock_channel (U8 unlock_channel_number, U8 unlock_key) |
Unlock an SAU channel. More... | |
void | sau_write_channel (uint32_t data, unsigned char channel_num) |
Write the HSB memory value by the SAU channel. More... | |