Microchip® Advanced Software Framework

Todo List
Group External oscillator
Need to measure the actual startup time on the hardware.
Group External oscillator
Need to measure the actual startup time on the hardware.
Global font_data_type
Add support for fonts in regular ram
Global pll_wait_for_lock (unsigned int pll_id)
Use a timeout to avoid waiting forever and hanging the system
Global RTC32
Remove when header files are fixed if WinAVR release
Global RTC32_t2
Remove when header files are fixed if WinAVR release
Global RTC32_t2
Remove when header files are fixed if WinAVR release
Global sysclk_get_main_hz (void)
This function assumes that the main clock source never changes once it's been set up, and that PLL0 always runs at the compile-time configured default rate. While this is probably the most common configuration, which we want to support as a special case for performance reasons, we will at some point need to support more dynamic setups as well.
Global VBAT_STATUS_XOSCFAIL
Determine minimum period for detection of oscillator outage.