![]() | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
![]() | Compiler abstraction layer and code utilities for 8-bit AVR |
![]() ![]() | This group provides a good handful of macros intended to smooth out the differences between various assemblers, similar to what compiler.h does for compilers, except that assemblers tend to be much less standardized than compilers |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | This is a driver for global enabling and disabling of interrupts |
![]() ![]() | |
![]() | This collection of macros identify which series and families that the various Atmel parts belong to |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | |
![]() ![]() | Generic clocks are configurable clocks which run outside the system clock domain |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs |
![]() ![]() | See Quick Start Guide for the System Clock Management service (XMEGA) |
![]() | See Quick start guide for CCP driver |
![]() | See reset_cause_quickstart |
![]() | See Quick Start Guide for the XMEGA NVM Driver |
![]() ![]() | Support functions for the NVM driver |
![]() ![]() | Handling of signature rows |
![]() ![]() | Functions for handling internal EEPROM memory |
![]() ![]() | Functions for handling internal flash memory |
![]() ![]() | Functions for reading fuses and writing lock bits |
![]() | This is the common API for GPIO |
![]() | See Quick start guide for the common IOPORT service |
![]() | See Quick Start Guide for the mono graphics service |
![]() ![]() | This module is an abstraction layer between the graphic library and the C12832_A1Z monochrome LCD display connected to a ST7565R LCD controller |
![]() ![]() | This is a service providing generic implementations of graphic primitives |
![]() ![]() | This module provides read/write from and to a framebuffer in RAM |
![]() ![]() | This modules provides functionality for outputting a monochrome font to a display |
![]() ![]() ![]() | The system font objects are globally available for a graphical application |
![]() ![]() | This module provides a simple menu system for monochrome graphical displays |
![]() ![]() | This module provides a spinner widget system for monochrome graphical displays |
![]() | This is a low level driver for the ST7565R LCD controller |
![]() | This module provides simple loop-based delay routines for those applications requiring a brief wait during execution |
![]() | This is the common API for USART in SPI mode |
![]() | See Quick start guide for USART module |
![]() | See Quick start guide for PMIC driver |
![]() | Self-diagnostic test for the ADC, DAC and analog multiplexer |
![]() | This is a basic driver for the Real Time Counter (RTC) |
![]() | This CRC module can be used to check the Flash and EEPROM memories |
![]() ![]() | Symbols that can be defined to configure the CRC computation |
![]() ![]() | Symbols for ensuring standard compliant CRC |
![]() ![]() | Data types used in connection with CRC computations |
![]() ![]() | Low-level driver implementation for the AVR XMEGA AU CRC module |
![]() ![]() | CRC computations implemented in software |
![]() | Definitions related to error handling for Class B tests |
![]() | Self-diagnostic test for the CPU frequency |
![]() ![]() | This should be configured by the user |
![]() ![]() | These constants should not be modified by user |
![]() ![]() | Setup and test functions |
![]() | A test for the frequency of interrupts |
![]() ![]() | Settings for the interrupt monitor |
![]() ![]() | Definition of data structures used by the monitor |
![]() ![]() | Functions related to the interrupt monitor |
![]() | This is the self-test module for the registers in the CPU |
![]() ![]() | Symbols to define behavior upon detected register faults |
![]() ![]() | Internal symbols that indicate presence of RAMPx and EIND registers |
![]() ![]() | In order to simplify the code, the assembly code is interfaced through macros |
![]() ![]() | This is the self-test for CPU registers |
![]() | Self-diagnostic test for coupling faults in internal SRAM memory |
![]() | Test to check that the watchdog timer (WDT) is working |
![]() | See Quick start guide for XMEGA ADC |
![]() ![]() | Management and configuration functions for the ADC module |
![]() ![]() | Management and configuration functions for the individual ADC channels |
![]() | The sleep manager is a service for ensuring that the device is not put to sleep in deeper sleep modes than the system (e.g., peripheral drivers, services or the application) allows at any given time |
![]() | This is a low-level driver implementation for the AVR XMEGA sleep controller |
![]() | See Quick start guide for XMEGA DAC |
![]() | See Quick start guide for RTC32 driver |
![]() | See Quick Start Guide for the XMEGA TC Driver |
![]() ![]() | This group provides functions to configure TC module interrupts |
![]() ![]() | This group provides low level drivers to configure AWeX extension |
![]() ![]() | This group provides low level drivers to configure Hi-Res extension |
![]() | See Quick start guide for WDT driver |
![]() | This is the QTouch Library for AVR and AVR32 devices that consists of one api header file(touch_api.h) and respective pre-compiled libraries |
![]() | |
![]() ![]() | |
![]() ![]() | |
![]() |