Display time since production date.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "stdio.h"
#include "keyboard.h"
#include "nvm.h"
#include "rtc32.h"
#include "calendar.h"
#include "sysfont.h"
#include "production_date.h"
#include "conf_application.h"
Functions | |
void | production_date_application (void) |
Production date application. More... | |
uint32_t | production_date_get_timestamp (void) |
Production date get timestamp. More... | |
void production_date_application | ( | void | ) |
Production date application.
This application will display the time since the XMEGA-A3BU Xplained board has been produced. During production the production time is stored in EEPROM and the RTC is initialized to the same time. The RTC is then left running from the battery backup. This application reads out the production date from EEPROM and shows the difference between the current time and the production date; in other words the time the RTC timer has been running on battery since production.
References calendar_time_between_dates(), calendar_timestamp_to_date(), calendar_date::date, gfx_mono_draw_filled_rect, gfx_mono_draw_string(), gfx_mono_get_string_bounding_box(), GFX_MONO_LCD_WIDTH, GFX_PIXEL_CLR, calendar_date::hour, KEYBOARD_BACK, keyboard_get_key_state(), KEYBOARD_RELEASE, keyboard_event::keycode, calendar_date::minute, calendar_date::month, production_date_get_timestamp(), rtc_get_time(), calendar_date::second, sysfont, keyboard_event::type, and calendar_date::year.
Referenced by main().
uint32_t production_date_get_timestamp | ( | void | ) |
Production date get timestamp.
This function reads the production date time stamp stored in the user signature row addresses PRODUCTION_DATE_ADDRESS to PRODUCTION_DATE_ADDRESS + 3 (4 bytes) and returns a 32 bit value in the UNIX time format.
References FIRST_POSSIBLE_TIMESTAMP, nvm_read_user_signature_row(), and PRODUCTION_DATE_ADDRESS.
Referenced by main(), and production_date_application().