Chip-specific example configuration.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | OUTPUT_STR_SIZE 32 |
Example configuration | |
#define | INPUT_PIN ADCCH_POS_PIN0 |
ID of ADC input pin. More... | |
#define | LED1_PIN LED0_GPIO |
ID of LED 1 control I/O pin. More... | |
#define | LED2_PIN LED1_GPIO |
ID of LED 2 control I/O pin. More... | |
#define | BUTTON_PIN GPIO_PUSH_BUTTON_0 |
ID of button input I/O pin. More... | |
#define | OVERSAMPLING_FACTOR 6 |
Number of calibration samples, as exponent of 2. More... | |
#define BUTTON_PIN GPIO_PUSH_BUTTON_0 |
ID of button input I/O pin.
This pin is checked for active low status when the example is waiting for user input, i.e., after the external voltage supply has been adjusted.
Referenced by wait_for_button().
#define INPUT_PIN ADCCH_POS_PIN0 |
ID of ADC input pin.
This pin is the one used for all measurements with the ADC.
Referenced by main().
#define LED1_PIN LED0_GPIO |
ID of LED 1 control I/O pin.
This pin is driven low when the example is waiting for the external voltage supply to be adjusted to 0 Volts. It is driven high once calibration is done.
Referenced by main().
#define LED2_PIN LED1_GPIO |
ID of LED 2 control I/O pin.
This pin is driven low when the example is waiting for the external voltage supply to be adjusted to 0.9 Volts. It is driven high once calibration is done.
Referenced by main().
#define OUTPUT_STR_SIZE 32 |
Referenced by ISR().
#define OVERSAMPLING_FACTOR 6 |
Number of calibration samples, as exponent of 2.
This determines the number of samples used for the oversampling. It is given as an exponent of 2, i.e., setting this factor to 3 gives 2^3 = 8 samples.
Referenced by get_mean_sample_value().