See Quick start guide for XMEGA DES driver.
This is a driver for the AVR XMEGA DES core instruction. It provides functions for des, 3des and CBC des encryption and decryption operations.
DES is supported by a DES instruction in the AVR XMEGA core. The 8-byte key and 8-byte data blocks must be loaded into the Register file, and then DES must be executed 16 times to encrypt/decrypt the data block.
See Quick start guide for XMEGA DES driver
Functions | |
void | des_3des_decrypt (uint8_t *ciphertext, uint8_t *plaintext, uint8_t *keys) |
Function that does a 3DES decryption on one 64-bit data block. More... | |
void | des_3des_encrypt (uint8_t *plaintext, uint8_t *ciphertext, uint8_t *keys) |
Function that does a 3DES encryption on one 64-bit data block. More... | |
void | des_cbc_decrypt (uint8_t *ciphertext, uint8_t *plaintext, uint8_t *keys, uint8_t *init, bool triple_DES, uint16_t block_length) |
Function that does DES Cipher Block Chaining decryption on a given number of 64-bit data block. More... | |
void | des_cbc_encrypt (uint8_t *plaintext, uint8_t *ciphertext, uint8_t *keys, uint8_t *init, bool triple_DES, uint16_t block_length) |
Function that does DES Cipher Block Chaining encryption on a given number of 64-bit data block. More... | |
void | des_decrypt (uint8_t *ciphertext, uint8_t *plaintext, uint8_t *key) |
Function that does a DES decryption on one 64-bit data block. More... | |
void | des_encrypt (uint8_t *plaintext, uint8_t *ciphertext, uint8_t *key) |
Function that does a DES encryption on one 64-bit data block. More... | |
void des_3des_decrypt | ( | uint8_t * | ciphertext, |
uint8_t * | plaintext, | ||
uint8_t * | keys | ||
) |
Function that does a 3DES decryption on one 64-bit data block.
ciphertext | Pointer to the ciphertext that shall be decrypted. |
plaintext | Pointer to where in memory the plaintext (answer) shall be stored. |
keys | Pointer to the array of the 3 DES keys. |
Referenced by run_3des_decryption(), and run_3des_encryption_and_decryption_test().
void des_3des_encrypt | ( | uint8_t * | plaintext, |
uint8_t * | ciphertext, | ||
uint8_t * | keys | ||
) |
Function that does a 3DES encryption on one 64-bit data block.
plaintext | Pointer to the plaintext that shall be encrypted. |
ciphertext | Pointer to where in memory the ciphertext (answer) shall be stored. |
keys | Pointer to the array of the 3 DES keys. |
Referenced by run_3des_encryption(), and run_3des_encryption_and_decryption_test().
void des_cbc_decrypt | ( | uint8_t * | ciphertext, |
uint8_t * | plaintext, | ||
uint8_t * | keys, | ||
uint8_t * | init, | ||
bool | triple_DES, | ||
uint16_t | block_length | ||
) |
Function that does DES Cipher Block Chaining decryption on a given number of 64-bit data block.
ciphertext | Pointer to the ciphertext that shall be decrypted. |
plaintext | Pointer to where in memory the plaintext (answer) shall be stored. |
keys | Pointer to the array of the one or three DES keys needed. |
init | Pointer to initial vector used in in CBC. |
triple_DES | Bool that indicate if 3DES or DES shall be used. |
block_length | Value that tells how many blocks to encrypt. |
Referenced by run_3des_cbc_decryption_test(), and run_des_cbc_decryption_test().
void des_cbc_encrypt | ( | uint8_t * | plaintext, |
uint8_t * | ciphertext, | ||
uint8_t * | keys, | ||
uint8_t * | init, | ||
bool | triple_DES, | ||
uint16_t | block_length | ||
) |
Function that does DES Cipher Block Chaining encryption on a given number of 64-bit data block.
plaintext | Pointer to the plaintext that shall be encrypted. |
ciphertext | Pointer to where in memory the ciphertext(answer) shall be stored. |
keys | Pointer to the array of the one or three DES keys needed. |
init | Pointer to initial vector used in in CBC. |
triple_DES | Bool that indicate if 3DES or DES shall be used. |
block_length | Value that tells how many blocks to encrypt. |
Referenced by run_3des_cbc_encryption_test(), and run_des_cbc_encryption_test().
void des_decrypt | ( | uint8_t * | ciphertext, |
uint8_t * | plaintext, | ||
uint8_t * | key | ||
) |
Function that does a DES decryption on one 64-bit data block.
ciphertext | Pointer to the ciphertext that shall be decrypted. |
plaintext | Pointer to where in memory the plaintext (answer) shall be stored. |
key | Pointer to the DES key. |
Referenced by run_des_decryption(), and run_des_encryption_and_decryption_test().
void des_encrypt | ( | uint8_t * | plaintext, |
uint8_t * | ciphertext, | ||
uint8_t * | key | ||
) |
Function that does a DES encryption on one 64-bit data block.
plaintext | Pointer to the plaintext that shall be encrypted. |
ciphertext | Pointer to where in memory the ciphertext (answer) shall be stored. |
key | Pointer to the DES key. |
Referenced by run_des_encryption(), and run_des_encryption_and_decryption_test().