This is the unit test application for the External Bus Interface (EBI) and EBI port/pin configuration. In essence, it tests that the EBI has been correctly set up by employing test cases for:
All AVR XMEGA A1 devices can be used. This example has been tested with the following setup:
See the documentation for the individual test functions here for detailed descriptions of the tests.
Relevant module dependencies for this application are:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.