This example shows how to use the NVM signature handling of the NVM driver.
All AVR XMEGA devices can be used. This example have been tested with the following setup:
The example uses the NVM signature driver to read the device signature and the production signature and outputs the status on the Xplain LEDs:
If either LED0 or LED1 does not light up, this indicates a failure on these tests.
This example depends on the following modules:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.