This example shows how to use and tests the user signature access of the NVM flash handling of the NVM driver.
All AVR XMEGA devices can be used. This example have been tested with the following setup:
The example tests the user signature row functions and reports back the status on the Xplain LEDs:
If one of the LEDs does not light up, this indicates a failure on the test.
This example depends on the following modules:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.