This is the unit test application for the Watchdog Timer (WDT).
All AVR XMEGA devices can be used. This example has been tested with the following setup:
The application will set up a watchdog timeout, and the test will fail if the watchdog reset doesn't occur.
This example depends directly on the following modules:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.