#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
#include <stdlib.h>
#include "pal.h"
#include "return_val.h"
#include "tal.h"
#include "ieee_const.h"
#include "tal_pib.h"
#include "tal_irq_handler.h"
#include "at86rf231.h"
#include "stack_config.h"
#include "bmm.h"
#include "qmm.h"
#include "tal_rx.h"
#include "tal_tx.h"
#include "tal_constants.h"
#include "tal_internal.h"
#include "tal_slotted_csma.h"
#include "mac_build_config.h"
Macros | |
#define | PLL_LOCK_ATTEMPTS (3) |
Functions | |
tal_trx_status_t | set_trx_state (trx_cmd_t trx_cmd) |
Sets transceiver state. More... | |
static void | switch_pll_on (void) |
Switches the PLL on. More... | |
uint32_t | tal_convert_symbols_to_us_def (uint32_t symbols) |
Conversion of symbols to microseconds. More... | |
uint32_t | tal_convert_us_to_symbols_def (uint32_t time) |
Conversion of microseconds to symbols. More... | |
void | tal_task (void) |
TAL task handling. More... | |
Variables | |
uint8_t | last_frame_length |
frame_info_t * | mac_frame_ptr |
Frame pointer for the frame structure provided by the MCL. More... | |
volatile bool | tal_awake_end_flag |
csma_state_t | tal_csma_state |
CSMA state machine variable. More... | |
uint8_t * | tal_frame_to_tx |
Pointer to the 15.4 frame created by the TAL to be handed over to the transceiver. More... | |
queue_t | tal_incoming_frame_queue |
Queue that contains all frames that are uploaded from the trx, but have not be processed by the MCL yet. More... | |
tal_pib_t | tal_pib |
buffer_t * | tal_rx_buffer = NULL |
Pointer to receive buffer that can be used to upload a frame from the trx. More... | |
bool | tal_rx_on_required |
Indicates if the transceiver needs to switch on its receiver by tal_task(), because it could not be switched on due to buffer shortage. More... | |
uint32_t | tal_rx_timestamp |
Timestamp The timestamping is only required for beaconing networks or if timestamping is explicitly enabled. More... | |
tal_state_t | tal_state |
Current state of the TAL state machine. More... | |
tal_trx_status_t | tal_trx_status |
Current state of the transceiver. More... | |
#define PLL_LOCK_ATTEMPTS (3) |
Referenced by switch_pll_on().
uint32_t tal_convert_symbols_to_us_def | ( | uint32_t | symbols | ) |
Conversion of symbols to microseconds.
References TAL_CONVERT_SYMBOLS_TO_US.
uint32_t tal_convert_us_to_symbols_def | ( | uint32_t | time | ) |
Conversion of microseconds to symbols.
References TAL_CONVERT_US_TO_SYMBOLS.
void tal_task | ( | void | ) |
TAL task handling.
This function
Referenced by main(), performance_analyzer_task(), and wpan_task().
uint8_t last_frame_length |
Referenced by process_incoming_frame(), send_frame(), and tal_tx_frame().
frame_info_t* mac_frame_ptr |
Frame pointer for the frame structure provided by the MCL.
Referenced by calculate_transaction_duration(), handle_tx_end_irq(), tal_tx_frame(), tx_done(), and tx_done_handling().
volatile bool tal_awake_end_flag |
Referenced by set_trx_state(), and trx_irq_awake_handler_cb().
csma_state_t tal_csma_state |
CSMA state machine variable.
Referenced by beacon_loss_timer_cb(), cca_timer_handler_cb(), csma_backoff_calculation(), handle_tx_end_irq(), internal_tal_reset(), process_incoming_frame(), send_frame_at_next_backoff_boundary(), slotted_csma_state_handling(), and tx_done().
uint8_t* tal_frame_to_tx |
Pointer to the 15.4 frame created by the TAL to be handed over to the transceiver.
Referenced by calculate_transaction_duration(), send_frame(), tal_tx_frame(), and tx_done_handling().
queue_t tal_incoming_frame_queue |
Queue that contains all frames that are uploaded from the trx, but have not be processed by the MCL yet.
Referenced by handle_received_frame_irq(), mac_ready_to_sleep(), tal_init(), tal_reset(), and tal_task().
tal_pib_t tal_pib |
Referenced by apply_channel_page_configuration(), build_data_frame(), check_beacon_reception(), configure_frame_sending(), configure_pibs(), configure_pkt_stream_frames(), configure_range_test_frame_sending(), csma_backoff_calculation(), csma_param_init(), get_board_details(), get_node_info(), handle_gts_data_req(), handle_gts_sync_loss(), handle_received_frame_irq(), init_tal_pib(), limit_tx_pwr(), mac_coord_realignment_command_tx_success(), mac_gts_allocate(), mac_parse_bcn_gts_info(), mac_process_tal_data_ind(), mac_sleep_trans(), mac_t_gts_cb(), main(), mcps_data_request(), mlme_get(), mlme_gts_request(), mlme_start_request(), parse_mpdu(), process_data_ind_not_transient(), process_incoming_frame(), recalc_macMaxFrameTotalWaitTime(), reset_gts_expiry(), send_frame(), send_peer_conf(), set_default_tx_pwr(), slotted_csma_start(), slotted_csma_state_handling(), start_beacon_loss_timer(), start_ed_scan(), tal_get_rssi_base_val(), tal_init(), tal_pib_get(), tal_pib_set(), tal_rx_enable(), tal_task(), tal_tx_frame(), tfa_continuous_tx_start(), tfa_pib_set(), transmit_frame(), tx_done_handling(), validate_tx_power(), and write_all_tal_pib_to_trx().
buffer_t* tal_rx_buffer = NULL |
Pointer to receive buffer that can be used to upload a frame from the trx.
Referenced by handle_received_frame_irq(), handle_tx_end_irq(), tal_init(), tal_pib_set(), tal_rx_enable(), and tal_task().
uint32_t tal_rx_timestamp |
Timestamp The timestamping is only required for beaconing networks or if timestamping is explicitly enabled.
Referenced by handle_received_frame_irq(), and trx_irq_handler_cb().