Microchip® Advanced Software Framework

Use case #2

In this use case, the CRC module is configured for:

  • Performing CRC on data passing through a DMA channel
  • Using CRC-16

This use case shows how to calculate the checksum for data passing through a DMA channel.

Setup steps

Prerequisites

For the setup code of this use case to work, the following must be added to the project:

  1. PMIC driver for interrupt handling
  2. DMA driver for enabling DMA transaction
  3. The common Clock service.
  4. A callback function for DMA transfer complete must be provided by the user:
    static void callback_dma_transfer_done(enum dma_channel_status status)
    {
    uint32_t checksum;
    checksum = crc_dma_checksum_stop();
    }
  5. A static uint8_t array of data with at least DMA_BUFFER_SIZE entries to perform CRC on.

Example code

Some defines and data buffers must be set up:

#define DMA_CHANNEL 0
#define DMA_BUFFER_SIZE 8
static uint8_t source[DMA_BUFFER_SIZE];
static uint8_t destination[DMA_BUFFER_SIZE];

Add to application initialization:

Workflow

  1. Initialize system clock:

Usage steps

Example code

Workflow

  1. Enable the CRC module for DMA
  2. Enable DMA
  3. Set callback function for DMA completion
  4. Make sure config is all zeroed out so we don't get any stray bits
  5. Configure the DMA channel with the following settings:
  6. Use the configuration above by enabling the DMA channel in use.
  7. Enable interrupts
  8. Trigger the DMA transfer
  9. Do nothing while waiting for DMA transfer to complete
    • while (true) {
      }