This is a driver for global enabling and disabling of interrupts.
Modules | |
Related Project(s) | |
In this section you can find all the projects related to the Global interrupt management. | |
Deprecated interrupt definitions | |
Macros | |
#define | CONFIG_INTERRUPT_FORCE_INTC |
Force usage of the ASF INTC driver. More... | |
#define | ISR(vect) |
Define service routine for specified interrupt vector. More... | |
Global interrupt flags | |
typedef uint8_t | irqflags_t |
Type used for holding state of interrupt flag. More... | |
static irqflags_t | cpu_irq_save (void) |
Get and clear the global interrupt flags. More... | |
static void | cpu_irq_restore (irqflags_t flags) |
Restore global interrupt flags. More... | |
static bool | cpu_irq_is_enabled_flags (irqflags_t flags) |
Check if interrupts are globally enabled in supplied flags. More... | |
#define | cpu_irq_enable() sei() |
Enable interrupts globally. More... | |
#define | cpu_irq_disable() cli() |
Disable interrupts globally. More... | |
#define | cpu_irq_is_enabled() cpu_irq_is_enabled_flags(SREG) |
Check if interrupts are globally enabled. More... | |
#define CONFIG_INTERRUPT_FORCE_INTC |
Force usage of the ASF INTC driver.
Predefine this symbol when preprocessing to force the use of the ASF INTC driver. This is useful to ensure compatibility across compilers and shall be used only when required by the application needs.
#define cpu_irq_disable | ( | ) | cli() |
Disable interrupts globally.
Referenced by cpu_irq_save(), isp_start_appli(), ISR(), sensor_board_init(), sleepmgr_enter_sleep(), and usb_rx_notify().
#define cpu_irq_enable | ( | ) | sei() |
Enable interrupts globally.
Referenced by ISR(), main(), run_twi_master_recv_test(), run_twi_master_send_test(), run_twi_slave_recv_test(), sensor_board_init(), sleepmgr_enter_sleep(), sleepmgr_sleep(), twi_master_init(), and usb_rx_notify().
#define cpu_irq_is_enabled | ( | ) | cpu_irq_is_enabled_flags(SREG) |
Check if interrupts are globally enabled.
#define ISR | ( | vect | ) |
Define service routine for specified interrupt vector.
Usage:
vect | Interrupt vector name as found in the device header files. |
Type used for holding state of interrupt flag.
|
inlinestatic |
Check if interrupts are globally enabled in supplied flags.
flags | Currents state of interrupt flags. |
|
inlinestatic |
Restore global interrupt flags.
Use in conjunction with cpu_irq_save.
flags | State to set interrupt flag to. |
References barrier.
Referenced by ac_disable(), ac_enable(), ac_read_config(), ac_write_config(), adc_disable(), adc_enable(), adc_flush(), adc_get_signed_compare_value(), adc_get_signed_result(), adc_get_unsigned_compare_value(), adc_get_unsigned_result(), adc_read_configuration(), adc_set_callback(), adc_start_conversion(), adc_write_configuration(), adcch_read_configuration(), adcch_write_configuration(), arch_ioport_disable_pin(), arch_ioport_disable_port(), arch_ioport_enable_pin(), arch_ioport_enable_port(), arch_ioport_set_pin_mode(), arch_ioport_set_pin_sense_mode(), arch_ioport_set_port_mode(), arch_ioport_set_port_sense_mode(), dac_disable(), dac_enable(), dac_get_channel_value(), dac_read_configuration(), dac_set_channel_value(), dac_write_configuration(), dma_channel_disable(), dma_channel_enable(), dma_channel_read_config(), dma_channel_reset(), dma_channel_trigger_block_transfer(), dma_channel_write_burst_length(), dma_channel_write_config(), dma_channel_write_destination(), dma_channel_write_repeats(), dma_channel_write_source(), dma_channel_write_transfer_count(), dma_set_double_buffer_mode(), dma_set_priority_mode(), ebi_cs_read_config(), ebi_cs_write_config(), ebi_disable_cs(), ebi_enable_cs(), ebi_sdram_disable_self_refresh(), ebi_sdram_enable_self_refresh(), ebi_sdram_read_config(), ebi_sdram_write_config(), ili9341_send_byte(), lightsensor_data_is_ready(), ntc_data_is_ready(), osc_disable(), osc_enable_autocalibration(), osc_enable_external(), osc_enable_internal(), pll_disable(), pll_enable(), restore_cpu_interrupt(), rtc_get_time(), sleepmgr_lock_mode(), sleepmgr_unlock_mode(), sw_timer_service(), SYS_TimerTaskHandler(), sysclk_disable_module(), sysclk_enable_module(), tc_disable(), tc_enable(), timeout_start_offset(), timeout_stop(), timeout_test_and_clear_expired(), twim_acquire(), udd_attach(), udd_disable(), udd_enable(), udi_cdc_ctrl_state_change(), udi_cdc_multi_get_free_tx_buffer(), udi_cdc_multi_get_nb_received_data(), udi_cdc_multi_getc(), udi_cdc_multi_putc(), udi_cdc_multi_read_buf(), udi_cdc_multi_read_no_polling(), udi_cdc_multi_write_buf(), udi_cdc_rx_start(), udi_cdc_tx_send(), udi_hid_generic_send_report_in(), udi_hid_gpd_buttons(), udi_hid_gpd_moveX(), udi_hid_gpd_moveY(), udi_hid_gpd_throttle_move(), udi_hid_kbd_down(), udi_hid_kbd_modifier_down(), udi_hid_kbd_modifier_up(), udi_hid_kbd_up(), udi_hid_mkbd_modifier_down(), udi_hid_mkbd_modifier_up(), udi_hid_mouse_move(), udi_phdc_senddata(), udi_phdc_waitdata(), win_are_events_pending(), win_pop_front_event(), and win_queue_event().
|
inlinestatic |
Get and clear the global interrupt flags.
Use in conjunction with cpu_irq_restore.
References cpu_irq_disable.
Referenced by ac_disable(), ac_enable(), ac_read_config(), ac_write_config(), adc_disable(), adc_enable(), adc_flush(), adc_get_signed_compare_value(), adc_get_signed_result(), adc_get_unsigned_compare_value(), adc_get_unsigned_result(), adc_read_configuration(), adc_set_callback(), adc_start_conversion(), adc_write_configuration(), adcch_read_configuration(), adcch_write_configuration(), arch_ioport_disable_pin(), arch_ioport_disable_port(), arch_ioport_enable_pin(), arch_ioport_enable_port(), arch_ioport_set_pin_mode(), arch_ioport_set_pin_sense_mode(), arch_ioport_set_port_mode(), arch_ioport_set_port_sense_mode(), dac_disable(), dac_enable(), dac_get_channel_value(), dac_read_configuration(), dac_set_channel_value(), dac_write_configuration(), dma_channel_disable(), dma_channel_enable(), dma_channel_read_config(), dma_channel_reset(), dma_channel_trigger_block_transfer(), dma_channel_write_burst_length(), dma_channel_write_config(), dma_channel_write_destination(), dma_channel_write_repeats(), dma_channel_write_source(), dma_channel_write_transfer_count(), dma_set_double_buffer_mode(), dma_set_priority_mode(), ebi_cs_read_config(), ebi_cs_write_config(), ebi_disable_cs(), ebi_enable_cs(), ebi_sdram_disable_self_refresh(), ebi_sdram_enable_self_refresh(), ebi_sdram_read_config(), ebi_sdram_write_config(), ili9341_send_byte(), lightsensor_data_is_ready(), ntc_data_is_ready(), osc_disable(), osc_enable_autocalibration(), osc_enable_external(), osc_enable_internal(), pll_disable(), pll_enable(), rtc_get_time(), save_cpu_interrupt(), sleepmgr_lock_mode(), sleepmgr_unlock_mode(), sw_timer_service(), SYS_TimerTaskHandler(), sysclk_disable_module(), sysclk_enable_module(), tc_disable(), tc_enable(), timeout_start_offset(), timeout_stop(), timeout_test_and_clear_expired(), twim_acquire(), udd_attach(), udd_disable(), udd_enable(), udi_cdc_ctrl_state_change(), udi_cdc_multi_get_free_tx_buffer(), udi_cdc_multi_get_nb_received_data(), udi_cdc_multi_getc(), udi_cdc_multi_putc(), udi_cdc_multi_read_buf(), udi_cdc_multi_read_no_polling(), udi_cdc_multi_write_buf(), udi_cdc_rx_start(), udi_cdc_tx_send(), udi_hid_generic_send_report_in(), udi_hid_gpd_buttons(), udi_hid_gpd_moveX(), udi_hid_gpd_moveY(), udi_hid_gpd_throttle_move(), udi_hid_kbd_down(), udi_hid_kbd_modifier_down(), udi_hid_kbd_modifier_up(), udi_hid_kbd_up(), udi_hid_mkbd_modifier_down(), udi_hid_mkbd_modifier_up(), udi_hid_mouse_move(), udi_phdc_senddata(), udi_phdc_waitdata(), win_are_events_pending(), win_pop_front_event(), and win_queue_event().