#include "touch_api.h"
#include <avr/io.h>
Macros | |
#define | EEPROM_LIB_CONFIG_START_ADDRESS (EEPROM_START_ADDRESS + 2u) |
#define | EEPROM_START_ADDRESS 0x0000u /* User Eeprom address */ |
Functions | |
uint16_t | read_info_from_eeprom (void) |
read_info_from_eeprom is used to Read Info block from EEPROM More... | |
void | read_settings_from_eeprom (void) |
read_settings_from_eeprom is used to Will read settings from EEPROM More... | |
void | write_global_settings_to_eeprom (void) |
write_global_settings_to_eeprom is used to Save global parameter settings to EEPROM More... | |
void | write_info_to_eeprom (uint16_t lib_version) |
write_info_to_eeprom is used to Save information from library and sign in the EEPROM More... | |
void | write_sensor_settings_to_eeprom (void) |
write_sensor_settings_to_eeprom is used to Save sensor parameter settings to EEPROM More... | |
#define EEPROM_LIB_CONFIG_START_ADDRESS (EEPROM_START_ADDRESS + 2u) |
#define EEPROM_START_ADDRESS 0x0000u /* User Eeprom address */ |
Referenced by read_info_from_eeprom(), and write_info_to_eeprom().
uint16_t read_info_from_eeprom | ( | void | ) |
read_info_from_eeprom is used to Read Info block from EEPROM
read_info_from_eeprom is used to Read Info block from EEPROM
This function is used to read Info block from EEPROM
\note | Returns library version currently on chip |
References EEPROM_START_ADDRESS, and nvm_eeprom_read_byte().
Referenced by QDebug_Init().
void read_settings_from_eeprom | ( | void | ) |
read_settings_from_eeprom is used to Will read settings from EEPROM
read_settings_from_eeprom is used to Will read settings from EEPROM
This function is used to read settings from EEPROM
\note | Data is stored in 'eeprom_gv_block[]' in the format shown above |
References EEPROM_LIB_CONFIG_START_ADDRESS, num_sensors, nvm_eeprom_read_byte(), qt_config_data, tag_qt_touch_lib_config_data_t::qt_di, tag_qt_touch_lib_config_data_t::qt_drift_hold_time, tag_qt_touch_lib_config_data_t::qt_max_on_duration, tag_qt_touch_lib_config_data_t::qt_neg_drift_rate, tag_qt_touch_lib_config_data_t::qt_pos_drift_rate, tag_qt_touch_lib_config_data_t::qt_pos_recal_delay, tag_qt_touch_lib_config_data_t::qt_recal_threshold, tag_sensor_t::threshold, and tag_sensor_t::type_aks_pos_hyst.
Referenced by QDebug_Init().
void write_global_settings_to_eeprom | ( | void | ) |
write_global_settings_to_eeprom is used to Save global parameter settings to EEPROM
write_global_settings_to_eeprom is used to Save global parameter settings to EEPROM
This function is used to Save global parameter settings to EEPROM
\note |
References EEPROM_LIB_CONFIG_START_ADDRESS, nvm_eeprom_write_byte(), qt_config_data, tag_qt_touch_lib_config_data_t::qt_di, tag_qt_touch_lib_config_data_t::qt_drift_hold_time, tag_qt_touch_lib_config_data_t::qt_max_on_duration, tag_qt_touch_lib_config_data_t::qt_neg_drift_rate, tag_qt_touch_lib_config_data_t::qt_pos_drift_rate, tag_qt_touch_lib_config_data_t::qt_pos_recal_delay, and tag_qt_touch_lib_config_data_t::qt_recal_threshold.
Referenced by QDebug_Init(), and Set_Global_Config().
void write_info_to_eeprom | ( | uint16_t | lib_version | ) |
write_info_to_eeprom is used to Save information from library and sign in the EEPROM
write_info_to_eeprom is used to Save information from library and sign in the EEPROM
This function is used to Save information from library and sign in the EEPROM
\note | Will write the current library version to EEPROM |
References EEPROM_START_ADDRESS, and nvm_eeprom_write_byte().
Referenced by QDebug_Init().
void write_sensor_settings_to_eeprom | ( | void | ) |
write_sensor_settings_to_eeprom is used to Save sensor parameter settings to EEPROM
write_sensor_settings_to_eeprom is used to Save sensor parameter settings to EEPROM
This function is used to Save sensor parameter settings to EEPROM
\note |
References EEPROM_LIB_CONFIG_START_ADDRESS, num_sensors, and nvm_eeprom_write_byte().
Referenced by QDebug_Init(), and Set_Channel_Config().