In this section you can find all the projects related to the USB/CDC Standard I/O (stdio).
USB Device CDC Example for ATxmega128a1u on STK600 | |
Provide an application example of USB Communication Device Class (CDC) implementation: a bridge between USART and USB CDC interface. | |
USB Device CDC Example for ATxmega128a4u on STK600 | |
Provide an application example of USB Communication Device Class (CDC) implementation: a bridge between USART and USB CDC interface. | |
USB Device CDC Example for ATxmega256a3bu on STK600 | |
Provide an application example of USB Communication Device Class (CDC) implementation: a bridge between USART and USB CDC interface. | |
USB Device CDC Example for ATxmega32a4u on STK600 | |
Provide an application example of USB Communication Device Class (CDC) implementation: a bridge between USART and USB CDC interface. | |
USB Device CDC Example for XMEGA-A1U Xplained Pro | |
Provide an application example of USB Communication Device Class (CDC) implementation: a bridge between USART and USB CDC interface. | |
USB Device CDC Example for XMEGA-A3BU Xplained | |
Provide an application example of USB Communication Device Class (CDC) implementation: a bridge between USART and USB CDC interface. | |
USB Device HID Generic for ATxmega32a4u on STK600 | |
Provide an application example of USB Device HID Generic implementation. Relies on the native HID driver and uses buttons and LEDs available on the board. | |
USB Device HID Keyboard for ATxmega128a1u on STK600 | |
Provide an application example of USB Device HID Keyboard implementation. Relies on the native HID driver and uses buttons available on the board as a keyboard interfaces. | |
USB Device HID Keyboard for ATxmega128a4u on STK600 | |
Provide an application example of USB Device HID Keyboard implementation. Relies on the native HID driver and uses buttons available on the board as a keyboard interfaces. | |
USB Device HID Keyboard for ATxmega256a3bu on STK600 | |
Provide an application example of USB Device HID Keyboard implementation. Relies on the native HID driver and uses buttons available on the board as a keyboard interfaces. | |
USB Device HID Keyboard for ATxmega32a4u on STK600 | |
Provide an application example of USB Device HID Keyboard implementation. Relies on the native HID driver and uses buttons available on the board as a keyboard interfaces. | |
USB Device HID Keyboard for XMEGA-A3BU Xplained | |
Provide an application example of USB Device HID Keyboard implementation. Relies on the native HID driver and uses buttons available on the board as a keyboard interfaces. | |
USB Device HID Mouse for ATxmega128a1u on STK600 | |
Provide an application example of USB Device HID Mouse implementation. Relies on the native HID driver and uses buttons available on the board as a mouse interfaces. | |
USB Device HID Mouse for ATxmega128a4u on STK600 | |
Provide an application example of USB Device HID Mouse implementation. Relies on the native HID driver and uses buttons available on the board as a mouse interfaces. | |
USB Device HID Mouse for ATxmega256a3bu on STK600 | |
Provide an application example of USB Device HID Mouse implementation. Relies on the native HID driver and uses buttons available on the board as a mouse interfaces. | |
USB Device HID Mouse for ATxmega32a4u on STK600 | |
Provide an application example of USB Device HID Mouse implementation. Relies on the native HID driver and uses buttons available on the board as a mouse interfaces. | |
USB Device HID Mouse for XMEGA-A3BU Xplained | |
Provide an application example of USB Device HID Mouse implementation. Relies on the native HID driver and uses buttons available on the board as a mouse interfaces. | |
USB Device Mass Storage for ATxmega128a1u on STK600 | |
Provide an application example of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98). | |
USB Device Mass Storage for ATxmega128a4u on STK600 | |
Provide an application example of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98). | |
USB Device Mass Storage for ATxmega256a3bu on STK600 | |
Provide an application example of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98). | |
USB Device Mass Storage for ATxmega32a4u on STK600 | |
Provide an application example of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98). | |
USB Device Mass Storage for XMEGA-A3BU Xplained | |
Provide an application example of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98). | |
USB Device PHDC for XMEGA-A3BU Xplained | |
Provide an application example of USB Device PHDC implementation. Relies on the PHDC driver and uses buttons available on the board as a sensor interfaces. | |
USB Device Vendor Class example for ATxmega256a3bu on STK600 | |
Provide an application example of USB Vendor Class implementation. The example implements a look back application between IN and OUT enpoints of interrupt, bulk and isochronous types. Note that this example relies on a specific driver on the Host Operating System. For more detail documentation and PC drivers and application, please refer to AVR4001 application note. | |
USB Device Vendor Class example for ATxmega32a4u on STK600 | |
Provide an application example of USB Vendor Class implementation. The example implements a look back application between IN and OUT enpoints of interrupt, bulk and isochronous types. Note that this example relies on a specific driver on the Host Operating System. For more detail documentation and PC drivers and application, please refer to AVR4001 application note. | |
USB Device Vendor Class example for XMEGA-A3BU Xplained | |
Provide an application example of USB Vendor Class implementation. The example implements a look back application between IN and OUT enpoints of interrupt, bulk and isochronous types. Note that this example relies on a specific driver on the Host Operating System. For more detail documentation and PC drivers and application, please refer to AVR4001 application note. | |
USB QTouch Device HID Generic Example for ATxmega256A3BU on XMEGA-A3BU Xplained | |
Provide an application example of USB Device HID Generic implementation that uses QTouch key. Relies on the native HID driver and uses buttons and LEDs available on the board. |
USB Device CDC unit tests for ATxmega128a1u on STK600 | |
Provide an unit test of USB Device CDC implementation. | |
USB Device CDC unit tests for ATxmega32a4u on STK600 | |
Provide an unit test of USB Device CDC implementation. | |
USB Device CDC unit tests for XMEGA-A3BU Xplained | |
Provide an unit test of USB Device CDC implementation. | |
USB Device HID Mouse unit tests for ATxmega128a1u on STK600 | |
Provide an unit test of USB Device HID keyboard implementation. | |
USB Device HID Mouse unit tests for ATxmega128a1u on STK600 | |
Provide an unit test of USB Device HID Mouse implementation. | |
USB Device HID Mouse unit tests for ATxmega256a3bu on STK600 | |
Provide an unit test of USB Device HID Mouse implementation. | |
USB Device HID Mouse unit tests for ATxmega32a4u on STK600 | |
Provide an unit test of USB Device HID keyboard implementation. | |
USB Device HID Mouse unit tests for ATxmega32a4u on STK600 | |
Provide an unit test of USB Device HID Mouse implementation. | |
USB Device HID Mouse unit tests for XMEGA-A3BU Xplained | |
Provide an unit test of USB Device HID keyboard implementation. | |
USB Device HID Mouse unit tests for XMEGA-A3BU Xplained | |
Provide an unit test of USB Device HID Mouse implementation. | |
USB Device Mass Storage unit tests for ATxmega128a1u on STK600 | |
Provide a unit test of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98). | |
USB Device Mass Storage unit tests for ATxmega128a4u on STK600 | |
Provide a unit test of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98). | |
USB Device Mass Storage unit tests for XMEGA-A3BU Xplained | |
Provide a unit test of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98). |